Siemens Digital Industries Software Blog Network

Siemens Digital Industries Software Blogs


Corporate Blog

PLM Connection Americas Change of Venue

Below are a few videos on the flooding in Nashville that started two weeks ago. Our thoughts are with all those affected. As you can imagine, it’s created a little havoc for our PLM Conne...

Embedded Software

Books and e-books

All my life I have loved books. I was surrounded by them as a child and cannot remember a time...

Simulating the Real World

The art of modelling using CFD. Part II - Grilles

Wiki quote: “A grille is an opening of several slits side by side in a wall or metal sheet or...

Verification Horizons

High-Level Design Validation and Test (HLDVT) 2010

I’ve had the pleasure of participating in the IEEE International High-Level Design Validation and Test (HLDVT) workshop off and on...

Verification Horizons

New OVM Sequence Layering Package – For Easier Tests

Download Now A new OVM Layering Package that provides a means to add layers of tests (sequences) without modifying the...

Simulating the Real World

The art of modelling using CFD. Part I - What happens if you cross art with science?

Considering that CFD (Computational Fluid Dynamics) is an advanced mathematical method for predicting fluid flow and heat transfer using a computational...

Verification Horizons

OVM 2.0 Register Package Released

In January 2010 we released the OVM 1.0 Register Package.  It has now been updated to enhance capabilities and address...

Embedded Software

OS influence on power consumption

Power consumption is an issue. With portable devices this affects battery life. [I am irritated by the short intervals between...

Corporate Blog

Want to Design a Factory?

This is not an easy task as the amount of information to take into account is huge. Starting with architectural information like the plant layout to libraries of standard manufacturing equipment whic...