What’s new in Opcenter MES Medical Device 2607
Modernized application, reduced total cost of ownership (TCO), improved performance.
Summary
Opcenter™ MES software serves as the foundation for leading global manufacturers and product innovators that want to enable rapid change, lean manufacturing, consistent quality output, rapid new product introduction (NPI) and higher profit margins.
Integrated with enterprise resource planning (ERP), product lifecycle management (PLM), supply chain management (SCM), customer relationship management (CRM) and the shop floor, Opcenter MES completes the technology infrastructure for manufacturing. Solutions are architected for global use, enabling worldwide visibility for real-time control and mission-critical operations.
Opcenter MES Medical Device 2607 along with the Mendix™ Low-code platform, which is part of the Siemens Xcelerator business platform of software, hardware and services, delivers new enhancements to improve an application’s capabilities and user experience.
The application has been modernized to deliver greater business value such as reduced total cost of ownership, enhanced configurability, richer metadata management, greatly improved performance, embedded observability and a simple upgrade. An artificial intelligence (AI) performance copilot enables users to interact with manufacturing performance data using natural language.
Several key Mendix enhancements have been introduced, including streamlined user experience for the AQL Sampling and Audit Trail user interfaces. A more configurable resource job maintenance workflow empowers equipment technicians to manage equipment maintenance jobs more effectively. Finally, an equipment logbook supports easily recording and tracking activities performed on the resource.
Benefits
- Reduced TCO
- Enhanced configurability
- Rich metadata management
- Greatly improved performance
- Simple upgrade
Capabilities
Reduced Total Cost of Ownership (TCO)
- Reduces the overall hardware footprint through a more efficient, modernized deployment architecture
- Supports Linux‑based containers orchestrated using Kubernetes
- Enables zero‑downtime updates through a containerized deployment model
Enhanced Configurability
- Centralizes application configuration through a browser-based management interface, including:
- Model design
- Application configuration
- Deployment settings
- Application deployment and updates
- Application status monitoring
Rich Metadata Management
- Streamlines development using standard tools such as Microsoft Visual Studio
- Improves troubleshooting capabilities through enhanced diagnostics and step through debugging
- Supports collaborative development and structured source control practices
- Enables metadata code scanning and more efficient metadata release management
Greatly Improved Performance
- Architectural and processing optimizations enable faster transaction handling and improved responsiveness in high volume manufacturing environments
- The modernized platform supports higher throughput and scalability, providing a more resilient foundation for demanding shopfloor operations
Observability and Telemetry
- Collects and exposes application logs, metrics, and traces, along with Kubernetes‑level logs and telemetry, to support enhanced monitoring and diagnostics
Simple Transition
- Supports a streamlined upgrade through compatibility across four key areas:
- User interface – protects existing investments in Portal and Mendix applications
- API interfaces – preserves compatibility with existing WCF, REST, and XML APIs
- Metadata – safeguards existing metadata investments
- Reporting – enables the majority of existing reports to run without modification
Flexible Deployment
- Containerized deployment and orchestration in Kubernetes
- Deployable on premise / local private cloud or in a virtual private cloud on Amazon Web Services (AWS) or Microsoft
Mendix Audit Trail Enhancements
- Enhances the audit trail to be displayed from Operational View and Electronic Procedures pages
- Can be download as a PDF
- Supports filtering by:
- Transaction type
- Date
- Operation
- Employee
- Resource
- Displays information based on fields selected in the audit trail configuration modelling page

Artificial Intelligence – Performance Copilot
- AI-powered Mendix application that enables users to interact with manufacturing performance data using natural language
- Delivers real-time KPI insights, trend analysis, and production performance visibility
- Accelerates decision-making by reducing dependency on manual reporting and dashboard navigation

Electronic Procedures: AQL Sampling Enhancement
- Simplifies the presentation of sample requirements to the operator
- Configuration is available on the Sample Test
- If option is selected for the Sample Test, the remaining number of samples to be collected will be presented by default to the operator
- Removes the need for the operator to manually add the additional samples to be collected
Resource Job Maintenance
- Introduces a new maintenance workflow capability that supports resource maintenance execution
- Delivers a new maintenance specification to create and manage a maintenance workflow
- Provides enhanced shop floor settings with configurable numbering rules
- Associates job maintenance settings with the factory to support maintenance job execution
- Associates’ maintenance workflow with thruput requirements for usage-based maintenance
- Adds an option to close a job container in maintenance specifications to automatically close maintenance containers upon completion
- Can automatically trigger a maintenance workflow based on:
- Thruput requirement
- Date requirement
- Recurring date requirement
Equipment logbook
- Easily record and track all activities performed on a resource
- Defines a consistent structure and content for logbooks associated with the same resource type using logbook templates
- Quickly associate predefined actions and sub-actions when creating logbook entries, speeding up the creation process
- Collect specific data during logbook entry execution through configurable datapoints defined within sub-actions
- Perform multi-level reviews, enabling reviewers to efficiently approve or reject logbook entries
Additional enhancements
- Updates the browser tab to additionally show the page name
- Automatically selects the resource on the Move In / Move task if a resource is set on a container
- The splitter in the Mendix Electronic Procedures page is now draggable
Want to learn more? Opcenter MES Medical Device serves as the foundation for top-tier global manufacturers and product innovators that want to enable rapid change, lean manufacturing, consistent quality output, rapid new product introduction (NPI) and higher profit margins. Find out more about Opcenter MES Medical Device.