Products

Five Benefits of Integrated CAD/CAM for Mold and Die

This article first appeared in MoldMaking Technology magazine, Gardner Publications Inc., USA. www.moldmakingtechnology.com

Integrated NX CAD-CAM for Mold Manufacture 


Integrated computer-aided design and manufacturing (CAD/CAM) software that combines CAD, CAM, electrode design and CMM programming capabilities in one system can save you time and effort in the following five ways: 


  1. Eliminate extra and costly data translation steps between applications that are operating on the same 3-D model.  Some systems offer a complete set of fully integrated applications for the complete process from part design through mold design, NC programming, electrode design and CMM inspection programming.


  2. Automate more of the manufacturing authoring process: (a) automate NC and CMM programming by using design requirements (GD&T and product manufacturing information (PMI), and color coding) directly on the 3-D model; and, (b)  store NC data inside the standard part’s 3-D model file.  For example, the NC data inside a standard slide model can be easily updated to its determined design dimensions.


  3. Use integrated validation tools throughout the process. Integrated CAD/CAM systems can include tools to validate (and even improve) part and tool designs: molded part manufacturability checks, injection molding simulation, and tool motion simulation with collision detection. Before machining, validate NC data with integrated g-code driven machine tool simulation.


  4. Keep your data organized so you can work in teams, work in parallel and react faster to design changes.  For example, using a master model with associativity allows you to update your mold design, NC programs, electrodes, and setup sheets when the CAD model changes. Associativity makes design changes go faster and simple changes can be updated automatically— they don’t require reprogramming because they automatically re-adjust.  More than one designer can work on the same tool at the same time; and, you can start NC programming before the tool design is completed.


  5. Share knowledge between departments so designs can be done right the first time with manufacturability taken into consideration. When everyone works on the same system, this is much easier to do and the benefits can be substantial. Unfortunately in some cases, designers do not realize the impact of their decisions on the manufacturing process.  Design features that are difficult to manufacture can add extra costs to jobs. They can add extra manufacturing steps and extra NC programming time due to feature redesign.  When NC programmers and designers work with the same system, it’s much easier for both disciplines to work together. Some CAD/CAM systems have the ability to copy features and store them in a library for later use or can create custom features. When this is the case, NC programmers can work with designers to specify features that include manufacturability considerations. Designers can reuse these features from a library (saves design time) with the confidence that manufacturing knows how to machine them.


 


Summary Statement


When you are able to start with a clean sheet and complete the whole process with the same system, the value of using one integrated CAD/CAM system pays off.  Besides the process-based benefits summarized above, additional benefits are to be gained in the forms of reduced training costs due to one easy-to-learn consistent user interface, administration of one system and working with one vendor.

If you’re interested in reading how mold and die manufacturers are using NX, here’s a sampling of some interesting customer stories from across the globe:
































Minco Minco (United States) – “We don’t just design a part, we manufacture it, so it is important to take it all the way through the process with the same software.”
Moules Mirplex Moules Mirplex (Canada) – “To help us stay ahead of the competition, we use the combination of NX CAD, NX CAM and the SINUMERIK 840D controller from Siemens.”
Flextronics Flextronics (Guadalajara, Mexico facility) – Guadalajara facility sets corporate-wide example for quality, shorter lead times and effective implementation of new technologies. 
Jaguarmold Jaguarmold (Brazil) – Leading mold manufacturer reduces project development time by 40 percent; NX CAM and synchronous technology play critical role
Fu Sheng Group.png Fu Sheng Group (Taiwan) – Golf manufacturer reduces mold production time 67 percent – from three weeks to 7 days
Rasandik Rasandik Engineering Industries (India) – 3D die design and optimized toolpath programming result in big time savings for Rasandik Engineering
Hofmann Hofmann Werkzeugbau (Germany) – NX enables design lead-time savings

About the Author








Community.jpg Aaron Frankel is with the marketing team at Siemens PLM Software and focuses on part manufacturing solutions. He has been in the PLM industry for over 15 years and enjoys helping companies apply innovative technology solutions to design and manufacturing challenges. Aaron resides in Southern California with his family.

Aaron Frankel

Aaron Frankel is with the marketing team at Siemens PLM Software and focuses on part manufacturing solutions. He has been in the PLM industry for over 15 years and enjoys helping companies apply innovative technology solutions to design and manufacturing challenges.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/nx-manufacturing/five-benefits-of-integrated-cad-cam-for-mold-and-die/