Products

NX X Essentials | How to | Editing Imported Geometry

NX X Essentials empowers users to upload, edit and save designs from any device, removing the barriers of traditional CAD setups. In this post, we’ll walk through how NX X Essentials helps teams import files, make synchronous edits and maintain design intent, all while working in the cloud. 


Import models with ease 

NX X Essentials simplifies the process of importing geometry. Users can upload files from popular platforms such as SolidWorks, Creo, Inventor, Solid Edge, NX and more. Once processed, the model is ready for 3D markup or direct editing—all from within the browser. 

No additional software is required. No installation is needed. Just instant access to your design. 


Synchronous editing, built-in 

Editing geometry in NX X Essentials is intuitive and powerful. Users can easily adjust angles, move features and resize components with full control: 

  • Select a face and use the triad to rotate components—drag interactively or key in exact angles like 4° 
  • Resize geometry while preserving relationships, such as symmetry, automatically detected by the system 
  • Move holes or other features to precise positions with simple drag-and-drop interactions or numerical input 
  • Remove features instantly using the delete command 
  • Every edit happens in real time, giving teams the flexibility to iterate quickly and maintain momentum. 

Design intent, preserved automatically 

NX X Essentials doesn’t just modify geometry—it understands it. Design intent such as concentricity and symmetry is retained throughout the editing process, ensuring that key relationships stay intact even as models evolve. 

When resizing a plate or shifting features, constraints defined in the original CAD file are honored, helping reduce errors and maintain design consistency. 


Smart version control for peace of mind 

Once edits are complete, NX X Essentials saves a modified version of non-NX files while preserving the original. This dual-saving approach gives users confidence to explore changes while always retaining a backup for reference or reuse. 

When working with NX files, edits are applied directly to the original file, though users can choose ‘Save As’ to create a separate version if needed. Both original and modified files are stored within the project and remain fully accessible at any time. 


Access CAD, CAM and CAE in one place 

More than just a CAD editor, NX X Essentials brings together design, manufacturing and simulation tools in one lightweight, web-based platform. From modeling to documentation, teams can handle every phase of the product lifecycle—all from a browser. 


Designed for modern engineering teams 

Whether you’re on the shop floor, in the field, or working remotely, NX X Essentials gives you the power to design and collaborate wherever work happens. Its browser-based interface ensures fast access, low setup overhead and seamless team coordination. 


Try NX X Essentials today 

Explore the future of design with a flexible, browser-based solution that moves as fast as your ideas. 

Learn more 

Akos Owusu-korkor
Shannon McGinty
Senior Marketing Co-Ordinator

Shannon studied Creative Writing at university where she thrived in exploring different ways to express her ideas. Across different written forms Shannon was able to establish her writing skills and continue to improve them throughout her degree and beyond. After moving to Madrid and completing an internship in publishing, Shannon began her role at Siemens Digital Industries Software in 2018 where she was able to hone her learnt skills into a new area. Although not from a background in software, Shannon is able to tailor her written skills to be relatable and useful for readers through her experience of events at Siemens. Shannon works very closely with our customers for these events and helps them sculpt their business challenges and achievements into compelling stories. Across Designcenter NX CAD software, Siemens Xcelerator products, including Teamcenter, NX CAM and Simcenter these carefully crafted pieces tie in her love for Creative Writing and key marketing outputs across a range of business sectors.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/nx-design/nx-x-editing-imported-geometry/