Products

What’s new in NX | June 2024 | Advanced Design

Welcome to our latest What’s new blog, where we delve into the cutting-edge advancements in NX™ software’s design functionality. In this edition, we explore the powerful new features and enhancements that are revolutionizing the way engineers and designers approach advanced design challenges.

From the innovative Sketch Navigator to the expanded lattice filtering capabilities, NX continues to push the boundaries of what’s possible in digital design and manufacturing. Join us as we uncover how these updates not only enhance user experience but also significantly improve efficiency and precision in creating performance-optimized structures.

Let’s dive into the details and see how NX is setting new standards in the industry.

Introducing the new Sketch Navigator

The latest Sketch Navigator in NX transforms sketch interaction by enabling continuous browsing of geometry, relations, and dimensions. Organized into tabs for Curves, Relations (both Found and Persistent), External References and Issues, it offers streamlined and intuitive user experience.

Each tab includes columns for Title, Status, Source, and Value, providing detailed insights into object types, definition status, origins, and editable dimensions or expressions. The Curves tab shows the status of each curve, while the Relations tab displays both relaxed and active found relations, dimensions, and expressions.

This image shows the user interface for the sketch navigator

The External References tab highlights the source geometry for projected or included entities, and the Issues tab identifies any conflicting persistent relations and expressions. Right-clicking on a sketch name and selecting Edit Parameters reveals all found relations, with new options to Show/Hide Parents and Reset Navigator Panes enhancing overall functionality and user control.

Expanded lattice filtering and connecting capabilities

This release has also shown greater control over lattice designs, allowing you to tailor structures to meet specific functional requirements. These improvements significantly boost engineering flexibility and speed, enabling the design of performance-optimized structures achievable only through additive manufacturing.

The Filter Lattice Enhancements introduce new capabilities, such as connecting dangling rods back to the body lattice, enhancing the robustness of lattice structures. The Voronoi Lattice Enhancements expand lattice filtering abilities, making it easier to create complex structures.

This image shows lattice filtering for advanced design

New filter options—Filter by Thickness and Filter by Ratio—along with filtering parameters provide precise control over lattice design. Additionally, the new feature allows for connecting dangling rods to the inner lattice, only to other dangling rods, or a combination of both, with options to control the connection based on proximity or within a specified region. These advancements collectively enhance the design process, making it a more intuitive and efficient interface for users.

Gaussian pore size distribution for Voronoi lattice structures

The June 2024 release has also introduced a Gaussian distribution option, providing further control over lattice designs by enabling the creation of randomized Voronoi structures. This new distribution option randomizes pore sizes based on a bell curve, allowing for more natural and varied lattice formations.

This image shows the creation of randomized Voronoi structures.

Additionally, it includes a feature to create spikes at selected faces of the lattice structure, enhancing the design’s complexity and functionality. The Gaussian distribution joins existing options like Uniform and Variable, and now both Uniform and Gaussian distributions support variable rod diameters via fields.

This update also introduces the ability to create spikes on both volume and surface volume Voronoi structures, offering designers more flexibility and precision in their lattice designs.

Improved efficiency in constructing complex wireframes

This release has also shown significant workflow efficiency for constructing complex wireframe shapes on bodies. The Curve on Surface command now supports new input types and enables the creation of geodesic curves, which follow the shortest path on a surface.

With the introduction of Line and Arc/Circle options, users can utilize standard construction methods to generate curves on surfaces. These resulting curves can be created using either the Projection method, which is normal to the surface, or the Geodesic method, which minimizes arc length on the surface.

For spline types, you now have control over Tangent Magnitude at endpoints and can access U/V values in the Part Navigator Details pane. Beyond this, the Bridge Curve with Face Constraint feature now supports G2 continuity, ensuring smoother transitions between curves and surfaces.

Conclusion

The latest updates in NX bring a host of advanced design functionalities that enhance user experience, improve efficiency, and provide greater control over complex designs. These features collectively make NX a powerful tool for engineers and designers aiming to achieve performance-optimized structures tailored to specific engineering requirements.


Continue your journey with NX

Be sure to check out the full premiere on YouTube, where you can see a range of other capabilities added to the June 2024 release of NX.

Drew Wilson
Copywriter - Siemens Digital Industries Software

Drew Wilson is a Copywriter at Siemens Digital Industries Software where he crafts compelling, technically-informed content for Designcenter NX. As a graduate of Xavier University with a degree in Advertising + Public Relations and a concentration in Technical Writing, Drew brings a unique blend of creative storytelling and precision to his work. Before his time at Siemens, Drew honed his skills in an agency environment, writing for over 70 midsized manufacturing companies. His experience spans both traditional industrial sectors and the fast-paced startup world, giving him a versatile perspective writing styles and outlets. Since joining Siemens Digital Industries Software in 2023, Drew has contributed to a wide range of initiatives that have deepened his expertise in CAD software, PLM systems, and particularly Designcenter NX. His work supports product teams, marketing campaigns and customer-facing content, helping to translate technical innovation into accessible narratives that resonate with engineers, decision-makers and end users alike.

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/designcenter/whats-new-nx-june-2024-advanced-design/