Thought Leadership

Designing power management software for embedded systems

An increasingly important factor in embedded software development is power management. Historically, this was a solely hardware issue; that has all changed in recent years. Once the software has the ability to take control of factors that affect the system’s power consumption, it is logical that it should exercise that control in an efficient way.

Much is said about the implementation of power management software, but less is said about its design …

There are a few key concepts that need to be understood when discussing power management software.

The first is the idea of a Use Case. This is a scenario of operation of the device. It may be the performance of a specific operation – like displaying some data, or taking a sample from sensors or sending data over a network. It could also be an idle state, when the device is just waiting for something to happen. A use case may be initiated by a human user, but could equally be triggered by an external event or a timer.

Each use case puts a number of demands on the system. A specific amount of CPU power is required to do the job in hand. By using DVFS [Dynamic Frequency and Voltage Scaling], the power management software can select a voltage/frequency combination that delivers just the necessary computing power, thus minimizing power consumption. These parameters are called an Operating Point. In addition, each use case will require access to a different set of resources – peripheral devices etc. – and these can be selected [powered up] by the power management software, as required.

So, the implementation of an application using power management is a question of transitioning between each use case – the PM software takes care of selecting the operating points and resource availability. It occurred to me that this kind of structure was very familiar. It sounds like a state machine. So, it must make sense to use a design approach – UML comes to mind – where a state machine is a possible paradigm. Just a thought …

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2017/07/24/designing-power-management-software-for-embedded-systems/