PCBflow, Cloud DFM for PCBs

PCB 102: How PCB Design Requirements Affect Fabrication

Printed Circuit Boards (PCBs) are an essential component of modern electronics, and their design and fabrication are critical to the…

Making Parts Part of Manufacturing Driven Design

When it comes to PCB assembly level MDD, many designers have not concerned themselves with the component manufacturing Bill of Material (BOM). Designers work from a CAD library that has component libraries associated with internal part numbers (IPN) their company uses. The CAD Design Rule Checking software uses those CAD library shapes for its analysis and even, in some cases, the avoidance of where components are placed. There is nothing wrong conceptually with this mentality. However, like all things, the details matter.

detectives investigate DFM within a PCB design

The Mysterious Case of the Missing Bowties Part III

Previously… People often say ‘better late than never’, but I’ve never heard my boss say that. After much difficulty in…

The Mysterious Case of the Missing Bowties Part II

Previously… After receiving our boards and having them pass inspection I breathed a sigh of relief as this project was…

The Mysterious Case of the Missing Bowties Part I

It was just another Monday at the office. I had released a design I had been working on for four…

PCB DFM Constraints with Valor NPI

Advanced DFM Constraints management in ADM (Analysis Definition Manager)- Valor NPI 2211

The Analysis Definition Manager (ADM), introduced in Valor NPI 10.0, is a constraints management tool for creating and maintaining sets of Design for Manufacturing DFM rules to be used during the analysis in Valor NPI.

flex PCB technology

Top 5 rigid-flex design guidelines

Rigid-flex DFM I am not sure if you have seen a rigid-flex circuit before, but I bet you must have…

PCB manufacturing capabilities

Why is Design for Manufacturing important?

Who is PCB DFM for? For those of us that have climbed a mountain to take in the gaze of…

What's new with Valor NPI DFM software release 11.5

What’s new in Valor NPI v11.5

Valor NPI 11.5 continues to introduce new and existing capabilities in MRA-Revolution, with a more complete Classification set which includes design preparations and analysis use of copper reference layers. Comparing an ODB++ to fabricator changes becomes easy and precise with the new CAM Compare flow and the first connection to stackup setup is established with Z-Planner integration.