Products

Why bother with Rust in Embedded Software Engineering?

Why Rust, and why now

Embedded software is being asked to do more, more connectivity, more parallelism, more security, and more safety, on the same tight hardware budgets and development timelines. For decades, C (and later C++) were the default answers. Today, Rust is increasingly showing up as a credible alternative for parts of embedded systems where reliability and long-term maintainability matter as much as raw performance (The Top Programming Languages 2025 – IEEE Spectrum).

This post focuses on the “why”: what is driving Rust adoption, what it changes for embedded engineering, and what tradeoffs to expect. In upcoming posts, I’ll go deeper into (1) Rust technical foundations for embedded, (2) Rust in AUTOSAR (Classic and Adaptive), (3) multi-core and performance considerations, and (4) model-driven development workflows with Rust.

Why Rust now: signals that embedded is paying attention

  • Rising mindshare: Rust is climbing language popularity rankings (e.g., it reached rank 14 in an IEEE “Top Languages” list for 2025) and appears frequently in conference talks and industry news.
  • Platform-level endorsements: Rust code is accepted into the Linux kernel, and major vendors increasingly ship Rust-capable toolchains.
  • Adoption beyond “web backends”: Aerospace and defense communities are actively evaluating Rust for safety- and security-relevant software.
  • Big-tech usage at the lowest layers: Microsoft has publicly discussed using Rust for low-level components such as drivers, exactly the kind of territory embedded engineers care about.
  • Automotive pull: Automotive customers have started asking tool and platform vendors about Rust support. The realistic trend is not “rewrite everything in Rust”, but “start where it hurts most and integrate well with existing code”.

What Rust brings to embedded engineering (beyond hype)

Rust’s core promise is straightforward: memory safety and data-race freedom enforced at compile time, without a garbage collector and without giving up predictable performance (The Move to Memory-Safe Programming – IEEE Spectrum).

  • Compile-time memory safety: eliminates whole classes of bugs (use-after-free, double free, many buffer overflows) before code ever runs.
  • Compile-time type safety: expressive types, enums, and pattern matching make illegal states harder to represent.
  • Safe and efficient concurrency: Rust’s rules around ownership and borrowing prevent many data races by construction, which matters as embedded platforms become increasingly multi-core.
  • Performance: Rust is designed for “no surprises” efficiency (ahead-of-time compilation, no mandatory runtime, no garbage collection pauses).
  • Ecosystem and tooling: a modern build and dependency workflow (Cargo + crates) and strong IDE support reduce friction compared to many traditional embedded toolchains.

Two common objections are worth addressing early. First, the learning curve: Rust can feel “steep” mainly because it is different, especially around ownership and lifetimes, but many teams report that the upfront investment pays back in fewer late-cycle debugging surprises. Second, compilation time: Rust’s compiler performs extensive checks, so builds can be slower than in some C/C++ setups; the trade is that more defects are pushed left into compile time.

The business angle: why engineering leaders care

Rust featureBusiness impactTypical benefit
Memory & type safetyReduced development and maintenance costFewer production defects; fewer late-cycle bug hunts
Safe concurrencyFaster time-to-market for multi-threaded/multi-core featuresMore predictable behavior under load; fewer concurrency regressions
Build system (Cargo) + dependency managementFaster and cheaper extensionsReusable modules (crates); easier cross-team collaboration
Rich library ecosystemReduced release issuesLess reinvention; quicker prototyping and integration
Portability across platformsLonger product lifetime, easier platform transitionsMore reuse across ECUs/MCUs and operating environments

Rust fits how embedded teams actually program

Rust isn’t “purely functional” or “purely object-oriented”, and that’s a strength for embedded. It supports multiple styles while keeping its safety guarantees.

  • Functional-friendly: immutability by default, higher-order functions and closures, algebraic data types (enums), and pattern matching. For performance, Rust does not force recursion, loops are idiomatic, and allows explicit mutability when you need it.
  • Object-oriented & procedural-friendly: structs/enums, methods, macros, and polymorphism via traits. Rust strongly favors composition over inheritance and avoids implementation inheritance (preventing classic issues like the diamond problem), while still supporting “interface inheritance” patterns through traits.

Crucially for embedded, Rust enforces memory safety without runtime garbage collection. The compiler’s borrow checker tracks lifetimes and reference integrity at compile time, which is why many memory safety errors and data races simply don’t compile.

Tooling maturity: embedded Rust is no longer “just a language”

What makes Rust interesting for embedded isn’t only the syntax, it’s the surrounding ecosystem that reduces “glue work” and makes cross-platform development realistic.

  • rustc + LLVM backends: the Rust compiler builds on LLVM and supports a wide range of targets, including common embedded architectures.
  • Cargo + crates: a default build system and dependency manager that makes modularization and reuse straightforward.
  • FFI support: bindings to connect Rust with existing C/C++ code (critical for brownfield embedded codebases).
  • Hardware Abstraction Layers (HALs): community and vendor layers that standardize peripheral access patterns.
  • Execution frameworks: async and concurrency frameworks such as Embassy (aiming for compile-time safe concurrency and power efficiency without a heavy runtime) and Tokio (more common in OS-based/networked contexts).
  • OS/RTOS options: Rust can run bare metal or integrate with environments such as AUTOSAR, Zephyr, QNX, FreeRTOS, Fuchsia, and Linux, depending on the target and constraints.

Commercial toolchains and IDE support

Rust is also supported by commercial compiler toolchains and vendors, which matters for regulated embedded domains that require qualified tools, long-term support, and audited supply chains. In practice, many teams combine the standard Rust toolchain with vendor-specific compilers, debuggers, and analysis tools where certification and support commitments are needed.

On the developer experience side, Rust works well in mainstream editors: VS Code has strong Rust extensions, there are terminal-first options (Vim/Emacs/Helix), and JetBrains IDEs such as IntelliJ IDEA and CLion offer Rust plugins. This matters because embedded teams rarely adopt a language in isolation, they adopt (or reject) the whole workflow.

Competitive reality: the industry is positioning for Rust

Even if you ignore the hype cycle, it’s hard to ignore the messaging: across the embedded tooling market, vendors increasingly highlight Rust in roadmaps, experiments, or supported workflows (Volvo with Julius Gustavsson – Rust in Production Podcast | corrode Rust Consulting). That’s usually a sign of two things: (1) customers are asking, and (2) vendors believe Rust can become a differentiator for safety, security, and maintainability. See also Rust at Volvo Cars – Julius Gustavsson – NDC TechTown 2025 – YouTube.

A pragmatic adoption model: brownfield first

One rumor that regularly pops up is that entire existing codebases will be “ported to Rust.” In most embedded organizations, that’s unrealistic and unnecessary. The more credible path is incremental adoption: keep proven C/C++ where it makes sense, and introduce Rust where safety and concurrency risks are highest. That makes language bindings and FFI a first-class requirement, not an afterthought.

Conclusion: “Why bother?” Because the pain points are shifting

Embedded engineering is moving toward more connected, more parallel, and more security-relevant systems. Rust targets exactly the failure modes that become expensive at that scale—memory corruption, data races, and brittle integration, while keeping the performance profile that embedded systems require. If your organization is already feeling the cost of late-cycle debugging and long-term maintenance in C/C++, Rust is worth evaluating as an additional tool in the toolbox.

Next in this series

  • Rust for embedded, technical essentials: ownership/borrowing, lifetimes, error handling, and no-std patterns.
  • Rust in AUTOSAR: how Rust components can coexist with C in Classic, and what Rust bindings mean for Adaptive.
  • Multi-core and performance: what Rust guarantees, what it doesn’t, and how to measure impact.
  • Model-driven development with Rust: where code generation helps most, and how Rust can reduce integration mistakes.

If you’re working in embedded (especially automotive), I’d love to know: where would Rust help you most, device drivers, safety-critical control, integration glue, or network-facing components?

Capital Software Developer with IBM Rhapsody

Jan Richter

Armin Lichtblau

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/ee-systems/2026/07/29/why-bother-with-rust-in-embedded-software-engineering/