Products

Teamcenter Assistant, an Artificial Intelligence Application

By Projyal

Everyone can benefit from the convenience and user-friendliness of an artificial intelligence application.  AI makes tasks simple. No one needs to be an “expert” to use the products that are integrated with AI. ‘Siri’ and ‘Alexa’ are only some examples of how AI can be used to provide an outstanding user experience. Most modern users are habituated to using smart applications in their day to day life. They expect a similar experience from all products whether it is consumer or enterprise software. Users demand smarter applications which allows them to do their work quickly without incurring too much cognitive load.

While working with Teamcenter Active Workspace, have you ever wondered, what is the next step? Where is that command that I was working with last week? Or perhaps you are new to a domain and the entire user interface is completely new to you. A little assistance wouldn’t hurt… right?  Teamcenter is being used widely by users from various domains across the entire organization… our customers are demonstrating every day that PLM is not just for engineers!  

Introducing Teamcenter Assistant

An AI command prediction system that helps direct you inside Active Workspace to the relevant commands at your fingertips. Sounds like magic? We know.

Screenshot of Artificial Intelligence Application
Teamcenter Assistant provides the data and the commands in a clean user interface, allowing you to access the tips simply while ensuring you can concentrate on the task on hand.

Teamcenter Assistant uses machine learning techniques to learn from your peers, your usage, and your preferences. It has the ability to understand the context you are in to suggest the most relevant command and data. The tool provides the data and the commands in a clean user interface, allowing you to access the tips simply while ensuring you can concentrate on the task on hand. Teamcenter Assistant uses unsupervised learning techniques, the more you use it, the more it optimizes and provides better suggestions in the future.

Since Teamcenter Assistant is sensitive to the context of your current usage, it provides you the best possible actions for your current task. If you are new, the tool will provide the commands and data based on your team’s history of usage.

Artificial Intelligence Application Meets PLM

Within the demo, it’s obvious that Teamcenter Assistant is not just another UI widget, but it is a framework on which more capabilities can be built, and it is also possible to customize certain aspects of Teamcenter Assistant.

PLM success with AI/ML

Teamcenter Assistant is an artificial intelligence application that takes Teamcenter beyond traditional PLM and allows a wider user base to harness the power of PLM by making it simpler to use and provides guidance at your fingertips. This new advancement will help you and the rest of the organization perform tasks quickly and allow everyone to concentrate on their own expertise and creativity instead of spending time figuring out how to use the application. We will continue to add more features to ensure that you spend less time understanding the tool, and more time on your work.

If you’re interested in more details, check out the Active Workspace webpage and the recent blog written about Realize LIVE Americas 2020 where we dove into the productivity of the future and the basics of Teamcenter Assistant.

Projyal Dev

Product Manager of Data Sharing, Extensibility, FMS and Dispatcher in the Foundation area

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/teamcenter/teamcenter-assistant-an-artificial-intelligence-application/