Products

Benefits of a Solid Edge CAM Pro Bundle

By wrightj

bun-dle; noun – a collection of things, or a quantity of material, tied or wrapped up together.  Software is often sold in bundles, and we are no exception to the rule.  Over time, individually-developed features tend to get pushed into a bundle, and then get sold at a discount.  For example, when we first released Cavity Milling it was an extra-cost feature, but now it is part of the 3-Axis bundle.

There is an advantage to our customers for buying bundles – we discount bundles over the individual features.  You get more features at a cheaper price.  There is also an advantage for our sales force – we don’t have to spend a tremendously long time explaining a feature and justifying it’s price on a quote sheet.  “I’m not sure I really need ZEN-PIE conversion feature.  Could you explain that one again?”  Instead, we group feature sets into typical workflows or product capability, like 2.5 Axis, 3 Axis, etc…

There are several buying options for Solid Edge CAM Pro, so let’s break down the possibilities a little:



  1. CAM-only bundle

  2. CAD + CAM bundle (my favorite)

  3. Ad hoc combination of add-ons


CAM-only bundles


There are 4 main varieties of the CAM-only bundle:











































































































































































Product Name



Feature Set



Add-ons



2.5 Axis Milling



Gateway and CAM Base



3-Axis Milling Add-on



Translators



5-Axis Milling Add-on



Assemblies



Simulation Add-on



WAVE Geometry Linker



Turning Add-on



Machining Wizard Builder



Machining Knowledge Editor



Toolpath visualization and material removal



4-Axis Wire EDM



Graphical toolpath editing



Turbomachinery



Postprocessing



Post Builder and Post Configurator



Shop Documentation



Work Instruction Authoring



Planar Milling



Face Milling



Cavity Milling



Z-Level Profiling



Feature Based Machining



Generic Motion Control



Probing



3+2 Positioning



3-Axis Milling



Everything above plus…



5-Axis Milling Add-on



Fixed Axis Area Milling



Simulation Add-on



Flow Cut for Valley Rest Milling



Turning Add-on



Streamline Milling



Machining Knowledge Editor



Cut Between Levels for Semi-finishing



4-Axis Wire EDM



Nurbs and spline output



Turbomachinery



Facet Machining



Adaptive Clearance Strategy



5-Axis Milling



Everything above plus…



Simulation Add-on



Sequential Milling



Turning Add-on



Variable Axis Surface Milling



Machining Knowledge Editor



Contour Profiling



4-Axis Wire EDM



3-to-5 Axis tilt tool



Total Machining



Everything above plus…



Turbomachinery



Turning



4-Axis Wire EDM



Integrated Verification and Simulation – both tool path and G-Code driven



Machine Tool Builder



Machining Knowledge Editor



Multi-channel synchronization


As you can see, Total Machining gives you everything except Turbomachinery, and you can expect the bundle prices to be lower than individual items.

CAD + CAM bundle


You can take any bundle above and combine it with Solid Edge Foundation, and get it at a reduced price versus buying them separately.  This is a very big advantage, because these are still separate seats of software.  You could install Solid Edge on one computer and have someone working on a new design, while another person works on a separate computer creating tool paths with Solid Edge CAM Pro at the same time.  That’s a value that embedded CAD/CAM products can’t provide.

Ad hoc combination of  add-ons


Let’s say you want to have a CAM seat that does Turning and Wire EDM.  You can do that:


1 seat of Solid Edge CAM Pro Foundation (the gateway application)


1 seat of Turning


1 Seat of Wire EDM


I can’t think of another ad hoc combo.  Most other combinations are included in one of the above bundles at a cheaper price.

If you’re attending IMTS, why not stop by booth 134500, East Building and see us?  You can get a live demo of both Solid Edge and Solid Edge CAM Pro.  We will also be showing off some live machining.

Comments

13 thoughts about “Benefits of a Solid Edge CAM Pro Bundle

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/solidedge/benefits-of-a-solid-edge-cam-pro-bundle/