Can Cows Fly? Simcenter FLOEFD Investigates. Part 1 – Only in the Mooovies
It has been observed that cows tend to stand with their rumps facing the oncoming wind. There has been much debate (if you know where to look), stretching back almost weeks, as to why this might be. We’ll come back to this pressing question at the end of this blog series. In the mean time I’ll present some simulation studies performed by a colleague, Sergio Antioquia (bio at the end of this blog), that investigate the aerodynamic nature of cows, using Simcenter FLOEFD, our MCAD embedded highly automated CFD (Computational Fluid Dynamics) software product.
Cows haven’t evolved to fly. Quite the opposite. Actually the only people known to have witnessed flying cows have been Helen Hunt and Bill Paxton. So what kind of wind forces must cows withstand as they munch away? What chance is there of them flying off
when the wind picks up? Sticking something in an oncoming air flow and simulating the resulting air flow and noting the cow’s integrated surface pressure distribution is a very straight forward with Simcenter FLOEFD.
The original CAD image of the cow that we used is shown here. Hardly distinguishable from real life, it’s no surprise that the web site I downloaded it from had this disclaimer!
Over the coming parts of this blog we’ll be using Simcenter FLOEFD‘s unique octree splitting, polyhedral meshing system and its integral boundary layer approach to study lift and drag coefficients, the effect of the Beaufort Scale and how windy it will have to get for the cow to lift off!
For now, a sneak peek at Simcenter FLOEFD‘s adaptive mesh refinement technology, mesh just where you need it, automatically:
and cow surface pressure distribution and 2D streamlines shown using arrows on a downstream plane:
Can Cows Fly? Simcenter FLOEFD Investigates. Part 1 – Only in the Mooovies
Can Cows Fly? Simcenter FLOEFD Investigates. Part 2 – Aerocownamic Lift and Drag
Can Cows Fly? Simcenter FLOEFD Investigates. Part 3 – Superbly Sonic

17th September 2015, Hampton Court (Sergio), Ross-on-Wye (Robin)