Products

Simcenter Tire launches Tire Model Marketplace to democratize tire model parameters

Siemens Digital Industries Software announces the launch of the Simcenter Tire Model Marketplace, a new way for vehicle OEMs and their TIER suppliers to obtain high quality tire model parameters at a significantly lower price than traditional engineering services. Using a methodology centered around the MF-Tyre/MF-Swift tire model, fit-for-purpose tire model parameters sets are provided with an optimal balance between accuracy and cost. Simcenter Tire Model Marketplace offers close to 100 predefined and validated tire model parameter sets that are directly available and can be used for a variety of vehicle dynamic simulation applications.

Simcenter Tire performs on-road tire measurements from which parameters are derived that feed the MF-Tyre/MF-Swift tire model. While this method creates very accurate models, it is also cost-intensive. With Simcenter Tire Model Marketplace, customers can use off-the-shelf tire model parameter sets based on on-road tire measurements. This model lowers the price level of parameter sets significantly, giving a wide variety of customers access to a premium solution used by world-leading passenger car manufacturers.

More information and the extensive list of tire model parameter sets is available in this downloadable PDF.

For more information or/and to receive an official offer, please visit our website.

Loes vanHaasteren
This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/simcenter-tire-launches-tire-model-marketplace-to-democratize-tire-model-parameters/