Products

Femap 11.2.1 Release

Femap version 11.2.1 is now available for download from the GTAC site.

Femap 11.2.1 SplashScreen



Choose the Download and Upload Files option to access the SPLM Download Server. Then choose All Siemens Products, pick Femap, and version 11.2.1 can be downloaded from the Full Products, Windows 64-bit selection.



The download consists of a zipped image of the Femap 11.2.1 DVD. Unzip to a temporary location and install as usual.

Femap v11.2.1 addresses several issues evident in version 11.2, and also includes the latest version of NX Nastran. It is highly recommended that all v11.2 customers switch to v11.2.1. Customers upgrading from previous versions of Femap should install v11.2.1, not v11.2. Femap v11.2.1 corrects the CBUSH issue detailed in SFB-FEMAP-9054. For those customers using Femap with NX/Nastran, v11.2.1 also includes the recently released NX Nastran v10.2.

Femap v11.2.1 is 100% licensing and database compatible with v11.2. 



Details of the contents of this release can be found in the README.PDF file that is installed with Femap v11.2.1

Alastair Robertson
This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/femap-11-2-1-release/