Products

The brain in a jar problem – Why AI without context is failing the enterprise

This article explains why enterprise AI initiatives are underperforming despite significant investment — and introduces Intelligence Center X, Siemens’ answer to the context problem. It covers the disconnected nature of core enterprise systems, the concept of the “context layer” as the missing foundation for effective AI and how Intelligence Center X brings together a knowledge graph, AI modeling, agentic application development and unified governance into a single integrated solution for the autonomous enterprise.

 Published following the Intelligence Center X announcement at Realize Live 2026 in Detroit.

The problem most enterprises can’t name yet

They’ve invested in AI. They’ve run pilots. They’ve hired data scientists and stood up data platforms. And yet, the results are underwhelming —not because the AI is bad, but because it can’t see the whole picture.

At Realize Live 2026 in Detroit, Siemens Digital Industries Software announced Intelligence Center X to solve this exact challenge.

To find out more about Intelligence Center X listen to the conversation between Sam Mahalingam (EVP simulation, HPC and AI), Ravi Kunju (SVP product strategy and marketing) and Yeshwant Mummaneni (SVP HPC, AI, MDAO & SaaS):

To set the scene, Ravi, put it simply:

Without connecting the heartbeat, the nervous system and the brain, intelligence is nothing but a brain in a jar. It does nothing.

That’s not hyperbole. That’s the diagnosis.

lit up brain

The golden triangle is broken

Ask any CIO in manufacturing, aerospace or automotive what their core systems are, and you’ll get the same three answers: Product Lifecycle Management (PLM), Enterprise Resource Planning (ERP) and Manufacturing Execution System (MES).

  • PLM (like Teamcenter) is the digital brain – it holds the engineering intent, design, geometry and the bill of materials.
  • MES (like Opcenter) is the heartbeat – it captures manufacturing processes and real-time equipment status.
  • ERP is the nervous system – supply chains, financials, cost and procurement.

These three systems are the golden triangle of any modern enterprise. And they are almost entirely disconnected from each other.

The same physical component is called a part in PLM, a material in ERP and a component in MES. Three systems. Three vocabularies. Three isolated lenses on the same object.

manufacturing plant floot

Context is not a nice-to-have

There’s a statistical concept that illustrates the danger of missing context perfectly. If you have one leg in water at 100 degrees and the other in water at 0 degrees, you are – on average – perfectly comfortable. But you are not fine.

Context is what separates a statistic from a truth.

Enterprise AI without context is the same problem at scale. You can have the most sophisticated large language model, the most capable AI agents and the most modern data platform – and still make catastrophically wrong decisions, because the context those systems are reasoning over is incomplete, siloed or stale.

The answer isn’t better AI. The answer is better context.

What is Intelligence Center X?

Intelligence Center X is Siemens’ answer to the context problem – and it’s built on four integrated capabilities:

  • The knowledge graph and industrial ontologies – the data layer that connects every enterprise system into a single, semantically coherent view. Not by moving data, but by creating a shared understanding of what data means and how it relates. Rapidminer Graph Studio, the enterprise knowledge graph solution at the heart of Intelligence Center X, handles hundreds of billions of data relationships and scales horizontally as your enterprise grows.
  • Machine learning and AI modeling – the tools to build precise, domain-grounded predictive and prescriptive models on top of that context. Not generic AI, but AI that understands your manufacturing logic, your engineering data and your quality history. Rapidminer AI Studio brings those models to life – giving data scientists and domain experts a shared environment to build, govern and deploy AI that’s grounded in your actual operations.
  • Agentic application development – low-code, no-code tools (powered by Mendix) to build, deploy and orchestrate AI agents and intelligent applications. Agents can act across systems, not just within them.
  • Unified governance – a platform-wide trust layer that ensures every agent decision, every model inference and every data access is traceable, auditable and aligned with your enterprise security and sovereignty requirements. Your data stays yours.

The insight that makes this different: these four capabilities only work when they work together. A data platform without context produces siloed AI. AI without governance produces invisible risk. Agents without orchestration produce chaos. Intelligence Center X is the architecture that connects them.

The autonomous enterprise is not a destination – it’s a direction

Nobody becomes an autonomous enterprise overnight. The journey starts with connecting data, building context and enabling the first cross-domain questions that no single system could answer before.

But the direction matters. And the foundation matters even more.

The enterprises that will lead their industries in the next decade are not the ones that ran the most AI pilots. They are the ones that built the context layer – the shared, governed, semantically rich understanding of how their enterprise actually works – and then let AI agents’ reason over it.

Intelligence Center X is that foundation.

The brain doesn’t have to stay in the jar.

Key takeaways

Enterprise AI is underperforming not because the technology is wrong, but because the context is missing.

PLM, ERP and MES – the golden triangle of the modern enterprise – are almost entirely disconnected from each other.

AI agents that reason over siloed, incomplete data inherit those blind spots and make decisions without the full picture.

Context is not a nice-to-have. It is the foundation that separates a statistic from a truth.

Intelligence Center X brings together a knowledge graph, AI modeling, agentic application development and unified governance into a single integrated solution.

The enterprises that will lead the next decade are the ones building the context layer now.

Intelligence Center X was announced at Realize Live 2026 by Siemens Digital Industries Software. It brings together Rapidminer Graph Studio (enterprise knowledge graph), Rapidminer AI Studio (ML modeling) and Mendix (agentic application development and orchestration) into a unified solution for the autonomous enterprise.

Abbie Wise

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/rapidminer/the-brain-in-a-jar-problem-why-ai-without-context-is-failing-the-enterprise/