Products

Vectorworks and Siemens: a shared vision to deliver continuous innovation

By SilviaP

Vectorworks has a proven track record of redefining what’s possible in the AEC and BIM software industry.

With an exceptional portfolio of products for architecture, interiors, landscape and entertainment, it allows designers to unleash their creativity and push technological boundaries.

Unlike other BIM software, Vectorworks stands out with its advanced 3D modeling capabilities, making it one of the most versatile solutions on the market and enabling users to seamlessly transition from initial concept and exploration to final design and construction documentation, all within a single platform.

This “limitless” approach to design is realized through fast, sophisticated yet intuitive workflows, while ensuring the highest quality of the data produced.

To navigate the complexity of creating pioneering solutions, Vectorworks has established a long and fruitful partnership with Siemens, integrating the Parasolid and D-Cubed 2D DCM toolkits across their whole product line.

Courtesy of Vectorworks

Elevating 3D modeling workflows for AEC with Parasolid

The integration of Parasolid came at a time when customers in the AEC software industry were increasingly adopting 3D modeling into their workflows. To remain competitive and meet evolving customer demands, it was essential for Vectorworks to offer robust, intuitive, and high-performance 3D modeling capabilities.

The company’s strategic vision was to leverage the technological expertise accrued by Parasolid in decades as the best-in-class modeling kernel for the parametric CAD and CAM industry to drive innovation and differentiation in the AEC industry.

Vectorworks features a hybrid drawing environment that enables fluid transitions between 2D and 3D modeling and back again.

Courtesy of Vectorworks

Boosting performance for 3D modeling in a hybrid 2D/3D environment has been and continues to be a top priority for Vectorworks. Before the integration of Parasolid, the team sought optimizations to enhance user capabilities, especially when dealing with complex geometries such as concave polygons and discontinuities.

The primary objective was to enhance 3D modeling workflows while reinforcing the precision and efficiency of the 2D drafting capabilities.

To achieve this, rather than undertaking a costly in-house revamp of their solid modelling engine, they decided to rely on a proven, industry-standard solution.

Parasolid was the best choice.

Its integration significantly accelerated the development of advanced 3D modeling features, to the point where most of the sophisticated 3D capabilities available today were introduced following its adoption.

Some examples

  • History-based modeling – History-based modeling in Vectorworks, an essential feature for many of its users, is powered by Parasolid. Users can easily modify previous design actions in their 3D models while automatically updating all dependent elements. Changes propagate throughout the model and assemblies without requiring manual rework, saving a significant amount of time.
  • Offset edge –  Parasolid’s edge offset on body and direct modeling functionalities allowed Vectorworks to implement edge offsetting on faces, extrusion and thickening, resulting in quick and direct modelling workflows for their customers.
  • Wall Closure: In architecture, wall closure defines how walls and inserts interact at openings. This includes defining the layers of a composite wall around an opening or how profiles, offsets, and wrappings interact. Generating accurate 2D and 3D geometries to represent wall closures is complex due to interactions with doors, windows, and other elements.
    Vectorworks developed a solution to generate the 3D geometry for wall closures, leveraging Parasolid’s functions like offsetting, trimming, thickening, extrusion along a path, and lofting. The 2D geometry at the cut plane is also created using Parasolid’s Boolean operations. This has made Vectorworks’ wall closure feature one of the most advanced in the industry.

Achieving the high precision and detailed geometries expected by our users would have been a monumental challenge without Parasolid.

Darick DeHart, Vectorworks Chief Product Officer

Vectorworks also takes advantage of the Parasolid translator toolkit for IGES interoperability, being able to import and export massive AEC models across different applications through the IGES format.

Bulletproof parametric design for BIM with D-Cubed

With the integration of D-Cubed, Vectorworks was determined to position itself as a leader in the BIM software industry.

Supporting the full lifecycle of a building, from design through construction to facility management, requires long-term data persistence and highly performant parametric modelling, where large, constraint-heavy models can react dynamically to changes with precision and speed.

Before integrating D-Cubed 2D DCM, Vectorworks recognized the need to improve its design workflows. The complex constraint networks posed a challenge, but this led to a commitment to enhancing the user experience.

To build such robust, advanced constraint-solving engine from scratch would have inevitably increased risk and time-to-market, weakening Vectorworks competitive edge.

Instead, the company decided to build atop the leading constraint solver in the CAD industry, D-Cubed 2D DCM from Siemens.

Courtesy of Vectorworks

The integration of D-Cubed 2D DCM has enabled Vectorworks to introduce a suite of features that leverage geometric constraints to efficiently solve complex 2D parametric modeling challenges.

D-Cubed 2D DCM ended up being integrated into areas of functionality that would have never been thought possible with Vectorworks’ previous parametric engine. This allowed them to innovate in a way that was not anticipated.

The stability of the 2D DCM algorithms, its ability to consistently provide a valid solution for geometry positioning given any applied constraint scheme, while offering the application information on any problematic area of the model, makes it very easy to experiment with.

Regardless of the initial integration plan, we decided to use D-Cubed 2D DCM to solve as many technical challenges as possible.

Darick DeHart, Vectorworks Chief Product Officer

Some examples

  • Graphic legends – The software’s graphic legend tool needed to generate dynamic annotated legends in grid-like layouts that could be fully customizable while maintaining defined spacing between elements.
    Using D-Cubed 2D DCM, Vectorworks was able to design an optimal solution to handle all geometric adjustments, ensuring that when the legend changes, the related elements are automatically repositioned to maintain predefined spacing and dimensional constraints.
  • Debugging tools – When Vectorworks was developing its wall connection feature, they also made extensive use of D-Cubed’s debugging capabilities.
    2D DCM – and all other D-Cubed components – allows the outputting of the model’s data structure at any point during the modelling session, isolated from the application’s data. This gives a direct, concise insight into how the application’s implementation of a feature is represented within the component, making it much easier to identify potential flaws.
    The D-Cubed deliverables include a simple graphical user interface to test the component’s APIs and it can load the model data output, helping to detect and rectify issues in the geometry or constraint scheme construction.
    This set of debugging features significantly contributed to streamlining Vectorworks development workflows.

Keys to success

The shared commitment to deliver continuous innovation is key to the success of Vectorworks’ partnership with Siemens.

By leveraging Parasolid and D-Cubed 2D DCM, Vectorworks has significantly reduced the complexity of handling advanced geometry creation, mathematical relationships, and low-level editing operations, allowing PLM Components technologies to do the heavy lifting.

This has not only improved efficiency but also unlocked new possibilities for innovation – enabling to explore design concepts that would have previously been impractical.

As a result, Vectorworks development and innovation cycles have accelerated, allowing the product development team to deliver more advanced and powerful solutions to users, faster.

Continuous support

Parasolid and D-Cubed are developed and maintained in Siemens’ UK Cambridge offices.

The technical support and development teams work side-by-side from this centralized location, to provide the quickest and most comprehensive feedback to customers, assisting them during evaluation, integration and post-integration phases.

Before the integration of PLM Components, Vectorworks was using a different geometry kernel and parametric solver.

Like with any new technology, transitioning to the new components involved a learning curve, but the Siemens PLM Components teams provided extensive support and training during the process. Vectorworks was also pleased to discover a wealth of documentation available, including tutorials and learning exercises, which greatly helped their engineering teams.

Courtesy of Vectorworks

Looking ahead

Vectorworks’ Public Roadmap includes more parametric modeling features based on D-Cubed 2D DCM, expanding their usage of the component.

Learn more

If you’d like to know more about Vectorworks, visit their website https://www.vectorworks.net, LinkedIn page https://www.linkedin.com/company/vectorworks-inc/ and Youtube channel https://www.youtube.com/vectorworks.  Stay up-to-date on social media by following @Vectorworks on Instagram, Facebook and X.

To know more about Parasolid and D-Cubed, visit the product pages Parasolid 3D Geometric Modeling | Siemens Software and D-Cubed | Siemens Software or request a free 60 days trial at Request your free 60-day evaluation of Parasolid | Siemens Software and Request your free 60-day evaluation of D-Cubed Components | Siemens Software .

Parasolid and D-Cubed are part of the Siemens PLM Components portfolio, a set of advanced, industry-proven Software Development Kits integrated by 3D applications in product design, simulation and manufacturing. To know more, visit PLM Components | Siemens Software.

If you are developing next-generation software for 3D product design, simulation or manufacturing, join us in Cambridge, UK, on April 28-29, 2026, for the fourth PLM Components Innovation Conference. This is a unique opportunity to understand the value of PLM Components and joining Siemens’ open software vendor ecosystem.

To know more and register for the free event, visit PLM Components Innovation Conference 2026 | Siemens Software.

Silvia Peruch
This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/plm-components/vectorworks-and-siemens-a-shared-vision-to-deliver-continuous-innovation/