Products
How to create VoluMill roughing patterns with NX CAM
Celeritive's VoluMill pattern is a patented approach to high speed roughing that is well-suited to hard materials. See how easy it is to use the VoluMill plug-in for NX CAM and create these ...
Celeritive’s VoluMill pattern is a patented approach to high speed roughing that is well-suited to hard materials. See how easy it is to use the VoluMill plug-in for NX CAM and create these roughing patterns right in the NX CAM environment. The operations are selected, modified, and displayed the same way as any other NX operation. They sequence themselves associatively in the Operation Navigator, too.
Check out the Tech Tip replay and see how easy it is to plug these patterns in to NX CAM: