Aerion Supersonic: The world’s first environmentally responsible supersonic aircraft

Aerion’s AS2 is the first-ever privately built supersonic commercial aircraft. Designed to be inherently environmentally responsible, the AS2 is the first supersonic aircraft with the ability to accept 100 percent synthetic fuel. It is also the first to be designed without an afterburner. Using Siemens’ Xcelerator portfolio, Aerion can use advanced design and simulation software to speed aircraft development, as well as achieve superior levels of performance in flight and excellence in operations.

Next Generation Design for the Automotive Industry

Join us on Thursday, Sep 10, 2020 from 8:00 AM – 9:00 AM EDT for a detailed take on the…

Next Generation Design for Heavy Equipment

Join us on September 11th at 12:30 U.S. EDT as industry experts detail the next generation of design for the…

Freeform Modeling Walk-through

Sam Kuan of Product Engineering Software is back at it again with a voice over demonstration of freeform modeling in…

Synchronous Modeling Walk-through

Video Walkthrough using Siemens NX to edit current design or translated data (with no features), or migrated CAD data

NX Join

NX’s continuous release model allows cutting-edge CAD tools to be instantly added to NX users’ tool-kits as soon as the…

Cloud Connected Products: Core, Advanced and Drafting

During times of increased demand, being able to scale up your company’s resources and production is critical. Companies can quickly…

Structure Designer Walk-through

See here for a demonstration on the all new Structure Designer with NX

Cloud Connected Products: Drafting & Layout

Drafting and Layout on the Cloud. See what you can do with NX Cloud Connected Products