Corporate
Femap Tips & Tricks: Coincident Node Move Only Option
Sometimes you may need to set up a model to have a set of coincident nodes which can be connected together using spring or gap elements. To help prepare such a model, Femap includes a method of movin...
Sometimes you may need to set up a model to have a set of coincident nodes which can be connected together using spring or gap elements. To help prepare such a model, Femap includes a method of moving nodes to be coincident within a tolerance. See how you can use Femap’s Move Only, No Merge option of the Check Coincident Node capability to achieve this.
Alastair
Follow Femap on facebook and the Femap group on LInkedin