Thought Leadership

Instrumentation

Embedded software development tools are important to all developers and a topic that I frequently discuss [like here]. The way such tools are described by vendors is interesting. For example, there might be a reference to an “optimizing compiler”. That is rather meaningless, as all compilers are optimizing to at least some degree. For an embedded compiler, the important factors are the quality of optimization and, more importantly, the degree of control that the user can apply.

Another interesting terminological issue is applied to debuggers and trace tools. They are commonly referred to as “non-intrusive” …

Most people will have heard of Heisenberg’s Uncertainty Principle. Although it has a precise meaning in the realm of quantum physics [which is well beyond the scope of this blog!], it does highlight a basic rule of life: you cannot measure something without affecting the thing that you are trying to measure; i.e. the act of measurement affects the result. This applies in a surprising diverse range of circumstances and has useful side benefits.

If you are an electronics designer, you may need to measure a voltage in a circuit. That measurement drains a [very tiny] current, which affects the voltage. If you measure a current, a resistance is introduced, which affects the current. To look at timings and waveforms, an oscilloscope is the standard tool. The application of the ‘scope probes, affects the capacitance of the circuit, which, in turn, may modify the timing behavior. Does all this matter? Normally, no, because the effects are so tiny that they may be ignored. Sometimes, however, the effect [of tiny timing changes] may cause the circuit to malfunction. Such a fault can be hard to track down, but it does indicate that the design is rather marginal and some work to make it more robust would be advisable.

Surprisingly, the rule applies to software as well. A debugger may use a hardware probe, which has a small effect upon the timing of the code. There may be a debug agent to facilitate “run mode” debug or extra OS instrumentation to enable profiling. Both of these affect the size of the code and, more importantly, its real time behavior. Just like with the hardware design, the effects are likely to be tiny. However, any problems that do arise simply serve to highlight poor [i.e. fragile] design.

On a future occasion maybe I will look at more parallels from nuclear physics, which teach useful principles. Maybe we can discuss the half life of executing software …

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2011/08/22/instrumentation/