Thought Leadership

Simple real-time task scheduling – a question and an answer

I recently received an email, from somebody with whom I was not acquainted, with the subject line “Probably a silly question”. This got my attention, as I think the only silly thing about a question is not asking it. It certainly was not a silly question. The emailer was asking about implementation of a real time system and I gave him some advice, which I hope was helpful.

With his permission, I will share the question and my answer …

As the question was about implementing a real time system, my default response would be advice about using an RTOS. Although, in this case, it might have been a valid response, it is probably not the best answer. Here is what he asked:

I am using a bare metal app with a super loop. Using polling inside for 3 tasks at different time periods. So am I better off using a simple for loop or using the timer module present in the Atmel SAM D20 Arm M0+ microcontroller ?

100usec – action A
1msec – action B
10msec – action C

Obviously, a for loop/delay is the easiest way but it keeps the processor working and it may not be easy to put the microcontroller to sleep to conserve power. So I am taking a look at implementing it using timers. Please let me know if I am doing it wrong ?!

The nature of the three actions is unimportant. Suffice it to say that they are small amounts of processing that needs to be performed at regular intervals.

It would be quite possible to use an RTOS. Each action would be coded as a task something like this:

void task_A()
{
 action_A();
 RTOS_delay(100);
}

void task_B()
{
 action_B();
 RTOS_delay(1000);
}

void task_C()
{
 action_C();
 RTOS_delay(10000);
}

If the application was the starting point for something bigger – i.e. much more functionality/complexity might be added later – utilizing an RTOS may be an excellent idea. This is because an RTOS supports a multi-threaded structure which is very scaleable, so adding new functionality is less likely to adversely affect existing code. Of course, I feel honor bound to recommend our own Nucleus RTOS, which is ideal for such an application.

However, in this case, I had the impression that the project was bounded and I suggested setting up a 100usec timer interrupt and coding the ISR thus:

interrupt void timer_ISR()
{
 static int timer_B = 0;
 static int timer_C = 0;

 action_A();

 if (timer_B-- == 0)
 {
  action_B();
  timer_B = 10;
 }

 if (timer_C-- == 0)
 {
  action_C();
  timer_C = 100;
 }
}

Any other suggestions on how to address this problem? Please comment, email or contact me via social media.

I am also very open to queries such as this, so please feel free to ask.

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2016/05/23/simple-task-scheduling-a-question-and-an-answer/