Products

S-parameters are for more than just packages

In the digital design world, we have typically only seen S-parameters used to model packages.  They are a popular output of 3D field solvers like IE3D.  But more and more, especially in SERDES design, we are seeing S-parameters being used for a variety of parts.  One of the reasons for their growing popularity is their fater simulation time, especially when advanced simulation techniques are used, as in the case of Mentor’s complex-pole fitting in HyperLynx and ELDO.

S-parameters are also used to model connectors, and even entire interconnects.  In fact, it is often a good idea to extract an S-parameter for your entire interconnect, including any packages and connectors.  This allows you to view the interconnect as one S-parameter, and look at data like the total loss across the interconnect.  Many industry standard SERDES busses like PCI Express and Serial ATA specify a maximum total insertion loss through an interconnect.  As such, comparing your total insertion loss from the channel S-parameter to that loss spec gives you an excellent indication of the performance of your link without having to run a long simulation.  Of course, to really see the benefits of things like pre-emphasis and equalization to overcome channel losses, you should run some kind of time-domain simulation with your buffer models.  FastEye in HyperLynx can really speed that up.

For more information on recent developments in SERDES simulation, take a peek at my recent article in PCD&F:
http://pcdandf.com/cms/component/content/article/171-current-issue/7704-designers-notebook

Patrick Carrier
This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/electronic-systems-design/2011/01/14/s-parameters-are-for-more-than-just-packages/