Products

When design meets manufacturing: Why the digital thread and digital twin are leadership imperatives

The relationship between design and manufacturing is not just an operational handoff—it is a strategic determinant of whether innovation becomes market leadership or a costly bottleneck. This connection directly affects profitability, speed to market, product quality, and an organization’s ability to compete in an increasingly complex and fast-moving landscape.

At the center of this relationship is the concept of the digital thread. In its ideal form, it represents a seamless, bidirectional flow of trusted information across the entire product lifecycle—from concept and design through production and beyond. Through the digital thread, design teams operate with real-time insight into manufacturing cost, capacity, and constraints, while manufacturing continuously feeds performance data and improvement opportunities back into future designs.

Crucially, the digital thread is also what enables the digital twin—a complete, authoritative digital representation of the product that is used consistently across design, manufacturing, and lifecycle operations. When executed correctly, the digital thread ensures that the digital twin created in design is not reinterpreted, reconstructed, or approximated downstream, but faithfully consumed and extended by manufacturing.

This vision is not merely technical. It is a blueprint for operational discipline, financial control, and sustained competitive advantage. Yet for many organizations, it remains out of reach. Rather than a connected lifecycle, enterprises often operate within a patchwork of disconnected tools, file formats, and manual handoffs—forcing manufacturing to recreate its own version of the product digital twin, with predictable consequences.

The tangled web: How value is lost when the digital thread—and digital twin—break down

From a leadership perspective, fragmented information flow creates systemic risk—often invisible until it impacts revenue, schedules, or customers. When the digital thread breaks, the digital twin fractures as well.

1. Email and shared drives: Eroding trust and forcing digital twin rework

Email attachments and shared folders are still widely used to exchange design files, BOMs, and change notices.

The management challenge:
There is no authoritative source of truth. Manufacturing teams frequently receive incomplete or ambiguous data, forcing them to reconstruct the product model needed for fabrication, assembly, and test. This reconstruction becomes an unofficial—and unmanaged—digital twin.

The business impact:
Rework, scrap, missed deadlines, and slower responses to market changes. Even worse, manufacturers may make well-intentioned optimizations to improve manufacturability, unknowingly compromising system-level performance, reliability, or compliance.

2. Spreadsheet dependency: Fragmented data, fragmented twins

Spreadsheets persist because they are familiar and adaptable. From a leadership standpoint, however, they introduce unmanaged risk.

The management challenge:
Disconnected spreadsheets create inconsistent views of product structure, cost, and configuration. These inconsistencies propagate into manufacturing models that no longer align with design intent.

The business impact:
Budget overruns, inaccurate product costing, inefficient inventory decisions, and digital twins that diverge from the engineered system—leading to surprises late in production or, worse, in the field.

3. Sequential handoffs: When manufacturing must rebuild what already exists

The traditional “throw it over the wall” approach—where design is completed before manufacturing engagement—remains deeply ingrained.

The management challenge:
Manufacturing receives design outputs that lack the full context required for execution. Without a complete, consumable product model, manufacturing teams must rebuild geometry, stackups, net intent, and constraints to create a usable digital twin.

The business impact:
Late-stage redesigns, longer lead times, higher production costs, and lost performance fidelity. Valuable manufacturing expertise is applied reactively instead of proactively, and continuous improvement stalls.

4. Version control failures: Multiple twins, no authority

Without centralized lifecycle management, multiple versions of designs and process plans coexist across systems and teams.

The management challenge:
Leaders cannot confidently answer which version of the digital twin is approved, released, or currently being built. Changes made in manufacturing may never reconcile with engineering’s intent.

The business impact:
Quality escapes, warranty claims, recalls, regulatory exposure, and slow, error-prone engineering change processes. The digital twin becomes fragmented, weakening governance and traceability.

5. Lost manufacturing feedback: A Static twin in a dynamic world

Manufacturing generates critical insight every day—about yield, variability, cost drivers, and improvement opportunities.

The management challenge:
Without a closed-loop digital thread, this insight never updates the authoritative digital twin. The product model stagnates while reality evolves.

The business impact:
Repeated design inefficiencies, slower learning cycles, missed sustainability gains, and declining innovation velocity across product generations.

The role of complete product models in preserving the digital twin

A resilient digital thread depends on delivering a complete, manufacturing-ready product model—not just files, but intent.

Standards such as ODB++ and IPC-2581 enable the transfer of a comprehensive digital product definition, including layout, materials, stackups, net connectivity, constraints, and manufacturing intent. When these formats are used effectively:

  • Manufacturing no longer needs to reconstruct the digital twin
  • Time is saved and errors are reduced
  • Design intent is preserved through fabrication and assembly
  • Manufacturability improvements occur collaboratively, not unilaterally
  • System performance is protected while production efficiency improves

From a leadership perspective, this is risk elimination—not optimization. It prevents downstream changes that improve manufacturability at the expense of electrical, thermal, or reliability performance.

The true cost of a broken digital thread and fragmented digital twins

When design and manufacturing operate without a cohesive digital backbone, the consequences ripple across the enterprise:

  • Financial erosion: Rework, scrap, expediting, and extended cycles depress margins
  • Market lag: Delayed launches reduce revenue potential and market share
  • Brand risk: Quality issues damage customer trust and reputation
  • Innovation stagnation: Teams manage data instead of improving products
  • Talent attrition: Persistent friction and rework erode morale and retention

These are not engineering problems—they are leadership outcomes.

Moving forward: Turning the digital thread and digital twin into competitive advantage

The promise of the digital thread is not limited to better tools—it is better decision-making at scale. Organizations that succeed treat both the digital thread and the digital twin as strategic assets that align design intent, manufacturing reality, and business objectives in real time.

By addressing where information flow breaks down today, leaders can:

  • Establish a single, trusted digital twin across the lifecycle
  • Deliver complete product models that manufacturing can consume directly
  • Enable earlier, data-driven collaboration
  • Reduce execution risk while accelerating innovation
  • Convert operational insight into lasting competitive advantage

In a market defined by speed, complexity, and margin pressure, a resilient digital thread—and a preserved digital twin—are no longer optional. They are foundational to how modern enterprises lead, compete, and grow.

Stephen V. Chavez
Sr. Product Marketing Manager

Stephen Chavez is a veteran PCB designer who has used Siemens EDA tools for more than twenty years. As Senior Product Marketing Manager at Siemens, his role expands into thought leadership for supply chain resilience and electronic systems design.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/electronic-systems-design/2025/12/22/when-design-meets-manufacturing-why-the-digital-thread-and-digital-twin-are-leadership-imperatives/