Thought Leadership

The hidden mechanics of cloud waste: How to eliminate idle infrastructure

Worldwide IT spending is projected to reach $6.08 trillion in 2026, a 9.8% increase from 2025, in large part due to cloud spending. As budgets climb, so does scrutiny. Cost has now outranked security as the top organizational challenge regarding the cloud for four consecutive years, cited by 85% of organizations, with security close behind at 82% and software license management at 78%. 

Most conversations about cloud waste stop at the headline stat: billions lost, budgets blown. What they skip is the mechanism. Waste is not usually the result of ambitious scaling or runaway AI experiments. It is the byproduct of unmanaged infrastructure: a test VM nobody terminated, a staging database left running after deployment, an IP address with nothing attached to it. Nothing breaks. No alarms fire. The bill just keeps growing. 

This piece looks past the top-line numbers to the actual anatomy of cloud waste: how it accumulates, why it persists and what it takes to reduce cloud spending through context-aware scheduling across hybrid environments. In short, cloud cost management starts with intelligent orchestration

The most common causes of silent cloud waste 

Idle infrastructure rarely announces itself. It survives because it remains under the radar: a resource that runs quietly, causes no incidents and triggers no alerts. Two patterns account for most of it. 

Orphaned nodes are assets still provisioned in a cloud environment but no longer attached to any active process, application or instance. A virtual machine spun up for a one-off test. A storage volume left behind after its parent instance was terminated. An IP address with nothing pointing to it. Each one keeps billing long after its purpose has expired. 

Zombie resources are a related but distinct problem: infrastructure that is technically active but functionally unnecessary. A staging database still running after deployment. An autoscaling group configured well beyond real demand. These resources pass every health check, but they just serve no genuine business purpose. 

Five conditions let this drift become permanent: 

  • Lack of structured tagging discipline 
  • No clear ownership accountability for cloud assets or cloud cost management 
  • Infrequent infrastructure audits 
  • Rapid deployment cycles without built-in cleanup policies 
  • Fear of decommissioning something that might be needed later 

Enterprises tend to equate “running without issue” with “necessary.” Without a structured review process, that assumption goes unchallenged, idle infrastructure becomes normalized and the drift compounds month over month into significant, silent cloud spend. To reduce cloud spending, it must first be identified and stopped with HPC solutions.

Hybrid cloud management

Beyond mismanaged resources, waste also comes from mismatched workload placement. Not every job belongs on cloud infrastructure, and running the wrong ones there is expensive. 

CPU-bound jobs are a common example. These workloads do not need the elastic, GPU-dense capacity that cloud nodes are priced for, yet they often land there anyway by default, simply because on-prem capacity was not on hand or was not the path of least resistance for the team submitting the job. The result is standard compute jobs billed at premium cloud rates. 

Autoscaling adds another layer of friction. Groups configured for peak-case demand, then left unadjusted, scale infrastructure well past what actual workloads require. Unlike orphaned or zombie resources, this waste is scaling with the environment. It looks like healthy elasticity on a dashboard. It is actually excess capacity, provisioned continuously and billed continuously. 

Underneath both problems is the same organizational habit: decommissioning and rightsizing are treated as optional cleanup steps rather than as ongoing discipline. The “fear of decommissioning” (the concern that a resource might be needed later) keeps unnecessary infrastructure alive by default. Over time, this normalizes idle capacity as a fixed cost of doing business rather than a controllable variable.

Solving cloud waste with Siemens HPCWorks and cloud cost optimization tools 

Reducing cloud spending is not simply a matter of using less computing resources. It requires context-aware scheduling that treats on-prem and cloud resources as a single, intelligently managed estate across global operations. This is the core function of Siemens HPCWorks

Dynamic workload placement. HPCWorks routes baseline jobs to on-prem hardware first and spills to the cloud only during true demand spikes. Instead of defaulting expensive cloud nodes for standard, CPU-bound work, orchestration logic matches each job to the resource actually suited for it. 

Agentic AI for resource estimation. An AI assistant estimates job resource requirements up front, reducing wait times and improving scheduling accuracy. In practice, this has driven 10 to 15% gains in job throughput. 

End-to-end HPC and cloud coverage. HPCWorks is built as a complete platform addressing every dimension of HPC, across industries, rather than a point solution for one piece of the pipeline. 

Comprehensive visibility and reporting. Intuitive HPC and cloud reporting gives teams full cluster visibility, supporting informed decisions instead of reactive firefighting. 

Prioritization and controlled scaling. Critical workloads get priority. Cloud resources scale on demand, dynamically, with detailed visibility into what is being spent and why. 

Collaboration across distributed teams. Researchers and engineers get a consistent interface to collaborate remotely, perform remote visualization and submit or monitor jobs across clusters, clouds and other resources. 

Workflow and parallelism analysis. Complex flows can be visualized and analyzed to identify inherent parallelism, optimizing how compute resources are allocated across applications, such as semiconductor design and software development. 

Enterprise-wide budget management. Budgets are managed across on-prem, cloud and multiple clusters from one place, keeping cloud spend visible and allowing software license allocation to adjust based on actual demand. 

GPU acceleration for AI workloads. HPCWorks supports today’s largest AI workloads with GPU acceleration, Jupyter Notebook integration and dynamic cloud scaling, including extensive support for containerized GPU workloads and topology-aware scheduling across HPC, AI and analytics use cases. 

Together, these capabilities replace guesswork with visibility, and reactive cleanup with proactive, automated orchestration. 

Zero waste is an operating model 

Zero-waste is not a spending target. It is an operating model. Orphaned nodes and zombie resources accumulate because infrastructure decisions are made in isolation, without visibility into what already exists or what a workload actually requires. Fixing that requires more than periodic audits. It requires a system that routes work intelligently, scales precisely and makes cost visible at every step. 

Siemens HPCWorks provides that system: dynamic workload placement, AI-driven resource estimation and enterprise-wide visibility across the entire hybrid estate. The outcome is not less compute, but compute that is never idle and never invisible. 

Click here to learn more about how Siemens HPCWorks can help reduce cloud waste and manage growing IT complexity.

Frequently asked questions 

  1. What is cloud waste and how does it occur? 
    Cloud waste occurs when provisioned infrastructure remains active but unused, such as orphaned VMs, zombie databases or over-scaled autoscaling groups. These resources continue billing without serving business purposes. 
  1. What’s the difference between orphaned nodes and zombie resources? 
    Orphaned nodes are assets no longer attached to any active process (like a test VM never terminated). Zombie resources are technically active but functionally unnecessary (like a staging database still running post-deployment). 
  1. How can hybrid cloud management reduce cloud costs? 
    Context-aware scheduling routes baseline jobs to on-prem hardware first, reserving cloud resources for true demand spikes. This prevents expensive cloud billing for standard CPU-bound workloads. 
  1. What role does AI play in cloud cost optimization? 
    AI-driven resource estimation predicts job requirements upfront, improving scheduling accuracy and reducing waste from over-provisioned resources—delivering 10-15% throughput gains. 
Ian Mark

Ian Mark is a primary writer at Siemens Digital Industries Software, where he writes about how industrial companies can accelerate Digital Transformation.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/thought-leadership/the-hidden-mechanics-of-cloud-waste-how-to-eliminate-idle-infrastructure/