Products

Beyond Automation: The Era of Agile, Adaptive and Autonomous Production 

The manufacturing world is undergoing a tectonic shift. We are moving past the era of “static automation,” where machines simply follow pre-programmed instructions, into a future defined by Autonomous Production. 

True factory autonomy isn’t just about faster robots; it’s about a “System of Systems” capable of independent sensing, planning, and action. 

Meet Siemens digital manufacturing experts & authors

The six levels of factory autonomy 

To understand this journey, we can look at a maturity framework inspired by the SAE (Society of Automotive Engineers) levels for autonomous vehicles. 

  • Level 0: Manual – Humans execute all tasks with manual tools. 
  • Level 1: Assisted – CNC machines execute specific programs. 
  • Level 2: Automated – Machines handle continuous activity, but humans monitor and handle all exceptions. 
  • Level 3: Predictive – AI handles maintenance and minor exceptions. A fallback operator is “disengaged but ready.” 
  • Level 4: Autonomous – The factory plans and programs itself. Humans focus on whole-system optimization. The Automation systems use AI to re-program themselves whenever a new task or a new job arrives to be processed. 
  • Level 5: Manufacturing as a Service – The factory self-optimizes, learns, and manages its own ecosystem. The human acts as an Orchestrator. 

Crossing the “trust chasm” 

The most critical leap occurs between Level 3 and Level 4. This is the Trust Chasm. 

At Level 3, we still rely on a human safety net. At Level 4, we shift the decision-making authority to the system itself. While Level 3 is where most industry leaders sit today, reaching Level 5 is a marathon, not a sprint. It requires a fundamental shift in how we view the relationship between man and machine. 

The engine of autonomy: the comprehensive Digital Twin. 

How does a factory “think?” – it uses a Digital Twin that is a comprehensive digital representation of the products, production systems, and processes. This isn’t just a 3D CAD model; it is a live, semantic representation of the physical floor. 

  1. SENSE: The digital twin ingests real-time data (IoT, sensors, SCADA) to understand the current state. 
  2. PLAN: AI agents run “what-if” simulations within the twin to find the optimal path to a goal. 
  3. ACT: The system executes the plan via software-defined robotics and feeds the results back into the twin. 

A growing number of manufacturers are using comprehensive Digital Twins to make critical decisions when building new production facilities or optimizing processes in existing factories. This approach offers them unique advantages, such as defining the most efficient and agile production processes needed to remain competitive. 

The Siemens Xcelerator portfolio, powered by AI capabilities, enables customers to create a comprehensive Digital Twin that covers the entire product lifecycle, from the product itself and its manufacturing processes to the production systems designed to realize these products. 

The Digital Twin in action 

Siemens is a leading manufacturer with a diverse product portfolio and rapidly adopting agile and adaptive production systems. For example, The “Siemens Numerical Control” (SNC) factory, in Nanjing, China uses digital twin technology to deliver outstanding results. Compared to 2022, the facility has improved most of the KPIs, including: 

  • Cutting lead times by 78% 
  • Reduced time-to-market by 33% 
  • Increased productivity by 14% 

Additionally, field failures decreased by 46% and the factory lowered its direct and energy-related carbon emissions by 28%. As a result, our SNC factory in Nanjing was recently recognized as a Lighthouse by the World Economic Forum.

What are the other expected values of agile, adaptable and autonomous factories? 

Operational Efficiency, Strategic Agility, and Human Empowerment. 

The shift from simple automation to a “system of systems” approach allows manufacturers to move from being reactive to being predictive and self-optimizing. 

1. Radical Operational Efficiency 

The primary value of an autonomous factory is its ability to eliminate the traditional bottlenecks that plague manual or semi-automated lines. 

  • Continuous Self-Optimization: By using the Sense-Plan-Act cycle, the system identifies inefficiencies in real-time. It doesn’t just flag a problem; it simulates solutions via the Digital Twin and executes the best path forward. 
  • Predictive Operations: Through Forecasting Agents, the factory can predict machine failures and utilization levels before they occur. This shifts maintenance from a “fix-it-when-it-breaks” model to a proactive, zero-downtime strategy. 
  • Closed-Loop Execution: Because the virtual model always matches the physical reality, the system can handle exceptions automatically, ensuring that production never grinds to a halt due to minor variables. 

2. Strategic Agility & Customization 

Agility in this context refers to the factory’s ability to pivot without the massive re-tooling costs or downtime typically associated with production changes. 

  • Manufacturing as a Service (MaaS): At Level 5 autonomy, the factory operates as a service platform, using digital twins and AI‑driven orchestration to continuously reconfigure production lines, capacity allocation, and partner networks in response to changing market demand, before changes are executed physically  
  • Rapid customization: Software-defined automation and robotics allow for high-mix, low-volume production. The system can “program itself” to handle new product variants, enabling businesses to respond to customer needs in days rather than months. 
  • Virtual commissioning: By validating production lines in a virtual space before physical implementation, companies can launch new products faster and with significantly less risk. 

The “orchestrator” value (human capital) 

One of the most significant values is the elevation of the human worker. By crossing the “Trust Chasm,” the organization unlocks the creative and strategic potential of its staff. 

  • Higher-level governance: Humans are freed from “doing” (manual labor and machine tending) to focus on “governing” (managing business goals and ecosystem health). 
  • Strategic problem solving: Using AI agents, humans can solve “multi-variant optimization problems”, such as minimizing material waste or carbon footprints, that would be too complex for a human to calculate manually. 
  • Safety and collaborative innovation: Digital twins allow for the simulation of human-robot interactions, ensuring a safer work environment while fostering a culture where humans work with technology rather than serving it. 

The bottom line

The transition toward autonomous production is no longer an academic exercise. 
As markets demand faster customization, higher productivity, and consistent quality at scale, manufacturers should increasingly move toward software‑defined automation to accelerate time‑to‑market, reduce cost, and optimize operational effort. 

The question is not whether autonomy is possible, but how quickly can organizations build the trust required to let autonomous systems operate on a scale. 

Zvi Feuer

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/tecnomatix/beyond-automation-the-era-of-agile-adaptive-and-autonomous-production/