Products

New Teamcenter Product Cost Management Capabilities

Cost estimators and other decision makers need accurate information for decision-making and they need this information earlier than ever. To address these needs we continuously improve our solution for Product Cost Management. The new version 8.2 provides enhanced capabilities which supports manufacturers to increase visibility of cost drivers in the early stages of product development, helping them to avoid costly engineering rework downstream before the start of production.

Optimized calculation process by updating existing work plans in Teamcenter product cost management

To avoid a manually executed synchronization by cost engineers, which is very time consuming and error prone, the new version provides a new capability to update BOMs (bill of materials), BOPs (work plans) and BOEs (plant resources such as tools and machines) within Teamcenter product cost management at a glance. These synchronization activities can be automated and cost engineers can focus on value adding activities as calculation, controlling, and analysis of cost drivers.

Improved calculation efficiency through automations in Excel or web service import

The new version provides several enhancements to increase automation during the data import stage which consequently results in efficiency improvements for cost engineers.

Possibility to save calculation results as master data material

Cost calculation can now be saved or “published” as a master data material; and therefore, improve the calculation re-use and automation.

Increased flexibility of calculation engine to support further use cases

OEM’s and suppliers demand more precise and transparent costing to be better prepared for negotiations with customers or suppliers and have a better understanding of underlying cost drivers. As a result, the new version 8.2 includes additional direct material cost types to support a more specific calculation and roll-up of product or commodity costs.

Increased consistency with the improved validation framework

Validation is an important part of Teamcenter product cost management to ensure consistency and avoid errors by showing corresponding warning or an error message. With the improvement of this capability, hard-coded validation was replaced with the possibility to generate custom specific validations.

Custom terminology for more consistency within calculations

Possibility to re-name fields to reflect custom terminology by generating a company or even department specific terminology as a parallel structure to the Teamcenter product cost management terminology.

Consistent and reliable tool cost estimates through advanced feature recognition with NX Feature2Cost

The new module NX Feature2Cost supports OEMs, suppliers and tool makers in the tool costing process. It recognizes important geometrical information like general part dimensions, ribs, undercuts, bends, etc. and drives them into actual cost drivers. In case of analysis, Teamcenter product cost management can start NX, pass a geometry file and wait for the result after further interaction of the user with NX. NX provides two feature recognition modules, NX Feature2Cost Molding and NX Feature2Cost Stamping. These modules are able to automatically analyze the geometry file, provide capabilities to manually modify the feature recognition and corresponding cost drivers and then pass them back to Teamcenter product cost management. Within, there are a crucial input into the actual tool cost calculation which is carried out based on existing capabilities within Teamcenter product cost management.

Emilia Maier
Sr. Product Marketing Manager

Emilia is a Product Marketing expert at Siemens Digital Industries Software, joining in 2013 with over 18 years of expertise in Software Marketing. Her extensive background spans marketing strategy, branding, customer experience management, and IT. As the lead for Product Marketing in Teamcenter's cost, sustainability, and compliance management solutions, Emilia is responsible for defining global marketing strategies and executing go-to-market plans. She consistently delivers first-class customer experiences through innovative technologies and has a strong portfolio of co-created white papers, case studies, and reference materials with customers across major industries like automotive, industrial machinery, and electronics.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/teamcenter/new-teamcenter-product-cost-management-capabilities/