Line balancing: finding the right balance between workload and capacity
Getting a production line to run at the required rate sounds straightforward: divide the work between stations, check the times, adjust where needed.
It rarely stays that simple once the work actually gets moved around.
One operation might need a specific resource. Another has to stay in sequence. A station may have capacity to spare, but not the equipment needed for the job. Move one operation to ease a bottleneck, and suddenly another station has more work to handle.
That’s what makes line balancing complicated. It’s not simply about getting station times as close as possible. The work, resources, sequence and available capacity all have to work together to meet the required production rate.

💡 Line Balancing
Line balancing isn’t just about splitting work evenly across stations. Work, resources, sequence and capacity all have to line up at once.
The line balancing challenge
Balancing a line means deciding what work belongs at each station while staying within the constraints of the process.
The challenge is finding a distribution of work that meets the required production pace while working within the available capacity, resources and process constraints.
For the engineer doing this work, it starts with understanding what has to happen at each station and what that station needs to complete the work.
That information cannot be treated as a snapshot. A change to an operation, resource, sequence or process can affect the balance elsewhere on the line. The engineer needs to see those changes in the context of the manufacturing plan.
That means looking beyond the time assigned to a station and at what’s behind it:
- Tasks and operations: What work needs to be completed at each station?
- Resources: Does the station have the required people, equipment and tooling?
- Sequence: Can operations be moved without disrupting the manufacturing process?
- Constraints: What limits the work that can be assigned to a station?
- Changes: Has a change to the product or manufacturing process affected the current balance?
The point is to understand not just how much time a station has, but whether the work assigned to it can actually be completed there. That means looking at the measures that show where the line has available capacity and where it does not.
Measure what matters
There are plenty of numbers to look at when balancing a line. The trick is knowing which ones actually tell you something useful about the line.
Manufacturing planning teams typically look at:
- Takt time: How much time is available to meet the required production pace?
- Cycle time: How long does the assigned work actually take?
- Workload: How much work is assigned to each station?
- Utilization: How much of the available capacity is being used?
- Capacity: How much room does each station have?
- Bottlenecks: Which stations are limiting the flow of the line?
Taken together, these measures show how the planned work fits across the line and where changes may be needed.
The goal is not to make every station identical. It is to find a practical distribution of work that supports the required production rate.
📌 Key takeaway
No single metric tells the whole story. Takt and cycle time show the pace; workload, utilization and capacity show whether stations can actually keep up; bottlenecks show where the line will break first.
Bringing line balancing into the manufacturing plan with Teamcenter Easy Plan
Line balancing works best when it is based on the same manufacturing data used to define the process. In Teamcenter Easy Plan, the MBOM (manufacturing bill of materials) , BOP (Bill of Process) , BOE (Bill of Equipment), workstations, operations, resources and work instructions are all managed, authored and connected within the same planning environment.
Get to know how Teamcenter Easy Plan helps you balance production lines based on workload and capacity to meet your production targets.
That connection matters when balancing a line. The parts being built, the operations needed to build them, the equipment required to carry them out and the instructions that guide the operator all contribute to how work can be distributed across stations — and all of it stays linked as the plan evolves.
Because everything lives in one environment, a change made anywhere shows up immediately in the line balance, instead of requiring a separate sync step or a re-export to another tool. A swapped resource, a new operation, an updated work instruction — the impact on workload and capacity is visible right away, not discovered downstream on the shop floor.
💎 Teamcenter Easy Plan Value
MBOM, BOP, BOE and work instructions are authored in the same environment as the line balance itself. So, balancing the line and building the rest of the manufacturing plan are never two disconnected steps.
Manufacturing Planning teams can use this information to:
- Compare station workload with takt and cycle time to see where work may exceed available time.
- View workload and utilization across stations to identify where capacity is tight or available.
- Reassign operations between stations and see how the change affects the line balance.
- Drill into the operations behind a workload to understand what is driving an overloaded station.
- Review assigned resources to check whether the people, equipment and tooling needed for an operation are available at the station.
Author and update work instructions alongside the balance, so operators always see the current plan — not a version that’s since changed.
And the balance does not stop when the initial plan is complete. When the manufacturing plan changes, engineers can review the impact on workload, capacity and station balance and make adjustments as needed , keeping production targets in check at every stage, not just at kickoff.
From a balanced plan to a production-ready line
A balanced line is never really “done.” Changes to the product, process, resources or production requirements can shift the balance and require another look.
With Teamcenter Easy Plan, line balancing isn’t a separate exercise bolted onto the manufacturing plan — it’s built on the same connected data used to define the MBOM, BOP, BOE and work instructions. That means every adjustment engineers make to keep the line balanced is grounded in the same source of truth the rest of the plan runs on.
Download the line balancing factsheet to learn more about Teamcenter Easy Plan.