Products

101 Uses of the Control and Shift Keys in Solid Edge – Part 1

When using the Shift and Control keys we tend to be creatures of habit. Often, there are a bunch of objects to be selected and we unknowingly press one of these keys. It could be files and folders in Windows Explorer or simply multiple items in a list box.

Solid Edge takes this to the next level where the Shift and Control keys when used individually and in combination with the mouse bring a large number of powerful features to your fingertips.

Selection in the Pathfinder


 


The foremost is the Pathfinder where the Shift key can be used to pick contiguous features. Click the first part in the list, then hold down the Shift key and select the last part in the list. The Ctrl key can be used similarly for non-sequential multiple features.

A potential use for this could be the Assembly PathFinder where you can use the Ctrl key to pick just a few components and start the Assembly Relationship Manager or A.R.M. which then shows the relationships for just the selected components instead of the entire assembly.

This is no doubt some smart behavior on part of the A.R.M. but using the Shift or Ctrl keys is the key here. No pun intended! The following video demonstrates the process.

It goes without saying, this technique can be used in the Part or Sheetmetal PathFinders as well.

Edge and Face Selection

When selecting edges or faces in a Solid Edge command, you can press the Shift or Ctrl keys to add to or remove from an existing selection, besides changing and restoring views, toggling the modeling mode, selecting multiple regions in synchronous all of which are demonstrated in this video:

TipIcon.png The above video shows that in the synchronous mode, Shift needs to be pressed only once to add the first object after which the add remove mode is ON and more edges/faces can be added to or removed from the current selection without keeping the Shift key pressed.

View Manipulation


 


Scroll wheel press-and-drag rotates the view SSE17.png

Keep the Shift key pressed and press-and-drag the wheel to Pan SSE18.png

Keep the Control key pressed and press-and-drag the wheel to zoom SSE16.png in a much smoother way as opposed to the jerky or incremental zoom with each tick of the scroll wheel.

Keep the Alt key pressed and press-and-drag the wheel to start the Zoom Area SSE19.png command.

Additionally keeping the Control key pressed allows zooming in an area centered around the drag start point.

The differences are illustrated below:

CSSE09.png


Did you know that in Solid Edge you can manipulate views i.e. pan, zoom and rotate all using just the keyboard?


A combination of the arrows keys, the Shift and Control keys makes this possible.

Arrow Keys = View Rotate


Shift + Arrow Keys = View Rotate about another axis


Ctrl + Arrow Keys = Zoom


Ctrl + Shift + Arrow Keys = Pan

The Zoom Fit command behaves differently when used in combination with the Shift and Control Keys.

Fit = Both Background Sheet and Drawing Objects


Shift + Fit = Only Drawing Objects and no concern for the Background Sheet


Ctrl + Fit = Only the Background Sheet

All the above techniques are illustrated in this video:


 


Perspective in a Jiffy

The View Overrides dialog on the View tab of the ribbon allows for a perspective view of the model with only 3 fixed settings, keeping the Ctrl + Shift pressed and scroll the wheel on the mouse to change the perspective of the model allows 12 values. 

CSSE02.png

 


Hip-Tip: Drawing View Power Update

TipIcon.png  If you hold Ctrl+Shift when you click Update Views CSSE10.png Solid Edge performs a full update, just as it would on initial view creation.  That is, it re-reads all of the model data to regenerate the view, rather than only the model data thought to have changed.

Universal Commands

Solid Edge supports all standard keyboard accelerators that use the Control key like:

Ctrl + N for New


Ctrl + O for Open


Ctrl + S for Save


Ctrl + P for Print


Ctrl + Z for Undo


Ctrl + Y for Redo


Ctrl + A for Select All, in Draft and Sketcher

Create New Keyboard Shortcuts

Any keyboard shortcut which is standard in your other favorite program, for example, Ctrl + W for closing a file, and is not supported by Solid Edge can be easily added using the Customize dialog as shown in the video below. The video begins with a handy shortcut Ctrl + Tab to cycle through all open docs and Ctrl + Shift + Tab to reverse the direction:

Standard Views

Sold Edge’s Control+First Letter system is perhaps the simple and the most elegant of all CAD programs for switching to standard views and are listed below:

Ctrl + I for Isometric

Ctrl + T for Top


Ctrl + B for Bottom

Ctrl + R for Right


Ctrl + L for Left

Ctrl + F for Front


Ctrl + K for Back

Ctrl + J for Dimetric


Ctrl + M for Trimetric

CSSE04.png

More Tip and Tricks

Some miscellaneous uses of the Control and shift keys in lesser used commands are:


  1. Keeping the Shift key pressed when drawing a rectangle turns it into a square.
  2. Same with box command, but this does not apply when specifying the height.
  3. When drawing a line, keeping the shift key pressed, increments the angle in steps of 15°
  4. When inspecting the area of closed regions, keeping the Shift key pressed additionally displays the total area.
  5. When applying a Smart Dimension to an inclined line, the Shift key allows toggling between horizontal, vertical and aligned dimensions.

All these techniques can be seen in action in the following video:

Selection Manager

Pressing Shift + Spacebar starts the Selection Manager mode in the synchronous environment. This reveals a menu with over a dozen methods to intelligently select faces and features in imported models.

CSSE06.png

The video below illustrates several methods from the menu above.

LoudSpeaker.png Note: This video has a voice-over.

More tips…


More tricks…


More videos…

For more videos tip about the Shift and Control keys in Solid Edge, go to part 2 of this article…

Tushar Suradkar


www.CADVertex.com


www.SurfAndCode.IN

Solid Edge User Group on FaceBook:


https://www.facebook.com/groups/solidedgeusers/

Tushar Suradkar

Solid Edge blogger, Programmer

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/solidedge/101-uses-of-the-control-and-shift-keys-in-solid-edge-part-1/