Products

Webinar: For accurate PCB quoting, you need more than Excel

Accurate job quoting is key to good business

While EMS companies compete for manufacturing jobs, they need to generate quotes for several jobs – while only winning some of them. Offering a competitive quote is tricky: on one hand, manufacturers want to offer an attractive price. But on the other, they need to take into account all possible costs, material and production costs, in order to make sure that the work isn’t underpriced. And since many factors can change between quotation and order, a thorough “re-calculation” needs to happen exactly when time is at a premium and any delays can affect delivery commitments.

As a rule of thumb, material costs are the lion’s share at around 70%. Production costs account for 30%. Seems simple enough, but what happens if you don’t get production costs right? If the work was underpriced, you’ll run into trust issues with your client as you’re forced to charge a higher sum than originally agreed. If it’s overpriced, it’s likely you won’t get the job at all…

What makes PCB quoting so difficult?

Finding accurate prices for material is a question of finding a good external resource: a database with real-time component prices and availability. But production costing is quite a different matter, relying entirely on internal company knowledge and expertise.

What machines will be used in production? Which line will be used? What is the cost of equipment? What are the labor rates? What are the energy rates, shipping rates? All of these, and more, need to be taken into account when calculating production costs.

Large companies typically have an entire department dedicated to cost calculation, which includes several process experts, a dedicated purchasing group, hardware engineers, and an up-to-date ERP system. But in smaller companies, accurate job quoting will require the input of SMT and THT assembly experts as well as testing engineers. Directing such experts’ time at job quoting, rather than production itself, is disruptive to the manufacturing flow.

An advanced method for accurate PCB quoting

In our on-demand webinar, Kevin Decker-Weiss of CircuitByte and Siemens expert Paul Carpine explore the challenges of accurate PCB quoting, and also explain how the common Excel-based solutions are holding companies back. Watch the webinar to:

  • Find out what’s impeding electronics manufacturers in their PCB assembly quoting process
  • See how other companies have accelerated their quoting process
  • Learn how to make use of existing data sources to speed up the quoting process and make it more accurate.

Paul Carpine also authored the white paper: “How can independent electronics manufacturers compete better for jobs?“, detailing the competitive advantage that accurate PCB quoting provides for smaller companies.

Tova Levy

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/process-preparation/2023/06/28/webinar-for-accurate-pcb-quoting-you-need-more-than-excel/