Products

Accelerate and Scale Early Validation with Polarion

How to Scale Early Validation with Polarion: Requirements Traceability, Approvals, and Simulation Evidence

Scaling Early Validation with Polarion: Improving Traceability, Approvals, and Simulation Evidence
Scaling Early Validation with Polarion: Improving Traceability, Approvals, and Simulation Evidence

Early validation only scales when requirements, tests, approvals, and simulation results stay connected. Polarion is an ALM platform that helps engineering teams manage these connections with end-to-end requirements traceability, governed workflows, and a single place to capture and link validation evidence – including evidence produced by simulation.

In the modern engineering landscape – where the transition toward the Software-Defined Product (SDP) is redefining everything from autonomous vehicles to medical devices and aerospace systems – the cost of discovering defects late is measured in delays, rework, and risk. That’s why teams adopt a rigorous shift-left approach: validate intent earlier and keep evidence traceable as requirements evolve.

The Bridge Between Modeling and Reality

Modern engineering organizations don’t wait for physical prototypes to begin testing. They simulate. They model. They validate in virtual environments – and they do it continuously, at scale, across distributed teams. By orchestrating simulations and test management within a single, unified ALM environment, teams can identify risks before a single physical prototype is ever built.

This is where test management and simulation integration become not just useful tools, but strategic competitive advantages.

But simulation alone is not enough. The results of simulation must be:

  • Captured systematically and traceably
  • Linked to requirements, test cases, and defects
  • Reported in a way that satisfies regulatory auditors
  • Reused across projects to maximize ROI

This is the gap that many ALM tools fail to bridge – and it’s exactly where Polarion excels by orchestrating the whole process.

Early Validation with Polarion Starts with Requirements

Polarion uses LiveDocs as structured, versioned specification documents rather than loose collections of individual items. Requirements are authored directly in these documents, reviewed in context, and versioned automatically. When a requirement changes, Polarion does not rely on manual tracking to understand impact. Instead, traceability links immediately show which downstream artifacts – such as derived requirements, test cases, or risks – are affected.

This matters for early validation because teams can see what must be re‑validated as soon as intent changes. Validation is not postponed until implementation or test execution; it starts at the requirement level, with full visibility into impact and coverage.

Governed process, and auditability built into the tool

Polarion makes governance part of execution. LiveDocs, Collections, controlled workflows, built-in e-signatures, baselines, and automatic change history all work together in one audit-ready system.

  • Governance is built into execution: Polarion uses configurable workflows, granular permissions, and automated process control to make sure requirements, reviews, approvals, and releases follow a defined path – not an informal process held together by emails and spreadsheets.
  • Formal approvals carry real weight: Polarion supports secure electronic signatures compliant with U.S. 21 CFR Part 11, and signatures can be required directly in the document workflow before content moves to the next stage. Approval is part of the process – not a manual afterthought.
  • Auditability is native, not bolted on: Workflow state, signature status, baselines, permissions, and change history are captured inside the system as work happens. You do not need to stop later and reconstruct the audit trail in a separate compliance exercise.
  • Always closer to audit-ready: Because documents, approvals, traceability, and validation evidence live in one governed environment, Polarion supports an audit-ready process by default – especially for organizations that need controlled releases, formal sign-off, and defensible compliance evidence.

Native test management connected to requirements

Polarion includes native test management, not a third‑party add‑on. Test cases, test runs, and results are first‑class artifacts that link directly back to requirements.

This allows teams to:

  • define verification strategy alongside requirements,
  • link test cases as soon as requirements are approved,
  • reuse test assets across releases and variants,
  • see real‑time coverage and validation status.
Document in a Collection, selected specification with traceability links and approvals

Because testing is not disconnected from requirements, teams can validate intent earlier. They can identify missing tests, incomplete coverage, or inconsistent verification long before execution starts.

Polarion’s direction continues to strengthen its role as a verification and validation hub for evidence coming from simulations, automated pipelines, and external engineering tools – so teams can keep audit-ready traceability even as validation becomes more distributed and automated.

Collections for controlled context and parallel validation

One of Polarion’s strongest enablers for early validation at scale is Collections. A Collection represents an immutable snapshot of requirements, tests, and other artifacts at a specific point in time.

Collections allow teams to:

  • freeze approved baselines,
  • validate against a known, stable context,
  • support parallel development and validation streams,
  • maintain audit‑ready evidence without copying data.

Early validation depends on knowing what exactly is being validated. Collections remove ambiguity by making context explicit and controlled.

Orchestrating validation across tools and simulations

Polarion does not aim to replace simulation or execution tools. Instead, it orchestrates validation by capturing results, linking evidence, and maintaining traceability. Roadmap direction makes this explicit: Polarion is evolving as a verification and validation hub, capable of collecting evidence from simulations, automated pipelines, and external tools into one governed model.

This approach allows teams to:

  • validate earlier using simulations or models,
  • keep evidence centralized,
  • preserve traceability and audit readiness.

Early validation is not isolated testing – it is governed validation with evidence.

The Siemens Advantage: More Than a Tool

It’s worth stepping back to acknowledge something that no feature comparison table can fully capture: Polarion is part of the Siemens Xcelerator portfolio.

This means that Polarion doesn’t operate in isolation. Polarion seamlessly connects to Siemens Xcelerator including:

  • Teamcenter for PLM and systems engineering
  • Capital for electrical/electronic architecture
  • Simcenter for simulation and testing

For organizations pursuing a true digital thread – where requirements, design, simulation, and tests are connected across the entire product lifecycle – Polarion is the only ALM solution that lives in such ecosystem.

Polarion doesn’t just manage tests. It orchestrates validation.

Frequently Asked Questions

  • What is Polarion used for in early validation?

For organizations scaling systems engineering, early validation with Polarion provides a controlled, audit‑ready backbone for linking requirements, approvals, tests, and simulation evidence. Teams use it to define what must be proven, track what evidence exists (including simulation outputs), and show coverage and status as requirements change.

  • Can Polarion scale for large engineering organizations?

Yes. Polarion is used in large deployments and is proven to support 7,000 concurrent active users on repositories with tens of millions of work items, and 80,000+ registered users. This matters when you need consistent workflows, permissions, and traceability across many teams and programs.

  • How does Polarion connect requirements, tests, and simulation evidence?

Polarion connects these domains through traceability links: requirements link to test cases and test runs; defects link back to the affected requirements and verification activities; and validation evidence (including simulation results) can be captured and linked so you can navigate from a requirement to the proof that it was verified. This creates audit-ready coverage views and impact analysis when requirements change.

  • How does Polarion support audit-ready approvals and change control?

Polarion provides configurable workflows, baselines/Collections, and full change history so teams can control how requirements and validation artifacts move from draft to approved. For regulated or audit-focused work, it also supports electronic signatures (including 21 CFR Part 11 scenarios) so approvals are captured in the same system as the content and traceability.

  • Does Polarion only manage tests?

No. Polarion also manages requirements and reviews, maintains traceability across the lifecycle, and provides reporting on coverage and validation status. That makes it useful not just for executing tests, but for proving (with linked evidence) that requirements were verified – including when evidence comes from simulation or automation.

  • How does Polarion fit into the Siemens Xcelerator ecosystem?

Polarion is part of Siemens Xcelerator and is commonly used alongside tools such as Teamcenter (PLM) and Simcenter (simulation/testing). In practice, this supports a more connected digital thread where requirements and validation evidence in Polarion can align with downstream engineering and simulation activities.

  • Can Polarion support parallel development across releases and variants?

Yes. Teams commonly use baselines and Collections to validate against a defined snapshot while development continues elsewhere. This helps manage parallel work (for example, multiple releases in flight or product variants) without losing track of which requirements and tests were valid for which configuration.

Jandl Jiri

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/polarion/accelerate-and-scale-early-validation-with-polarion/