Siemens Digital Industries Software Blog Network

Siemens Digital Industries Software Blogs


Corporate Blog

Femap Symposium 2013 Detailed Agenda

We’ve just finalized and published a detailed agenda with a dual track for the Femap Symposium 2013. Topics include: Keynote – Mars Science Laboratory Rover Curiosity - The role that FEA pla...

Academic and Future Workforce

EcoCAR2 Year Two Competition Report

Several of us were at the EcoCAR 2 Year Two Competition last week in San Diego. Check out the news release and related links for more information on the event and program. Penn Stat...

Designcenter Solid Edge

Solid Edge ST5 Maintenance Pack (MP7)

The latest Maintenance Pack (MP7) for Solid Edge ST5 is now available for download. Thanks for helping us make Solid Edge more productive.

Embedded Software

Two heads are better than one

Sometimes I have an idea, or gain an understanding or insight into something, and I have to share. That is...

NX Manufacturing

In Simulation We Trust

This article appeared in MoldMaking Technology magazine, Gardner Publications, Inc., USA. www.moldmakingtechnology.com Some CAD systems come equipped with directly integrated mold flo...

Verification Horizons

IEEE 1801™-2013 UPF Standard Is Published

Download the standard now – at no charge The IEEE Standards Association (IEEE-SA) has published the latest UPF 2.1 standard,...

NX Manufacturing

Virtual Machine inside NX CAM

The Virtual Machine Tool can be used for training, setup, postprocessed NC code validation and even manual editing of NC code just like at the real, physical machine. Machine tool builders that offer...

NX Manufacturing TV

Virtual Machine inside NX CAM

The Virtual Machine Tool can be used for training, setup, postprocessed NC code validation and even manual editing of NC code just like at the real, physical machine. Machine tool builders that offer...

NX Manufacturing TV

Analyze Mold Flow in NX

Sam Kuan, Siemens PLM, demonstrates the new injection flow capabilities in NX 8.5. Capabilities include melt front time, air trap, weld line, pressure drop, melt front temperature, maximum temperatur...