Products

Sketch | June 2023 | NX Tips and Tricks

Welcome to the new series of NX Tips and Tricks

Today, we are going to look at several ways to enhance your performance in NX™ software Sketch using some simple sketching features. NX Sketch is a powerful tool that allows you to create and edit 2D sketches with ease and precision. Whether you are a beginner or an expert, you can benefit from these tips and tricks to make your sketching process faster and more efficient.

Let’s get right into it!


Create a profile with the profile command

Let’s first open a sketch and create a profile. A profile is a closed shape that can be used to create 3D features such as extrusions, revolutions, sweeps, and lofts. To create a profile, we can use the profile command, which is located in the sketch ribbon bar. The profile command allows us to create continuous straight and curved lines, which reduces the number of commands we need to use to make our sketch.


Drag points and relax relations

Now that we have created our profile, we can modify it by dragging its points. When we drag a point, we can see that it has some relations that constrain its position. Relations are geometric constraints that define how sketch entities relate to each other or to the sketch plane. For example, a point can have horizontal or vertical relations that keep it aligned with the origin.

In this example, when we selected the vertical relation, it turned purple and relaxes. This means that it is temporarily ignored and does not affect the point’s position. And when we move the point, the horizontal relation remains allowing the top line to stay horizontal.

These horizontal relations are an easy way to control the shape and angle of a sketch. We can also add or delete relations manually by using the tools in the sketch ribbon bar.


Move multiple curves by selecting them

Sometimes we want to change the length of a curve and also move several other curves with it. To do this, we can select the curve we want to change, and then select the other curves we want to move along with it. When we change the length of the curve, either by dragging its end point or entering a value in the mini toolbar, the other selected curves move along with it.


Forming collinear relations

Another useful relation that we can use in NX Sketch is the collinear relation. This relation makes two lines share the same line of action. We can use this relation to make two peaks of our sketch collinear, which means that they lie on the same line.

To apply this relation, we simply select two lines that we want to make collinear, and then click on the collinear icon in the mini toolbar or in the sketch ribbon bar.

When we apply this relation, we can see that one of the lines moves to align with the other line. When one line is moved, the second one moves with it, maintaining the collinear relation.


Ignore relations to change the design intent

Sometimes we want to change the design intent of our sketch, which means that we want to change how our sketch behaves when we modify it. For example, we may want to move one peak of our sketch without affecting the other peak, even though they have a collinear relation.

To do this, we can use the ignore relation feature, which allows us to temporarily disable a relation without deleting it. This way, we can change our sketch without losing the original relations.

To use this feature, we first select the curve that we want to move, and then select the relation that we want to ignore. We can see that the relation turns gray and has an ignore symbol on it. As you can see, the ignore relation symbol appears, and when we move one peak, the second one does not move with it like it did before.


Recap and conclusion

In this blog post, you learned several tips and tricks to enhance your performance in NX Sketch. You saw how to:

  • Create a profile with the profile command
  • Drag points and relax relations
  • Move multiple curves by selecting them
  • Forming collinear relations
  • Ignore relations to change the design intent

We hope you found these tips and tricks useful and that they will help you create better sketches in NX Sketch. Happy sketching!


Continue your journey with NX


NX Sketch | Summer 2023 | Tips and Tricks Video

Drew Wilson
Copywriter - Siemens Digital Industries Software

Drew Wilson is a Copywriter at Siemens Digital Industries Software where he crafts compelling, technically-informed content for Designcenter NX. As a graduate of Xavier University with a degree in Advertising + Public Relations and a concentration in Technical Writing, Drew brings a unique blend of creative storytelling and precision to his work. Before his time at Siemens, Drew honed his skills in an agency environment, writing for over 70 midsized manufacturing companies. His experience spans both traditional industrial sectors and the fast-paced startup world, giving him a versatile perspective writing styles and outlets. Since joining Siemens Digital Industries Software in 2023, Drew has contributed to a wide range of initiatives that have deepened his expertise in CAD software, PLM systems, and particularly Designcenter NX. His work supports product teams, marketing campaigns and customer-facing content, helping to translate technical innovation into accessible narratives that resonate with engineers, decision-makers and end users alike.

More from this author

Jamie Tyler
Senior Marketing Coordinator - Siemens Digital Industries Software

Business Studies was Jamie's degree of choice at university, which he tailored to marketing during his final year. He's always been intrigued by the role high-quality visualization plays in product design. Jamie's first job out of university was with an SDK renderer, giving him the writing experience he needed to tailor visualization content across a range of industries. He also previously worked at Sheffield Hallam University, where he provided key marketing support to students embarking on their journey through higher education. Since joining Siemens Digital Industries Software in 2018, Jamie has built on his visualization expertise to create content across a wide breadth of disciplines. Whilst at Siemens, he has developed his expertise with Designcenter NX CAD software, alongside other Siemens Xcelerator products, including Teamcenter, NX CAM and Simcenter. It's rather fitting that Jamie's story has come full circle with regards to visualization; Jamie is heavily involved in Immersive Engineering; a new collaboration between Sony and Siemens that combines a new XR headset with Immersive Designer; a software package developed by Siemens Digital Industries Software.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/nx-design/sketch-summer-2023-nx-tips-and-tricks/