Products

Automatic Draft Calculation | NX Tips and Tricks | January 2024

NX’s™ continuous release cycle means that there are always new ways to improve your designs and your workflows. Automatic Draft Calculation in NX’s Molded Part Design add-on module is just one of the many enhancements you can find in the December 2023 release.

Automatic Draft Calculation is an AI-enabled tool that helps you quickly make the right design decisions to create better products with fewer iterations. It analyses your design based on a wide range of variables and recommends a suitable draft angle when using the Draft command on a particular face.

Read on or watch the video to learn more about how it works.

Step 1 – Moldability Validation

Before adding draft, we want to check the overall moldability of the part. Molded Part Design’s Moldability Validation report will quickly highlight any areas of the design that need draft.

First, use the Draw Direction command to check that the draw is correct and specify the draw direction if not.

A screenshot of the Draw Direction command in Siemens' NX Molded Part Design

Now you’re ready to run Moldability Validation to automatically check for a number of potential design issues, such as:

  • Thin walls
  • Thick walls
  • Vertical walls
  • Undercut regions

All these are highlighted in an intuitive, color-coded visual report in the Graphics Window, with extra details available in the Molded Part Design Navigation.

A screenshot of the Moldability command in Siemens' NX Molded Part Design showing moldability issues such as vertical walls

Read more about Moldability Validation

Step 2 – Draft & Recommended Draft Angle Report

Moldability Validation has highlighted some vertical walls on our design. We need to add draft to these faces to ensure that the component is moldable.

But what draft angle should you choose?

A larger draft angle can make parts easier to remove from a mold, while smaller draft angles can result in smoother surface finishes. The optimum draft angle is a balance of these two factors.

Molded Part Design’s Draft command now includes a Recommend Draft Angle option which can answer this question for you.

Once you’ve selected the face on which to add draft, the AI-enabled Recommended Draft Angle Report analyses the design to suggest a draft angle. It balances the two criteria above, while computing variables such as:

  • Design thickness
  • Draw direction
  • Assigned material
  • Geometric conditions (such as maximum depth of the face along the draw direction)

Make sure you check the recommended draft angle each time you add draft to a new face – the specific geometric conditions of each face may mean different results.

If you run the report without a material assigned, it’ll show you the minimum draft angle for a range of material options. If you have a material assigned, you’ll only see the material relevant to you.

Step 3 – Revalidate

Once you’ve added draft to the part using the Recommended Draft Angle Report’s suggested angles, you can run Moldability Validation again to check that it’s resolved the issues flagged earlier.

In our case, adding draft to certain faces has dealt with the vertical walls highlighted when we first ran the report.

You’re now ready to address any other moldability issues such as unsuitable wall thickness or undercut areas.

Watch the Automatic Draft Calculation video

Automatic Draft Calculation can save time for your designers and reduce time to market for your molded parts by leveraging AI to ensure right-first-time design.

Watch NX Molded Part Design’s draft angle recommendations at work in the video below.

And don’t forget to check out all the other powerful new enhancements in the December 2023 release of NX.

Michael Hobson
Senior Copywriter - Siemens Digital Industry Software

While Michael studied Philosophy at university, Michael comes from a family background of engineers and engineering. He’s taken an interest in engineering from an early age and as a competitive cyclist, has a particular focus on the application of mechanical engineering, material science and design simulation to sports technology. Michael’s first job out of university was at a bicycle manufacturer, where he got his first experience writing about product design and engineering within the sports industry. This later became a specialism while Michael was working as a freelance copywriter. He has also worked at Sheffield Hallam University, where he wrote about a variety of their advanced engineering research projects and industry collaborations, among other things. Since joining Siemens Digital Industry Software in 2023, he is now back in the family business of engineering. While at Siemens, he has developed his expertise with Designcenter NX CAD software, along with other Siemens Xcelerator products across the PLM, CAM and simulation domains such as Teamcenter, NX CAM and Simcenter. As well as producing software demonstrations for videos such as the yearly Designcenter NX Premiere, Michael uses Designcenter NX to design and model various 3D-printed DIY projects around the home. He's currently working towards Designcenter NX certification through the Siemens Xcelerator Academy.

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/designcenter/auto-draft-calculation-nx-jan-2024/