Thought Leadership

Embedded articles – medical systems, C function parameters, multitasking and Forth

Although I regard the New Year as a time to look forward, I am continuing my catch-up process of cataloging embedded software articles that I have had published on embedded.com in the recent past. This time they cover medical systems, C function parameters, the basics of multitasking and the Forth language…

Electronics for the Sick

Electronics is used for numerous applications, but one, for which most of us feel grateful, is medical instrumentation. A modern hospital or doctor’s surgery is bristling with electronics. This article reviews the embedded software technology that drives such systems and looks at how this application area is driving many new developments as well as leveraging existing techniques and devices. At the same time, medical applications present new challenges to embedded software developers, which cannot be ignored.

Key Health Care Trends and Issues

Function Parameters

Passing parameters to a C function seems simple enough, the details of how that process takes place have a significant impact on the behavior and performance of the code. Programmers of desktop computers do not care about this impact; embedded developers do not have that luxury. This article looks at parameter passing mechanisms and how to use them optimally.

A multitasking kernel in one line of code – almost

In a world dominated real time operating systems with enormous arrays of functionality and full scale operating systems, like Linux, it can be useful to stand back and consider the basics. What if you just need some basic multi-threading? How complex does that need to be? In this article, some ideas are proposed for almost trivially simple multi-threading, which might even be implemented in a single line of code!

Fig

Go Forth!

The most commonly used programming language for embedded applications is C, with C++ gradually becoming more popular. C was never designed for embedded use, but a handful of languages were intended from day 1 to be used for this purpose. One of those languages is Forth. Although it may be argued that the language’s heyday was about 30 years ago, there are still a loyal band for Forth fanatics who keep the language alive. In this article, there is a very brief introduction to the language and we consider whether it might have a place in modern embedded systems.

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

More from this author

Comments

One thought about “Embedded articles – medical systems, C function parameters, multitasking and Forth
  • Colin, I think that Forth has a revival. Bloatware is an issue, as is IoT. In Iot you want to have very small code, and you want to be sure that the number of wholes for others to get in is minimized. As far as I know Forth is actually the only option if you want a fully certified compiler. And for people who are new to it, we have just done a project with the scouts, where they soldered their own “beating heart”, 450 Forth systems, now they can start programming – all software is actually on the chip, just talk to a terminal (or PC). Interactive is one important point here, Just google “Time of your Light”. Definitely not old or over – the features are required more and more. Software is built in small pieces and can be tested immediately It grows as you design, based on tested substructures. There are letters (assembly ) to write words ( actually called Words), words are combined to phrases, then chapters – and at some point the novel ( application) is ready. We know who uses it, as well sell the Forth Compilers from the UK – see http://www.mpeforth.com

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2015/01/05/embedded-articles-medical-systems-c-function-parameters-multitasking-and-forth/