Thought Leadership

On the move

I recently talked about the process that might be applied to the selection of an embedded operating system and I hope that these guidelines are useful. I am currently working on a Web seminar on this topic, so I would welcome any input. However, developers tend to stick with a particular OS [or, at least, with a particular OS vendor] – recent research suggested that only about 20% of developers anticipated a change of OS for their next project.

I started thinking about why there is this apparently high degree of loyalty …

I do not think that there is a single, simple reason why embedded software engineers choose to use the same OS time and again. One motivation is that embedded guys have a pragmatic conservatism: “if it ain’t broke, don’t fix it”. Although that attitude is quite reasonable, I think that we can identify two specific reasons not to change OS:

1) Vendor satisfaction. If the level of support and quality of documentation is very good or excellent, that is definitely a reason to stick with a particular OS vendor [as it is with almost any product].

2) Skills and IP lock-in. The technical characteristics of a given OS permeate the application code and the skill set of the team. This has primarily two manifestations:

a) Drivers and middleware are often very specific to a particular OS. Moving to a new OS implies the acquisition of new skills and rewriting of a lot of code.

b) The application program interface [API] ties the application code to the OS and also represents part of the team’s skill set. It is true that many RTOS products have a proprietary API. Moving to another OS would require changes to the application code. Alternatively, many developers us an OS abstraction layer to protect themselves from such a change – only the layer needs to be modified to accommodate a change in OS. Another approach is to embrace a standard and the common API standard is POSIX. Although this is the native API for Linux, it is also supported by many RTOS products and its use provides a degree of code portability.

If you are sticking with a particular OS for other reasons, I would be interested to hear by comment or email.

 

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2011/06/20/on-the-move/