Products

NX Tips & Tricks | Move and Offset Curves

It’s time for another set of NX™ Software Tips & Tricks! This edition covers two more commands that can save you time and effort while sketching – Move Curve and Offset Move Curve.

As ever, you can watch the video below to see these commands in action as part of a step-by-step workflow demonstration. Or keep scrolling if you’d prefer to read about them instead.

Move Curve

Move Curve lets you move or rotate a set of curve sketches. With the Motion option set to Dynamic, you can manually drag the curves into place or input specific co-ordinates for greater precision.

NX will automatically adjust relations and adjacent curves in the sketch to enable the change.

A screenshot of NX Software showing the Curve Finder within the Move Curve command dialog

That may seem simple enough, but there are some extra features that really make this command shine.
Select the Curve Finder option and NX will look at your selected curves and find other related curves in the sketch based on specific geometry conditions. For example, that means you can move one curve and any others that are collinear just with a single Move Curve command.

You can also select an axis or curve as the symmetry axis for the move operation. NX will retain symmetry when move your selected curves so you don’t have to judge it manually or adjust afterwards.

Offset Move Curve

Offset Move Curve moves a whole set of sketch curves by offsetting them a specified distance.

As with Move Curve, NX will automatically adjust relations and adjacent curves in the sketch if necessary. It also has the same Curve Finder and symmetry axis functionality adding extra utility.

In the video above, Scott shows how useful the Curve Finder can be.

He wants to offset a set of curves, but this would detach them from the rest of the sketch.

A screenshot of NX software showing the Offset Move Curve command in use. A preview shows that the operation would result in the offset curves becoming detached from the rest of the sketch.

The Curve Finder, however, has automatically detected Coincident and Parallel curves that it can add to the operation. With the additional curves included, NX offsets and moves the rest of the sketch to match the main set of curves.

A screenshot of NX software showing the Offset Move Curve command's Curve Finder functionality in use. It has moved and offset related curves as well as the initial selection to ensure that the whole sketch remains connected.

Tips & Tricks – Delete Curves

We’ll have more Tips & Tricks again for you shortly. In the mean time, here’s another recent edition related to sketching curves. It demonstrates a nifty command that not only deletes curves in your sketch, but automatically replaces them with new geometry too!

Michael Hobson
Senior Copywriter - Siemens Digital Industry Software

While Michael studied Philosophy at university, Michael comes from a family background of engineers and engineering. He’s taken an interest in engineering from an early age and as a competitive cyclist, has a particular focus on the application of mechanical engineering, material science and design simulation to sports technology. Michael’s first job out of university was at a bicycle manufacturer, where he got his first experience writing about product design and engineering within the sports industry. This later became a specialism while Michael was working as a freelance copywriter. He has also worked at Sheffield Hallam University, where he wrote about a variety of their advanced engineering research projects and industry collaborations, among other things. Since joining Siemens Digital Industry Software in 2023, he is now back in the family business of engineering. While at Siemens, he has developed his expertise with Designcenter NX CAD software, along with other Siemens Xcelerator products across the PLM, CAM and simulation domains such as Teamcenter, NX CAM and Simcenter. As well as producing software demonstrations for videos such as the yearly Designcenter NX Premiere, Michael uses Designcenter NX to design and model various 3D-printed DIY projects around the home. He's currently working towards Designcenter NX certification through the Siemens Xcelerator Academy.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/designcenter/nx-tips-tricks-move-offset-curves/