Products

Compare Body | NX Tips and Tricks

Welcome back to another installment of the Tips and Tricks series for NX™ software. Today, we will be checking out functionality around the Compare Body command. If you work with different versions of the same part, you might want to know what changes have been made between them. This can help you avoid errors, track modifications, and communicate better with your team. In this week’s tips and tricks post, I will show you how to use the Compare Body command in NX to easily compare and visualize the differences between two bodies.

What is Compare Body

Compare Body is a command that allows you to compare two bodies and see the changes in color, shape, and position. You can use it to compare bodies from different files, different versions, or different configurations. You can also save the comparison results as a linked body that updates automatically when the original bodies change.

How to use Compare Body

To use Compare Body, you need to have two bodies that you want to compare. They can be in the same file or in different files. For this example, I have an original version and a modified version of a model.

To start the comparison, go to Tools > Compare > Compare Body. In the dialog box, select the Control Body and the Sample Body. The Control Body is the reference body that you want to compare against, and the Sample Body is the body that has been changed. You can also choose the color settings for the comparison results.

This image shows two separate bodies that can be compared within NX.

After clicking Compare, you will see three windows: one showing the Control Body, one showing the Sample Body, and one showing an Overlay of both bodies. The Overlay window shows the changes in color according to your settings. For example, red means absent (the feature exists in the Control Body but not in the Sample Body), green means new (the feature exists in the Sample Body but not in the Control Body), and yellow means changed (the feature exists in both bodies but has a different shape or position).

You can use the slider at the bottom of the Overlay window to fade between the Control Body and the Sample Body and see how they differ. You can also rotate, zoom, and pan in any of the windows to inspect the changes more closely.

How to analyze changes

One of the powerful features of Compare Body is that it allows you to analyze the changes in more detail using different criteria. You can access these criteria by clicking on the Face Change Criteria button in the dialog box.

The default criterion is Color Only, which shows only the color differences between the bodies. However, you can also choose Deviation, which shows how much each face has moved or changed shape from the Control Body to the Sample Body. This can help you measure and quantify the changes more precisely.

This image shows the command bar to change to deviation.

When you choose Deviation, you will see numbers and points on the faces that have changed. The numbers indicate the distance between corresponding points on the Control Body and the Sample Body. The points are referenced from the Sample Body to the Control Body. You can also see more faces highlighted in yellow, which means they are affected by the changes.

How to save comparison results

If you want to save your comparison results for future reference or communication, you can do so by creating a Linked Body. A Linked Body is a special type of body that contains only the faces that have changed between the Control Body and the Sample Body. It also updates automatically when either of the original bodies changes.

To create a Linked Body, make sure you check the Save Analysis Object option in the dialog box before clicking Compare. This will create a new body under your Part Navigator with a link icon next to it.

You can then show or hide this body as you wish. You can also rename it or change its color for clarity.

This image shows what the body looks like with the show and hide command presented.

Continue your journey with NX

Compare Body is a useful command that can help you compare and visualize changes between two bodies in NX. It can help you avoid errors, track modifications, and communicate better with your team. You can also analyze changes using different criteria and save comparison results as a Linked Body that updates automatically. If you have enjoyed this installment, there is an entire series dedicated to providing Tips and Tricks within NX.

Compare Body | Tips and Tricks | YouTube Video

Drew Wilson
Copywriter - Siemens Digital Industries Software

Drew Wilson is a Copywriter at Siemens Digital Industries Software where he crafts compelling, technically-informed content for Designcenter NX. As a graduate of Xavier University with a degree in Advertising + Public Relations and a concentration in Technical Writing, Drew brings a unique blend of creative storytelling and precision to his work. Before his time at Siemens, Drew honed his skills in an agency environment, writing for over 70 midsized manufacturing companies. His experience spans both traditional industrial sectors and the fast-paced startup world, giving him a versatile perspective writing styles and outlets. Since joining Siemens Digital Industries Software in 2023, Drew has contributed to a wide range of initiatives that have deepened his expertise in CAD software, PLM systems, and particularly Designcenter NX. His work supports product teams, marketing campaigns and customer-facing content, helping to translate technical innovation into accessible narratives that resonate with engineers, decision-makers and end users alike.

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/designcenter/compare-body-nx-tips-and-tricks/