What’s New in NX | June 2025 | Core Design
Welcome to the latest edition of What’s New in NX™ software series! Built around industry-specific workflows, NX is the engine behind the digital twin—delivering powerful, flexible tools that drive innovation from concept to production.
The June 2025 release brings a host of powerful new features designed to elevate your productivity and streamline your workflows. In this update, we’ll take a closer look at the latest enhancements in Core Design and spotlight improvements to the Sketch Curve Creation functionality as well as improvements to the overall user interface.
Let’s dive in!
New Curve Creation functionality for interaction and feedback
The latest NX release introduces powerful new Curve Creation functions within NX Sketch that deliver enhanced usability and feedback. At the core of this update is a modern, intuitive UI for creating Sketch curves—including a pencil cursor that indicates “Create Curve Mode” and a dynamic handle that follows cursor movement. An intuitive color-coding system conveys corresponding functionality:
- Red indicates no snapping
- Yellow signals point-on-curve snapping
- Green confirms coincident snapping

These enhancements support multiple input methods, including mouse, stylus, and touch screens, while providing comprehensive journaling API support for creating programmatic functions, making it a valuable addition for both end-users and developers.
Updated and more intuitive user interface interaction
Enhanced functionality for Curve Creation now supports both traditional and modern interaction methods, offering legacy MB1 click behavior alongside new MB1 press-and-drag capabilities. Direction locking has been improved with the ability to trigger this feature through MB2 when previewing snap conditions, or by pausing the cursor for automatic direction lock. You can also unlock directions using either MB2 or a simple shake gesture.

Enhanced manipulation features include the ability to adjust a line or arc’s start handle through MB1 press-and-drag interactions; while in-command trimming and extending can be accomplished through intuitive scribble gestures.
The new NX Sketch UI also introduces the ability to:
- Lock length, angle, and radius parameters with a “stamp” feature
- Chain curves to create Profiles
- Generate Reference Geometry
- Create Segments, Infinite Lines, or both
Create Profiles using the Line and Arc commands
In this most recent version of NX, you can now create Profiles seamlessly using Line and Arc commands, with the notable addition of MB3 functionality. You can activate Chaining to create profiles and switch between Lines and Arcs using MB3—eliminating the need to access the dialog box. Both tangent and perpendicular snapping to preceding curves in the chain is also supported, ensuring precise and connected profile creation.


Increased tangency control for quicker profile creation
Improved Curve Creation functions feature intelligent Line to Arc snapping capabilities, offering greater control and flexibility. With enhanced tangency features, you can now break tangency simply by passing the cursor through the snap point—while mouse direction after snapping determines whether a line is created tangent or not.
A notable addition is the Tangent Sliding feature, which allows arcs to slide smoothly along lines for precise positioning. Users can dynamically modify arc definitions by passing the cursor through arc points, and a simple shake gesture provides a quick way to break tangency when needed.
New Line Creation methods provide flexibility
In response to customer feedback, NX’s latest release introduces valuable new curve creation methods that enhance design flexibility. The update features two highly requested functions: Line from Mid-point and Rectangle from Center.
The Line from Mid-point capability introduces a new approach to line creation where the initial point serves as the midpoint, allowing the line to extend bidirectionally with the same core functionality as the standard Line command. It is worth noting here that Chaining, Relative Angle, and Change to Arc features are not supported using this method.

The Rectangle from Center function builds upon previous enhancements, offering an improved workflow where reference lines and center points are automatically generated, resulting in superior modification capabilities.
Axial Pattern enables support for cylindrical and conical shaped parts
The Axial Pattern capability of NX supports workflows that require patterns along cylindrical or conical faces. This innovative feature enables users to combine cylindrical and linear patterns in a single operation, significantly streamlining workflows for components with circular and axial repeated elements.

This comprehensive functionality allows for precise patterning around a diameter while simultaneously extending along an axis, with full support for conical faces as well as axial stagger. With the June 2025 release of NX, Axial Pattern has been integrated across multiple pattern tools, including Pattern Feature, Pattern Geometry, and Pattern Face commands, while also being supported within Reference Pattern operations.
Conclusion
Thanks for stopping by learn about and explore some of the exciting new Core Design features in the June 2025 release of NX! We’ll continue to share more What’s New in NX highlights as we cover additional topics and industry-specific capabilities—so be sure to bookmark the NX Design Blog and check back regularly!
In addition to the What’s New in NX series, don’t miss our Tips & Tricks series to explore even more content and videos from the June 2025 Premiere. The Tips & Tricks posts are a great way to dive deeper in NX functionality and learn how to streamline your design workflows.
Comments
Leave a Reply
You must be logged in to post a comment.
The new Curve Creation tools and intuitive UI enhancements in NX June 2025 are a game-changer for precision and speed in sketching workflows. Features like tangent sliding, Retro Bowl College dynamic snapping, and gesture-based commands show Siemens is listening closely to user feedback and pushing usability forward.
Great rundown of the June 2025 NX updates—especially the Sketch Curve Creation tweaks and Axial Pattern support on conical faces. The MB1 press-and-drag plus MB3 switching for Line/Arc is a big quality-of-life win, and the “stamp” locks for length/angle/radius feel spot-on for precision sketching. Looking forward to trying Tangent Sliding in real projects.
P.S. Quick brain break between design sprints? Try
retro bowl.
Once, I was trying to design a complex interlocking gear system for a personal project, and the CAD software kept crashing when I tried to boolean operations, leaving me frustrated and behind schedule. The feeling of struggling to create smooth, curved shapes felt like I was stuck in a giant Slither io game, endlessly trying to navigate a maze with limited tools!
Tubidy is a multimedia search platform designed to help users find, stream, and download music and videos with ease. Tubidy.ke offers a lightweight interface that works smoothly on mobile phones, tablets, and desktops.
The new Curve Creation tools and intuitive UI enhancements in NX June 2025 are a game-changer for precision and speed in sketching workflows.
Regards
https://retrobowl25.games/
Your problem-solving abilities are as remarkable as Tubidy ability to curate diverse content for every user.
Like Tubidy, you have a unique talent for bringing people together with your ideas and collaborative spirit.
This update sounds like a solid step forward for NX, especially for people who spend a lot of time in sketching and design mp3 juice workflows. The improved curve creation UI with real-time feedback is a nice touch, it makes the process feel more intuitive and less like you’re constantly second-guessing what the software is doing.
The color-coded snapping system also seems really helpful. Small visual cues like red, yellow, and green can make a big difference in ytmp3 precision work, especially in complex sketches where accuracy matters a lot.
Amazing guys .. you will keep spirit.. tubidy
Launched in the early 2010s, Tubidy mp3 started as a basic mobile video search engine. Over the years, it expanded its repertoire to cover a vast array of music genres and high-quality videos.
It gained popularity for its user-friendly interface and simplicity, providing a quick and accessible way for users to find a diverse range of music. Users can input the name of a song or artist into the search bar, and MP3 Juice provides links to either stream or download the requested music.