Industries

The engineering vs. manufacturing divide is killing durable consumer goods innovation 

The durable consumer goods industry is experiencing its most significant transformation in decades. Product development cycles that once provided comfortable timeframes have compressed significantly, with companies facing increasing pressure to accelerate time-to-market. Market fragmentation demands mass customization at scale.   Sustainability expectations require companies to optimize for environmental impact alongside performance and cost. Finally, demands for better supply chain transparency has reached unprecedented levels. Without greater insight, brands run the risk of reputational damage, regulatory non-compliance and operational disruptions, for example. 

Yet most companies—whether developing next-gen bicycles, smart home appliances, innovative power tools, or state-of-the-art windows and doors— are still operating with an engineering-to-manufacturing handoff process designed for a different era. This disconnect isn’t just slowing innovation; it’s becoming an existential threat to competitive positioning. 

The companies that will dominate the next decade of durable consumer goods aren’t just those that innovate faster. They’re the ones fundamentally reimagining how engineering and manufacturing collaborate from concept to market. However, this transformation comes with significant organizational and technological challenges that many companies underestimate. 

The strategic cost of operational silos 

The engineering-to-manufacturing handoff has evolved into a primary bottleneck constraining innovation velocity across consumer goods categories. From bicycle manufacturers optimizing carbon fiber frames to appliance companies integrating smart (i.e. software-driven) features, the pattern is remarkably consistent: engineering teams optimize for performance and aesthetics, then discover manufacturing constraints that force costly redesigns and timeline extensions. 

Consider the broader strategic implications. While product teams cycle through design-test-redesign loops, market windows close. Meanwhile, competitors with integrated development processes capture first-mover advantages or consumer attention shifts to newer innovations. Investment in failed products becomes sunk cost rather than market success. 

The organizational structure that created this problem runs deeper than most companies realize. Engineering teams measure success through design optimization and innovation metrics while manufacturing teams focus on efficiency, quality, and cost control. These aren’t just different priorities—they’re often conflicting objectives embedded in performance reviews, budgets, and career advancement paths. 

The manual handoffs between these functions create multiple points of failure. Specifications are misinterpreted, design intent gets lost in translation, and manufacturing constraints discovered late in the process force expensive redesigns. Each handoff introduces delays and the possibility of errors that cascade through the entire development cycle. 

What integration looks like in practice 

Forward-thinking durable brand companies  are discovering that the solution isn’t faster handoffs—it’s eliminating the handoff entirely through parallel engineering and manufacturing decision-making with an integration that creates automatic translation from design decisions to production instructions. 

The key is having a single source of truth—a PLM digital backbone that both engineering and manufacturing teams can work from. This single source of truth enables the creation of digital twins of both the product and the production process, making true concurrent collaboration possible without manual handoffs. 

Giant Bicycles’ recent  showcase at Hannover Messe 2025 illustrates this transformation in practice. Giant Bicycles demonstrated how it has implemented Siemens’ cutting-edge Designcenter, Teamcenter and Simcenter software to create the bikes of the future. 

Two of Giant Bicycles’ latest innovative bikes were featured: Giant’s Trance X Advanced E+ Elite 0, a revolutionary e-mountain bike built around a lightweight, stiff and durable carbon frameset that combines advanced trail bike design with a powerful new motor and a fully integrated battery system. Giant’s Trinity Advanced SL 0 delivers dynamic speed and control, easily adapts to triathlon or time trial, and features aero-integrated hydration and fueling systems. It’s lighter, more aerodynamic and smoother riding than the previous generation, with greater adjustability to dial in position and fit. 

This integration extends beyond bicycles to every consumer goods category. For instance, home appliance manufacturers can simultaneously optimize product performance and assembly line efficiency or  consumer electronics companies can validate component placement and manufacturing sequences in parallel with circuit design. Even coffee machine developers can ensure that complex internal mechanisms are both functional and producible from day one. 

The democratization of enterprise capabilities 

The accessibility barrier that previously limited sophisticated engineering-manufacturing integration to Fortune 500 companies has largely disappeared. For this integration to work effectively, engineering and manufacturing teams need access to a portfolio of solutions that bring both disciplines together—from CAD and CAM to simulation and manufacturing planning. 

This is where Siemens Xcelerator comes into the picture. Siemens already offered Teamcenter, a product lifecycle management software suite; Simcenter, a portfolio of advanced engineering simulation and testing solutions; and Opcenter, a portfolio of software applications for manufacturing operations management. At CES 2025, Siemens announced the launch of Designcenter—a software suite for product development, bringing together Siemens design and engineering tools under one subscription. 

Here’s how Designcenter works in practice: Teams use streamlined design tools for everyday development, then access advanced simulation and manufacturing analysis capabilities when projects require them. For example, a small coffee machine manufacturer can use cost-effective tools for basic design work, then access enterprise-grade capabilities for complex thermal analysis or injection molding simulations when developing new brewing mechanisms. 

The coffee machine industry exemplifies this democratization in action. Traditional development required separate teams working sequentially: industrial designers creating the exterior, mechanical engineers developing internal mechanisms, software engineers coding the smart functionality, and manufacturing engineers solving production challenges. With integrated approaches, these teams can collaborate on the same digital product simultaneously, whether they’re a three-person startup or a major appliance manufacturer. 

This flexible approach means that whether you’re developing your first smart coffee machine or your hundredth appliance model, you’re working with the same foundational engineering collaboration platform. Designcenter brings different engineers together—mechanical, electrical, software, and industrial design teams—enabling them to work on the same digital product simultaneously. 

As companies scale from managing 3 product variants to 30 to 300, a key advantage emerges: they can include  all product variations needed for personalization, different market regulations, and customer-specific requirements in one comprehensive BOM (Bill of Materials). This 150% BOM approach allows companies to drive specific configurations for specific orders and markets, rather than managing separate product versions for each variation. 

This scalability delivers strategic advantages beyond cost accessibility. Companies can grow their engineering capabilities without switching platforms or rebuilding processes, while eliminating the complexity of maintaining multiple product definitions across global markets. 

Platform strategy and competitive differentiation 

The technology platform choice has become a strategic decision with lasting competitive implications. This is where fundamental differences between engineering solutions become apparent: some platforms stop at design optimization, leaving companies to solve manufacturing translation independently. Others bridge directly into manufacturing execution, providing automatic translation from Design Bill of Materials (DBOM) to Engineering Bill of Materials (EBOM) to Manufacturing Bill of Materials (MBOM) to Bill of Process (BOP). This eliminates the manual handoffs that traditionally occur at each stage. This end-to-end integration creates a fundamental competitive advantage that compounds over product cycles.  

When engineering changes automatically update manufacturing processes, companies can respond to market shifts without restarting development cycles. When design decisions include real-time manufacturing feasibility analyses, teams avoid the redesign cycles that extend timelines and increase costs. Most importantly, when there are no manual handoffs between engineering and manufacturing, companies eliminate the translation errors and delays that plague sequential development. 

This integration capability functions as a competitive moat that becomes more valuable as market velocity increases. Companies using integrated platforms can iterate products based on market feedback while planning next-generation innovations. Those relying on platforms that require manual manufacturing translation find themselves managing handoff delays while competitors advance their market positions. 

The complexity of organizational transformation 

Despite technological advances that make integration possible, the most significant barrier remains organizational. Companies attempting this transformation face several predictable challenges that require executive commitment and sustained change management. 

First, teams must develop new competencies. Engineering personnel need an understanding of manufacturing constraints they’ve historically ignored. Manufacturing teams need input into design decisions that were previously finalized before they provided feedback. Both groups require training on collaborative tools and processes that replace sequential handoffs. 

Second, performance measurement systems must align with integrated objectives. Traditional metrics that reward engineering innovation or manufacturing efficiency independently can undermine collaborative development. Companies need shared metrics that reward time-to-market, first-pass quality, total product cost and sustainability impact rather than specific departmental optimization. 

Third, existing technology infrastructure may require significant updating. Legacy CAD systems, manufacturing execution platforms, and data management tools often lack the integration capabilities that parallel development requires. The technological upgrade path can be complex and expensive, particularly for companies with established tool chains. 

However, companies that successfully navigate this transformation gain sustainable competitive advantages. They can respond to market changes without restarting development cycles, evaluate new opportunities against both design feasibility and production reality simultaneously, and compress development timelines while maintaining quality and cost discipline. 

The strategic choice ahead 

The industry stands at an inflection point where engineering-manufacturing integration is transitioning from competitive advantage to competitive necessity. Whether developing sporting goods, home appliances, tools, toys, consumer electronics, or any other branded consumer durable, companies face the same fundamental choice: invest in the organizational and technological transformation required for integrated development or  risk being left behind. 

This choice involves more than technology adoption. It requires honest assessment of organizational readiness, top executive sponsorship, sustained commitment to change management, and willingness to restructure processes that may have existed for decades shifting away from a “this is how we’ve always done it” mentality from users, stakeholders and management. Most importantly, it requires selecting technology platforms that provide end-to-end integration rather than just design optimization. 

The companies that make this transformation successfully—eliminating manual handoffs and achieving automatic translation from engineering to manufacturing—will set competitive standards for their categories and define what’s possible. Those that continue with sequential development will find themselves permanently reactive. Ready to assess where your engineering-manufacturing integration stands? Let’s talk! Whether you’re a major manufacturer looking to accelerate product development or an emerging company seeking competitive advantage, we’re offering a complimentary evaluation of your current development process. This data-driven analysis will provide insight on how to eliminate the manual handoffs that slow innovation and increase costs and how integrated engineering-manufacturing capabilities can define your competitive position in the durable consumer goods market. 

Mario Vollbracht
Vice President, Consumer Products and Retail

As Vice President of Consumer Products and Retail at Siemens Digital Industries Software, Mario brings over 25 years of industry experience, management consulting and an extensive background in IT management. Mario has traversed the entire value chain within retail and consumer products. From a software perspective, Mario has extensive experience with SaaS solutions and how to put customers on a path to the cloud. He has managed full P&L's, while leading diverse teams ranging from account management, sales, marketing and implementation services to product management, product development & strategy. His SaaS portfolio experience spans innovation management, supply chain, finance, sales and marketing.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/consumer-products-retail/2025/06/26/the-engineering-vs-manufacturing-divide-is-killing-durable-consumer-goods-innovation/