Do Not Display

Stop finding electromechanical problems at the prototype stage

How medical device teams can shift integration decisions left and identify packaging, routing and performance issues while designs can still change 

For medical device R&D teams, physical prototyping should validate good engineering decisions, not reveal problems that could have been found earlier. 

Yet, as devices become more compact and multidisciplinary, seemingly small decisions can ripple across the product. A change in electronics may affect packaging. A mechanical change may alter available routing space. Component placement can influence enclosure clearances and thermal behavior. 

The challenge is not simply that medical devices are becoming more complex. It is that engineering teams need enough product context to understand these interactions while they still have the flexibility to respond to them. 

That is changing the role of electromechanical integration. 

Rather than exchanging design information after individual disciplines have already made key decisions, engineering teams can bring electrical and mechanical product context together earlier. Using unified environments like Designcenter™ software, teams can evaluate fit, interfaces and performance before committing to boards, tooling or physical prototypes. 

The real cost of discovering integration problems late 

Consider a seemingly simple design change. 

An electrical engineer modifies a printed circuit board (PCB) to accommodate a component or connector. Electrically, the change works. But, within the complete physical product, that decision may have other consequences. 

Does the updated component height maintain sufficient enclosure clearance? Does the connector still align with the surrounding mechanical geometry? Are keep-out regions respected? Does the revised board configuration affect cooling? 

When teams lack a current, shared product context, they risk discovering these interactions only after individual design decisions have progressed further than they needed to. 

The better question for R&D leaders is not simply, “How quickly can we prototype?” 
Instead, it’s, “How much can we learn before we need the prototype?” 

Shift left by designing in the context of the complete product 

Moving electromechanical integration earlier begins by changing what engineers can see when they make decisions. 

Instead of treating the PCB and mechanical assembly as separate definitions connected primarily through handoffs, tools within the Siemens Xcelerator portfolio—such as Designcenter—allow teams to work with electronics in the context of the complete physical product. 

That means understanding relationships among the PCB, enclosure, connectors, cooling features and mounting geometry rather than evaluating them as isolated components. Maintaining those relationships as the product evolves reduces repeated reconstruction and manual reconciliation. 

This does not remove the specialized expertise of electrical computer-aided design (ECAD) and mechanical computer-aided design (MCAD) teams. It gives those disciplines a better common product context in which to make decisions. 

For medical device developers, that shift becomes increasingly important as physical space, electronic content and product requirements converge under strict regulatory oversight. 

See packaging problems before they become physical problems 

One of the most immediate benefits of bringing these domains together is the ability to evaluate the physical integration of the device earlier. 

Within an electronics-aware digital twin powered by Designcenter, engineering teams can assess board fit, component height, keep-outs, connector positioning and enclosure clearance using the current electronics representation. The same product context can also support thermal and structural studies. 

The goal is not to eliminate physical prototypes. It is to make those prototypes more valuable. 

Instead of using a physical build primarily to discover whether components fit together, teams have greater opportunity to identify integration risks virtually before committing to boards, tooling or prototypes—supporting ISO 13485 and FDA compliance readiness by ensuring rigorous design controls from the start. 

Preserve context when the design changes 

Finding an integration issue early is only part of the challenge. Medical device teams also need to understand what happens when the product inevitably evolves. 

A change rarely exists in isolation. That makes maintaining associations among product information increasingly valuable. 

A continuous digital thread anchored by Designcenter connects requirements, risk, design, simulation and manufacturing workflows while keeping design changes associated across product configurations and improving traceability from user needs through verification evidence. 

For the electromechanical workflow, this creates an important distinction: Data exchange moves information. A digital thread preserves context. 

As designs change, teams need to understand not only the latest geometry but also how changes affect the broader product definition. Connecting design data, changes and approvals helps maintains clearer design histories and visibility into change impact for medical audits. 

Turn virtual verification into an engineering habit 

Shift-left development becomes most valuable when virtual evaluation is not reserved for major design reviews. 

Instead, it becomes part of how everyday engineering decisions are made. A packaging decision can be evaluated against the current electronics definition in Designcenter. A change in component placement can be examined in its mechanical context. Thermal and structural studies can be informed by the same product context used to define the design. 

This is where electromechanical integration becomes something bigger than interoperability between two CAD environments. It becomes a foundation for continuously asking: 

– Does it fit? 

– Does it perform as intended? 

– What does this change affect? 

– Can we identify the issue before the cost of change rises? 

Build a development foundation that can scale with device complexity 

The value of shifting verification left extends beyond solving today’s packaging or routing problem. 

Medical device development involves requirements, risk, design, simulation, manufacturing and verification information that must stay connected as products evolve. Maintaining those connections improves traceability and supports the reuse of product knowledge across programs and variants. 

Rather than adding another point solution each time product complexity increases, R&D organizations can use Designcenter to establish a unified product context in which electrical, mechanical and other engineering decisions remain connected as the design progresses. 

This is the larger opportunity behind integrated electromechanical development: not simply exchanging information more efficiently, but creating an engineering environment in which teams can learn earlier, understand change more clearly and carry product context forward as devices evolve. 

From prototype-driven discovery to continuous engineering insight 

Physical testing will always play a critical role in medical device development. The opportunity lies in using digital engineering to answer more questions earlier so teams can approach physical testing with greater insight and confidence. 

A connected electromechanical environment like Designcenter gives teams greater opportunity to examine packaging, interfaces and performance earlier while maintaining the context surrounding design changes. Virtual prototyping, simulation and the digital twins help teams evaluate designs sooner and reduce reliance on physical prototypes for avoidable integration discovery. 

For R&D leaders, that represents an important evolution: Move discovery earlier. Preserve context longer. Use physical prototypes to validate innovation rather than uncover avoidable integration problems. 

Ready to shift electromechanical verification left? Explore how Designcenter can help connect mechanical and electrical development within a continuous digital thread at siemens.com/en-us/products/designcenter/. 

Maddie Goetze

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/stop-finding-electromechanical-problems-at-the-prototype-stage/