Products
Morris Medical Monday: Work Item type Anomaly
Welcome back to Morris Medical Monday: a weekly series for medical device development companies (and companies who are related to such companies), providing some useful information about Polario...
Welcome back to Morris Medical Monday: a weekly series for medical device development companies (and companies who are related to such companies), providing some useful information about Polarion solutions and Polarion extensions.
Today we will continue on the subject of Polarion’s MedPack extension, and have a look into MedPack’s Anomaly Work Item.
Anomaly
Description
An anomaly according to clause 5.6.8 of the IEC 62304:2006. An issue of this type contains a description of an anomaly that has been discovered during integration or a system test. It must be linked to a test and a resulting problem report.
Workflow Steps
The Anomaly Work Item uses the standard Evaluation Workflow.

Traceability & Impact
An Anomaly Work Item must be traceable to either a SW System Test Work Item or an Integration Test Work Item and has an impact on a Problem Report.
For more information on traceability and impacts, see the Traceability wiki page.
Attributes
Work Item Attributes
The following custom fields must be filled out before evaluation can be requested: None
Evaluation Attributes
The following custom fields must be filled out before evaluation can be finished and the work item can be closed:
Evaluation Checklist
The following checklist must be filled out before evaluation can be finished and the work item can be closed: None
Possible Resolutions
The following table shows the possible resolution values when the work item is closed:
For more information about Polarion’s MedPack visit our Extension Portal using following link: http://extensions.polarion.com/extensions/31-polarion-alm-medpack-iec-62304. I hope you liked this article and you will visit our Blog again when there is another Morris Medical Monday article.