Products

Insights Hub product update blog October 2022 

We empower industries to generate new insights

New in industrial IoT: Private Cloud updates, Asset Management subscriptions​, Edge Analytics and bulk ingestion of timeseries data 

Insights Hub releases deliver advanced industrial IoT capabilities and solutions that bring the physical and digital worlds closer together.   

Over the past few months, Insights Hub has unveiled enhancements such MindConnect with browsing capabilities and optimized bulk data transfers. We’re also excited to share our newly updated product documentation site

This update blog includes many of the newest and most exciting capabilities from the most recent Insights Hub releases: 

Industry solution updates 

  • Insights Hub OEE now available for Private Cloud 

Device connectivity and data integration 

  • MindConnect with device browsing capabilities 
  • Combining MindConnect and Integrated Data Lake capabilities   

Accessing and sharing IoT and non-IoT data 

  • Optimized bulk IoT data ingest 

Analytic applications, dashboarding capabilities and application development capabilities 

  • Edge Analytics 
  • Insights Hub Predict now available for Private Cloud 


Industry solution updates 

Insights Hub OEE now available for Private Cloud 

The Insights Hub OEE feature have been incorporated in Insights Hub for Private Cloud (Local Private Cloud) and will be available to all existing Insights Hub private cloud customers via regular updates. Insights Hub OEE Hub users to calculate Overall Equipment Effectiveness (OEE) and additional KPIs for lines and machines, in order to better understand the efficiency of underlying production processes and to be able to continuously improve. Additionally, it also helps the user to track the success of measures taken.  
Insights Hub OEE offers you the following core capabilities:  

  • Calculate OEE, Mean Time to Repair (MTTR), Mean Time Between Failure (MTBF) and further relevant KPIs for machines and lines  
  • Filter capabilities for timeframe, products, and orders  
  • Support of single- and/or multiproduct production systems  
  • Reason tree modelling and ability to change recorded downtime reasons afterwards  
  • Customization of OEE formulas for OEE calculation  
  • Set up production times, breaks, maintenances etc. in calendars 

Insights Hub OEE subscription supports a certain number of users and assets. Insights Hub OEE application can be further upgraded to support additional users and assets.  

More info on Insights Hub OEE can be found here: 

Insights Hub and Industrial IoT – What’s new July 2022


Device connectivity and data integration 

MindConnect with Device Browsing Capabilities 

We’re excited to announce that all MindConnect devices now have device browsing capabilities. To ensure a fast and error free configuration of data points direct out of the data servers on the industrial devices, ​we have enabled the MindConnect configuration within Asset Manager to ask the MindConnect device to read out the data structure of the industrial device. This new capability reduces the manual data modeling effort, i.e. there is more time to digest the ingested IoT data and to gain new insights. 

Already existing MindConnect adapters S7 Plus, MTConnect and IEC 61850 are now enabled with browsing capabilities (including in MindConnect Software Agent UI Plugin). Datapoint browsing “asks” the MindConnect device to read data and select meaningful variables. This means the server can be connected and asked for existing data structure. From these connections, we can generate Insights Hub data points and mappings, making the asset onboarding and datapoint configuration much easier, faster, scalable and flexible. High amounts of data can be read (and shown in a tree view) and created​, and the browsing results can be used for further enhancements, e.g. AI investigation on that data.  

Supported protocols: 

S7plus *​ 
MT connect * ​ 
IEC61850 * 

*Separate offering Advanced Driver Package​ 

Combining MindConnect with Integrated Data Lake Capabilities 

With this update, we are providing a new feature which allows users to, directly from their MindConnect devices (which might be hardware or software), upload files to the Insights Hub Integrated Data Lake. 
This opens the door for a wide range of new possibilities for users, let’s look at some examples: 

  • You can collect pictures of products on the factory line and upload them without any coding via a secure connection. These pictures can then be analyzed with AI based algorithms in Insights Hub– e.g., you could do image analysis for product quality inspection, or for trouble shooting of a machine.  

    This means that before you change something based on your shopfloor knowledge, which may or may not solve the problem, you can use digital twin apps to validate your assumptions and make sure that the solution will really solve the problem and optimizing manufacturing productivity. This quick and simple use case for both connected products and connected shopfloors is an offering unique to Insights Hub.  
  • Another fancy use case will be logfile analysis: Logfiles are typically small files created at the device level. A whole factory has a huge amount of log files. This feature helps users to upload all of them to Insights Hub, where they can be analyzed with the help of AI to detect anomalies or for troubleshooting. This will help users to quickly take advocate of log files that deliver important information needed to quickly troubleshoot and reduce downtime. 

This feature is available for MindConnect Software Agent and MindConnect IoT2050. 


Accessing and sharing IoT and non-IoT data 

Optimized bulk data ingestion of time series data 

The next update this month is around the bulk ingestion of time series data. A common use case for businesses is that huge chunks of historical data in external databases may have to be ingested in Insights Hub. The conventional ingest mechanisms have not been sufficient to carry out this activity earlier because of excessive costs and infeasible timeline, especially for customers migrating historical time series data from other databases to Insights Hub Time Series Storage.

We found a solution by upgrading our existing Bulk Data Transfer Mechanism with batch processing. Now users can reduce the cost and time of bulk time series data transfers to Insights Hub. A task that previously would have taken three months for one of our customers, who came up with this requirement, and could cost up to $300k now takes just about ten days and less than $50. This feature coincidentally is also very generic in nature and can be effectively used by any existing or probable customer having similar problems. The enhanced Time Series Bulk Ingest feature is thus instrumental for migrating “outsider data” to Insights Hub, given the substantial amounts of such historical data that users are dealing with in today’s era of ever-growing connected IIoT assets.  


Analytic applications, dashboarding capabilities and application development capabilities 

Edge Analytics 

Next up is Edge Analytics, which is an edge application that collects and preprocesses high and low frequency data, correlates the data and performs out of the box analysis as well. Additionally, custom KPI calculations can be designed using a large library of analyzing functions.​ 

Edge Analytics Engineer provides:​ 

  • Access to Edge Analytics Engineering Application​ 
  • Usage of a freemium mode to configure an Edge Device to stream up to 5 data points for a repeatable 7 days period​ 

Edge Analytics Engine provides:​ 

  • Improved asset availability through predictive maintenance​ 
  • Use of preconfigured KPIs as well as intuitive creation of customized workflows for KPI calculation ​ 
  • Data preprocessing at the edge level: analysis, aggregation, filtering – and upload of the preprocessed data to Insights Hub for display and further analysis​ 

The Engine can run on MindConnect Nano, MindConnect Software Agent or any Industrial Edge enabled device. 

Insights Hub Predict now available on Private Cloud 

We’re pleased to inform you that Insights Hub Predict has been incorporated in Insights Hub for Private Cloud (Local Private Cloud) and will be available to all existing Insights Hub private cloud customers via regular updates. With this update, we also ensure that private cloud follows the update cycle of public cloud very closely and ensure that users get unified Insights Hub experience irrespective of platform they choose. 
 
With artificial intelligence (AI) functionality, you can easily leverage time series data from IoT-connected assets and create forecast models. Implementing AI and machine learning then allows you to take advantage of a breadth of predictive capabilities and further IoT use cases, increasing the value and benefit of your connected devices. Some key features of Insights Hub Predict include: 

  • Accessible AI solutions for any skill and experience level 
  • Simple out-of-the-box implementation 
  • Easy access to data from IoT-connected assets 
  • Smart forecasting capabilities 

Insights Hub is part of Insights Hub Monitor and supports certain number of anomaly detections and forecasts as part of your capability package. This can be enhanced further by using specific add-ons.  

For more information on Insights Hub Predict, check out these blog posts: 


For complete details and availability on the new features of Insights Hub and its supporting releases, please refer to the Releases Notes, Region Table and new features presentations offered for all. 

Want to try Insights Hub for free? Start today with Insights Hub Start for Free

And, as always, hop on over to the public community and website for all things Insights Hub. 

Read our latest blog post about Insights Hub Predict in Insights Hub Start for Free. 

Carly Cohen

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/insights-hub/2023/04/17/insights-hub-product-update-blog-october-2022/