Corporate

Antara Ghosh

Antara Ghosh profile
Antara Ghosh

Do you speak waveform? Antara Ghosh does. Okay, so that’s not a language per se, though a waveform view of an integrated circuit design is, in many ways, a conversation between a future semiconductor device and the engineer who’s creating it today. So deciphering waveforms is an indispensable skill to have, especially given the increasing importance of chips to the outlook of the global economy in the years ahead. In this conversation, Ghosh, an associate director for R&D, talks about the roots of her passion for regression testing, whether computers designing computers will eventually put us all out of work, and why at least some discussion of gender stereotypes is okay.

So for mere mortals here for whom the whole chip design and verification process may be something of a mystery… What exactly is the Questa Verification Debugger tool? How is it used in chip design? And how do waveforms factor into all this?

Antara: We’re talking about what happens far upstream in the design process – way before fabrication, before tape out. A variety of our tools come into play here…simulators, emulators, formal verification software. Early on, design teams use a high-level language, maybe VHDL, to specify the functionality of a new chip or SoC at an abstract level. Next, they run these designs through various tools that take things down to lower levels of abstraction, say to the gate level or maybe register-transfer level, which can then be input into a simulator. Now let’s say the simulator indicates there’s a problem, though the designer is not sure why. That’s where Visualizer comes in. It helps users further explore and fix these problems in simulation and verification. The waveform is a representation of how signals travel through an IC over time. Just because an output at a given point in time is wrong, it doesn’t mean that’s where the problem is. Users can work with a waveform view to trace a signal back. There can be any number of problems…maybe multiple drivers are driving a single signal at the same time, creating a race condition, and there are all sorts of debugging issues with low-power designs. I’m in R&D and we’re exploring many ways to make things easier for users.

Such as…?

Antara: The perpetual question is how to make my tool faster and improve scalability, especially as we move to designs of gigantic proportions. Debugging often happens in real-time. It doesn’t matter if we can process billions of instructions flowing through a design…if a user is in our GUI and has to wait more than two seconds, the tool is useless. I’m also passionate about making regression testing and analysis more efficient. The way it works now and has for years is that chip design teams work on their designs during the day, then run their regression analysis overnight. If something fails, they start our debugging tool the next morning and look at what part of the checked-in code base caused the failure. I’m trying to figure out how we can automate the process and integrate our tool into the regression systems run by our customers. There might be some AI/ML involved, though an automated script might be enough for starters…even to just open the tool, take the user to a specific point, and save some time.

So you’re going to have computers designing computers and eventually put us all out of a job?

Antara: Ha! Hardly… I just want to make the debug engineer’s life easier. The engineers doing debugging often do that exclusively. It’s a different group of people than those who check in their code the night before. It’s massively time intensive. Currently, the industry spends 60% or even 80% of its design and verification time on debugging. Humans will be in the loop for a long while yet.

I have never seen a problem with just one solution, so the more input, the better.

– Antara Ghosh

How did you get into all this? Where does a passion for something like regression testing come from?

Antara: My father started his career as a maths teacher. Given India’s history last century, he was part of a generation that went through so much turmoil. He never could thoroughly explore his potential, though he had it in him, and he passed his passion on to me. I could spend hours doing maths, starting at a young age. I didn’t use a computer until college. I chose computer science in part because of the theoretical aspect. I fell in love with algorithms, with solving NP-hard problems…I guess you could say maths is my safe space.

How might a highly technical field like EDA benefit as more women make their way into senior roles?

Antara: There are stereotypical masculine and feminine qualities, and historically, even now, in the press coverage of very wealthy male technologists, you see outsized aggression and flamboyance being rewarded. A general stereotype attached to women is that they are more nurturing and better at listening and creating a space for sharing ideas, which is an asset in an engineering context…I have never seen a problem with just one solution, so the more input, the better.

Antara Ghosh profile 2
Antara Ghosh: “None of us fit into any box…”

Isn’t it a risk to talk about stereotypes?

Antara: None of us fit into any box, but there are differences over large numbers of people and by gender, also in terms of what is incentivized by management and culture at large. I’d say Siemens does an especially good job at celebrating diverse management styles. Perhaps I index high on classically masculine qualities…I’m logical and straightforward, and emotions make me uncomfortable. And yet, I owe a good deal of my career advancement to my line managers, all of whom have been men, and many of whom have been extraordinarily nurturing and empowering, and have always encouraged me to speak up. It’s about making space for all of us.

QUICK TAKES

Anything about you that might surprise colleagues?

I frequently daydream.

Book, music and streaming recommendations?

Book: “The Nutmeg’s Curse” by Amitav Ghosh. Music: Queen and Billie Eilish. Streaming: the BBC’s “Agatha Christie’s Poirot.”

One technology you couldn’t live without and one you wish had never been invented?

The same answer for both: my smartphone.

Best part of living where you do?

Family and culture. My roots are here in India. I can take care of my elderly family, my parents and my husband’s too. It’s reassuring to be surrounded by people with similar backgrounds…it’s very easy to make connections, maybe especially around family issues.

Wellness advice?

Regimented diet, walk and go to the gym, and for escape and relaxation…read a lot.

Geoffrey Koch
writer

Geoff Koch is a writer in Portland, Oregon.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/employee-spotlight/2023/03/07/antara-ghosh/