Thought Leadership

How big is a sheet of paper?

When I was a kid, the size of a piece of paper was described by a name, some of which were almost poetic. A “standard” working pad would be “Foolscap”, which was 13″ x 8″ – somewhat similar to the current US “Legal” size which is 14″ x 8.5″. A full Foolscap sheet was actually 17″ x 13.5″ and this was halved and trimmed for everyday use. Other sizes include “Emperor” [72″ × 48″], “Antiquarian” [53″ × 31″], “Grand Eagle” [42″ × 28.75″], “Double Elephant” [40″ × 27″], “Colombier” [34.5″ × 23.5″] and “Atlas” [34″ × 26″] and a whole load of smaller sizes. There seems to be a certain amount of fuzziness in the definitions of these archaic dimensions.

Nowadays, most countries outside of the US talk in terms of “A4” and its cousins …

The [almost] worldwide paper size standard is ISO 216. This is based on A0, which is a sheet that has an area of exactly 1 square meter, with sides on a ratio of 1 to the square root of 2 – i.e. approximately 1:1.4142. This yields dimension of approximately 841mm × 1189mm.

The system has the big advantage of scaling. If you divide an A0 sheet in two, parallel to the shortest side, you get two sheets with exactly the same aspect ratio – their size is A1. As you keep dividing, you get A2, A3, A4, A5 and so on. This also works for folding, of course. You can fold an A4 sheet to make an A5 brochure. Photocopying with enlargement/reduction is similarly straightforward.

In addition to the A series, the standard defines the B and C series of sizes. The B series are intermediate sizes based on similar mathematical relationships; B0 is 1000mm × 1414mm. The C series are for envelopes, which are designed to accommodate the A series of paper; a C4 envelope, for example, will comfortably take an A4 document without folding.

If you want all the details of the ISO standard and more on paper sizes, take a look here.

Something is a mystery to me. Given that paper size is more or less standardized, why do digital cameras have sensor sizes based on archaic ratios [i.e. that of 35mm and APS film]? Sure the 1:1.4142 ratio would make more sense?

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2013/04/11/how-big-is-a-sheet-of-paper/