Thought Leadership

There are 10 kinds of people in the world

If, like many embedded software developers, you need to work “close to the hardware”, you will want to be able to visualize the bit patterns that map on to CPU and peripheral registers. The obvious way to do this is in binary, as you can see the 1s and 0s directly. However, I do not think that I have ever seen the option, even in assembly language, to include binary constants in software. Do feel free to comment or email me if you know of examples.

When I started out with real-time programming, after I got through my Fortran phase, I worked on DEC minicomputers. As these machines originally had word sizes like 12 and 18 bits, grouping the bits into 3s and expressing values in octal was normal. A PDP-8, for example, was a “real” computer – i.e. it had a line of lights and switches on the front; the switches were grouped into 3s for mapping onto octal values. I was always comfortable with octal and could “see” the bit patterns quite intuitively.

Later on, a PDP-11 had 16 bit words, but DEC still insisted on using octal, which was rather odd – the left-most digit could only be 0 or 1. But the instruction set had 3-bit fields, which made some sense. In due course, with VAX machines, which had a 32-bit architecture, DEC gave in and started using hexadecimal like everyone else.
But I have never really quite felt at home with hex. Seeing “0x0C” does not immediately translate to “00001100” in my mind. So, for C/C++ code I wanted to fix this problem. All I need is my “binary.h” file, which contains 256 lines like this:

#define b00000000 ((unsigned char) 0x00)
#define b00000001 ((unsigned char) 0x01)
#define b00000010 ((unsigned char) 0x02)

This seems to do the job. If you would find this useful and would like a copy of the binary.h file, please email me.

It’s an old and rather geeky joke, but I like it:
There are 10 kinds of people in the world: those who understand binary and those who do not.

Sorry.

While I am on the subject of programming, you might be interested to attend a Webinar we are running on Thursday, which looks at compilers and embedded coding generally. A recording will be available after the live event.

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

More from this author

Comments

0 thoughts about “There are 10 kinds of people in the world
  • You are doing work that the compiler could do for you. Want a constant with bits 3, 5, and 17 set? Write 1 << 3 | 1 << 5 | 1 << 17. You get the idea.

  • Konrad:
    You are correct, I could do it that way – a compiler would certainly resolve that expression. But which is most readable and immediately understandable: “1 << 3 | 1 << 5 | 1 << 6” or “b01101000” ?

  • Thanks Victor. That’s an elegant approach, but I actually prefer the simplicity of mine [which can easily be extended to 16/32 bits]. Nice to have a choice.

  • One problem with your binary.h is that the constants contain a cast and therefore cannot be used in #if preprocessor directive. Code like:
    #if DATAMODE == b01101000
    /* Do something */
    #else
    #error Unsupported datamode
    #endif

    produces diagnostic “missing binary operator before token char” in GCC (surely confusing message for beginner programmers).

  • Intel’s PL/M allows binary constants (as well as octal, decimal and hex), and supports “$” as a “do nothing” separator. e.g.
    1101$0110B
    There’s the other joke: “Why do programmers get Halloween and Christmas confused?
    Because OCT31 = DEC25”

    • Good point Ed. Of course PL/M was probably the only language ever designed specifically for embedded programming. I do like that joke – thanks.

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2009/06/08/there-are-10-kinds-of-people-in-the-world/