{"id":66,"date":"2009-09-25T12:41:39","date_gmt":"2009-09-25T19:41:39","guid":{"rendered":"https:\/\/blogs.mentor.com\/nosimulation\/?p=66"},"modified":"2026-03-27T08:33:30","modified_gmt":"2026-03-27T12:33:30","slug":"unit-vs-root","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/2009\/09\/25\/unit-vs-root\/","title":{"rendered":"SystemVerilog: The finer details of $unit versus $root."},"content":{"rendered":"<p>Another installment of \u201cLongwinded Answers to Frequent SystemVerilog Questions: $root versus $unit\u201d<\/p>\n<p>Believe me \u2013 I tried to make this shorter. It\u2019s difficult for me to explain things without a historical perspective.<\/p>\n<p>Verilog was invented to be an <a href=\"http:\/\/en.wikipedia.org\/wiki\/Interpreted_language\" target=\"_blank\" rel=\"noopener\">interpreted language<\/a>. Verilog-XL was (and still is) an interpretive engine with single compilation unit use model. In an interpreted engine, all of the source code is parsed and loaded into memory. This means you have to specify all the source files of a design, including the source files of any required libraries, within a single command line before simulating.<\/p>\n<p>VCS (Verilog Compiled Simulator) continued this single compilation use model even though it compiled the code into a machine object saved on disk. Later, it introduced an incremental compile feature that only compiled certain files that needed it, but you still had to specify all the source files on the command line. This is not the same as separate compilation available in most software programming languages where source code can be converted into machine code independently.<\/p>\n<p>Tools such as NCsim and Modelsim introduced the concept of separate compilation, loosely based on the work library concept from VHDL. This is relatively easy to do in Verilog because module definitions are self contained.\u00a0 It turns out that module instantiation syntax is easy to recognize, so the compiler does not need to see the definition of module that is being instantiating beforehand. However, parameter overrides and hierarchical references limit the amount of machine code you can generate in the compilation step. The elaboration step that follows does a lot of the work of generating machine code to handle this.<\/p>\n<p>Superlog, the predecessor to SystemVerilog, was also invented as an interpreted language. It introduced the concept of $root as a global scope that allowed any kind of declaration (data types, classes, variables) along with module definitions nested in that global scope. Any uninstantiated module becomes implicitly instantiated in $root. That\u2019s fine for a single compilation unit, but you can no longer separately compile every\u00a0 module because they may have dependencies on declarations outside their scope. For example<\/p>\n<p><code>class C;<br \/>\nendclass<br \/>\nmodule top;<br \/>\nC c_h;<br \/>\nendmodule<\/code><\/p>\n<p>There\u2019s no problem if this is compiled as a single file, but if module top were to be compiled separately from the class C definition, it wouldn\u2019t know what the identifier C was supposed to represent, and wouldn\u2019t be able to parse the file.<\/p>\n<p>So the IEEE committee <em>borrowed <\/em>the concept of packages from VHDL and standardized the concept of a compilation unit. A package allows you to compile definitions in a separate step and import those definitions into another compilation step. Packages create separate namespaces for those definitions as wall as imposing compilation order dependencies.<\/p>\n<p>A compilation unit formalizes a scope that represents what is visible in a compilation step \u2013 called $unit in SystemVerilog. If you have a design that is compiled as a single compilation unit, there is really no conceptual difference between $unit and $root. However, once you have a design with multiple compilation units, then $unit represents the top level of each compilation unit, and there is nothing in $root except for the implicitly instantiated module instances. The only time you need to use $root or $unit is when a local name in the current scope hides a name in  a higher level scope. For example<\/p>\n<h4>Compilation unit 1<\/h4>\n<pre><code>function void print;\n  $display(\"comp1\");\nendfunction\nmodule mod1;<\/code><\/pre>\n<pre>  mod2 m2();\n\n function void print;\n   $display(\"mod1\");\n endfunction<\/pre>\n<pre>  initial $unit::print(); \/\/ prints \u201ccomp1\u201d\n          \/\/print() would print \u201cmod1\u201d)\nendmodule<\/pre>\n<h4>Compilation unit 2<\/h4>\n<pre><code>function void print;\n $display(\"comp2\");\nendfunction\nmodule mod2;<\/code><\/pre>\n<pre>  mod3 mod1(); \/\/ same name as top-level module\n  function void print;\n    $display(\"mod2\");\n  endfunction<\/pre>\n<pre>  initial $root.mod1.print(); \/\/ print \u201cmod1\u201d\n          \/\/ mod1.print() would print \u201cmod3\u201d\nendmodule<\/pre>\n<pre>module mod3;\n function void print;\n   $display(\"mod3\");\n endfunction\nendmodule<\/pre>\n<p>This example prints \u201ccomp1\u201d and  \u201cmod1\u201d in either order. Note that there is no way for compilation unit 1 to directly refer to anything in compilation unit 2, or the other way around.<\/p>\n<p>I hope this clears up some of the confusion between $root and $unit in SystemVerilog.<\/p>\n<p>Dave Rich<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Another installment of \u201cLongwinded Answers to Frequent SystemVerilog Questions: $root versus $unit\u201d Believe me \u2013 I tried to make this&#8230;<\/p>\n","protected":false},"author":71589,"featured_media":0,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[718,751],"industry":[],"product":[],"coauthors":[],"class_list":["post-66","post","type-post","status-publish","format-standard","hentry","category-news","tag-simulation","tag-systemverilog"],"_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/66","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/users\/71589"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/comments?post=66"}],"version-history":[{"count":1,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/66\/revisions"}],"predecessor-version":[{"id":19713,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/66\/revisions\/19713"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/media?parent=66"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/categories?post=66"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/tags?post=66"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/industry?post=66"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/product?post=66"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/coauthors?post=66"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}