{"id":19566,"date":"2025-09-26T01:31:16","date_gmt":"2025-09-26T05:31:16","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/?p=19566"},"modified":"2026-03-27T08:54:11","modified_gmt":"2026-03-27T12:54:11","slug":"from-manageability-to-3-0-unlocking-the-future-with-ucie-verification","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/2025\/09\/26\/from-manageability-to-3-0-unlocking-the-future-with-ucie-verification\/","title":{"rendered":"From manageability to 3.0: Unlocking the future with UCIe verification"},"content":{"rendered":"\n<p>The semiconductor industry is steadily moving toward multi-die integration, where chiplets from different sources are combined within a single package (known as a system in package or SiP) to deliver higher performance, scalability, and efficiency. The Universal Chiplet Interconnect Express (UCIe) standard is the backbone of this movement, offering a high-bandwidth, low-latency interconnect that enables heterogeneous chiplets to operate as one system.<\/p>\n\n\n\n<p>UCIe 2.0 introduced a major advancement: the manageability layer. This dedicated control plane ensures that chiplets can be configured, monitored, and coordinated independently of the mainband and sideband data paths. With it, designers gained a structured way to oversee discovery, initialization, and monitoring across complex topologies.<\/p>\n\n\n\n<p>Now UCIe 3.0 raises the bar once again. By adding higher data rates, runtime recalibration, priority sideband messaging, low-power sideband operation, and circular buffer transport, the standard improves both performance and efficiency. But it also increases verification complexity.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>The challenges of verifying manageability<\/strong><\/h2>\n\n\n\n<p>Verifying UCIe manageability is far from trivial. A single chiplet may contain multiple management elements and ports, and systems can scale from simple point-to-point connections to multi-hop meshes spanning several dies. Verification must ensure that each management element is instantiated, configured, and tracked accurately across the entire topology.<\/p>\n\n\n\n<p>Discovery and initialization add further complexity. Every management element must be identified and assigned a unique chiplet ID, while both front-door protocol-based flows and backdoor register accesses must be supported and validated. Routing is another critical challenge, since management transport packets (MTPs) must traverse potentially complex paths. Routing tables need to be built dynamically, updated at runtime, and verified to avoid loops or unreachable states.<\/p>\n\n\n\n<p>Beyond connectivity, transmitter and receiver rules must be validated. Transmitters are responsible for segmentation, interleaving, and flow control, while receivers handle decapsulation, reassembly, and out-of-order traffic. Any weakness at this level risks data corruption or system instability. Finally, because the manageability layer can carry multiple management protocols, such as UMAP or UDA, verification must confirm that payloads are decoded, interpreted, and enforced according to the specification.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-full is-resized\"><img loading=\"lazy\" decoding=\"async\" width=\"698\" height=\"571\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-1.png\" alt=\"\" class=\"wp-image-19567\" style=\"width:396px;height:auto\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-1.png 698w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-1-600x491.png 600w\" sizes=\"auto, (max-width: 698px) 100vw, 698px\" \/><figcaption class=\"wp-element-caption\">SiP supporting manageability<\/figcaption><\/figure><\/div>\n\n\n<h2 class=\"wp-block-heading\"><strong>Closing the verification gaps in UCIe 3.0<\/strong><\/h2>\n\n\n\n<p>As mentioned, UCIe 3.0 introduces new features that further complicate verification. Testing at 48\/64 GT\/s requires tighter timing checks, advanced equalization validation, and stress testing under jitter and skew. Runtime link recalibration must be validated during active traffic, ensuring data integrity and equalization tuning without disrupting operations.<\/p>\n\n\n\n<p>The introduction of priority sideband packets (PSTP) demands scenarios that validate pre-negotiation, interruption of normal traffic, chaining of priority messages, and seamless recovery once critical transfers are complete. Similarly, L2 sideband power-down (L2SPD) requires strict timing checks for entry and exit, ensuring that low-power transitions happen safely and that full functionality is restored on wake-up. The addition of circular buffer transport improves efficiency but requires careful validation of wraparound behavior, prevention of overflow and underflow, and protection against unauthorized access.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Next-generation verification framework<\/strong><\/h2>\n\n\n\n<p>The Questa\u2122 One Avery\u2122 UCIe Verification IP (VIP) provides a comprehensive framework purpose-built for the challenges of UCIe manageability and the new 3.0 features. At its core is a modular, class-based architecture that enables accurate modelling of management domains across a wide range of system topologies. Whether the design under test is a simple point-to-point connection or a complex multi-hop fabric with multiple chiplets, Avery VIP offers the flexibility to define management elements, assign roles such as directors or endpoints, and configure link attributes in line with the specification.<\/p>\n\n\n\n<p>Discovery and initialization are supported through both default and user-defined flows. This means the same environment can validate specification-driven initialization sequences while also exercising custom flows tailored to unique design requirements. Avery VIP supports configuration via both front-door transactions and backdoor register access, ensuring that all supported initialization paths can be thoroughly tested.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-full is-resized\"><img loading=\"lazy\" decoding=\"async\" width=\"908\" height=\"729\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-5.png\" alt=\"\" class=\"wp-image-19568\" style=\"width:357px;height:auto\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-5.png 908w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-5-600x482.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-5-768x617.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-5-900x723.png 900w\" sizes=\"auto, (max-width: 908px) 100vw, 908px\" \/><figcaption class=\"wp-element-caption\">Mult-chiplet management domain<\/figcaption><\/figure><\/div>\n\n\n<p>Routing logic is handled by a dedicated module that automatically builds and updates routing tables as discovery progresses and configuration changes occur. This module checks for table integrity, verifies reachability between management elements, and flags potential issues, such as unreachable paths or cyclic routes, early in the verification cycle.<\/p>\n\n\n\n<p>Debugging is elevated with protocol-aware visibility. Built-in MTP and MPG trackers correlate management transactions with their encapsulation layers, providing complete traceability from the management protocol all the way down to the physical link. This layered view allows verification teams to pinpoint the root cause of issues quickly, whether they stem from protocol handling, encapsulation, or physical transport.<\/p>\n\n\n\n<p>Finally, the Questa One Test Suite Configurator automates the creation of compliance suites based on DUT type, protocol layer, and feature set. Instead of requiring manual testbench scripting, teams can generate targeted test scenarios with just a few selections, ensuring coverage remains aligned with the evolving UCIe specification and significantly reducing set up effort.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-full is-resized\"><img loading=\"lazy\" decoding=\"async\" width=\"692\" height=\"244\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Picture2.png\" alt=\"\" class=\"wp-image-19569\" style=\"width:545px;height:auto\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Picture2.png 692w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Picture2-600x212.png 600w\" sizes=\"auto, (max-width: 692px) 100vw, 692px\" \/><figcaption class=\"wp-element-caption\">Questa One Test Suite Configurator<\/figcaption><\/figure><\/div>\n\n\n<p>For UCIe 3.0\u2019s new features, Avery VIP provides dedicated test capabilities. Recalibration events can be injected during live traffic to confirm uninterrupted data transfer. High-speed links are stress-tested at 48\/64 GT\/s under adverse conditions. PSTP handling is validated through scenarios that test PSTP pre-negotiation, mid-traffic interruption, chaining, and seamless resumption with full protocol compliance. L2SPD transitions are checked for strict compliance with timing requirements. Circular buffer behavior is verified across legal and illegal states to ensure both reliability and robustness.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"322\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-1024x322.png\" alt=\"\" class=\"wp-image-19570\" style=\"width:604px;height:auto\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-1024x322.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-600x188.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-768x241.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-1536x483.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-2048x643.png 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/Figure-9-900x283.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Handling of PSPT<\/figcaption><\/figure><\/div>\n\n\n<p>Together, these capabilities form a robust foundation for managing the dual challenge of validating UCIe manageability features and ensuring readiness for the advanced requirements of UCIe 3.0.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Why verification matters<\/strong><\/h2>\n\n\n\n<p>As UCIe continues to evolve, verification is becoming the key enabler for adoption. Without scalable, protocol-aware verification, the risk of hidden errors rises, threatening the interoperability and reliability that multi-die systems depend on. With its blend of automation, targeted test suites, and advanced debugging, the Questa One Avery UCIe VIP bridges the gap between the UCIe specification and silicon-ready confidence.<\/p>\n\n\n\n<p>By covering both manageability and UCIe 3.0\u2019s new performance and power features, this framework ensures that design teams can keep pace with the standard\u2019s rapid evolution and bring next generation chiplet systems to market with confidence.<\/p>\n\n\n\n<p>To explore the full details, download the whitepaper:<br><a href=\"https:\/\/resources.sw.siemens.com\/en-US\/white-paper-verifying-the-evolving-ucie-landscape\/\" target=\"_blank\" rel=\"noreferrer noopener\">Verifying the Evolving UCIe Landscape: A 3.0-Aware Architecture for Manageability and Beyond<\/a><\/p>\n\n\n\n<p><\/p>\n","protected":false},"excerpt":{"rendered":"<p>The semiconductor industry is steadily moving toward multi-die integration, where chiplets from different sources are combined within a single package (known as a system in package or SiP) to deliver higher performance, scalability, and efficiency. The Universal Chiplet Interconnect Express (UCIe) standard is the backbone of this movement, offering a high-bandwidth, low-latency interconnect that enables heterogeneous chiplets to operate as one system.<\/p>\n<p>UCIe 3.0 raises the bar once again. By adding higher data rates, runtime recalibration, priority sideband messaging, low-power sideband operation, and circular buffer transport, the standard improves both performance and efficiency. But it also increases verification complexity.<\/p>\n","protected":false},"author":105326,"featured_media":19573,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1,1634],"tags":[],"industry":[53],"product":[1593],"coauthors":[1616,1619],"class_list":["post-19566","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","category-avery-vip","industry-electronics-semiconductors","product-avery"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2025\/09\/ujjwal.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/19566","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/users\/105326"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/comments?post=19566"}],"version-history":[{"count":3,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/19566\/revisions"}],"predecessor-version":[{"id":19623,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/19566\/revisions\/19623"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/media\/19573"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/media?parent=19566"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/categories?post=19566"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/tags?post=19566"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/industry?post=19566"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/product?post=19566"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/coauthors?post=19566"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}