{"id":15951,"date":"2021-03-22T14:15:00","date_gmt":"2021-03-22T18:15:00","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/?p=15951"},"modified":"2026-03-27T08:47:47","modified_gmt":"2026-03-27T12:47:47","slug":"cocotb-bus-functional-models","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/2021\/03\/22\/cocotb-bus-functional-models\/","title":{"rendered":"Cocotb Bus Functional Models"},"content":{"rendered":"\n<p>In this series we&#8217;re talking about using Python as the testbench software in this testbench diagram:<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"405\" height=\"171\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/02\/Proxy-Testbench-1.png\" alt=\"Proxy-driven testbench\" class=\"wp-image-15808\"\/><figcaption>BFM-driven Testbench<\/figcaption><\/figure>\n\n\n\n<p>The testbench software uses blocking Python function calls to interact with the bfm and eventually the bus functional models (BFMs). In this example we&#8217;re going to look at a testbench for a simple design: the TinyALU.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"668\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/03\/Cocotb-Proxy.png\" alt=\"TinyALU and its BFMs\" class=\"wp-image-15952\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/03\/Cocotb-Proxy.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/03\/Cocotb-Proxy-600x391.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/03\/Cocotb-Proxy-768x501.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/03\/Cocotb-Proxy-900x587.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption>The TinyALU and BFMs<\/figcaption><\/figure>\n\n\n\n<p>The example above shows three bus functional models (BFMs).  A driver, a command monitor, and a result monitor.  These provide three functions for our testbench software:<\/p>\n\n\n\n<ul class=\"wp-block-list\"><li><code>send_op(A, B, op)<\/code>\u2014Sends a command to the ALU and blocks if the ALU is busy.<\/li><li><code>get_cmd()<\/code>\u2014Gets commands in the order they appeared at the TinyALU and blocks if there is none available.<\/li><li><code>get_result()<\/code>\u2014Gets results in the order they appeared at the TinyALU.<\/li><\/ul>\n\n\n\n<p>We&#8217;ll create a Python class named <code>TinyAluBfm<\/code> that implements the BFMs. Before we show the code in Python, let&#8217;s look at the result monitor written in SystemVerilog. Let&#8217;s assume we have an interface named <code>dut<\/code> and a <code>result_queue<\/code>.  We could write our SystemVerilog BFM like this:<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>task done_bfm();\n   prev_done = 0;\n   forever begin\n       @(negedge clk)\n       done = dut.done;\n       if (done == 1 and prev_done == 0)\n           result_queue.push_back(dut.result);\n       prev_done = done;\n   end\n endtask;<\/code><\/pre>\n\n\n\n<p>This task loops indefinitely and waits at the negative edge of the clock.  At each clock it looks at <code>done<\/code>. If done is high and <code>prev_done<\/code> is low then we push <code>dut.result<\/code> into the queue.<\/p>\n\n\n\n<p>How do we write this in <strong>cocotb<\/strong>? <\/p>\n\n\n\n<h2 class=\"wp-block-heading\">The Result Monitor BFM<\/h2>\n\n\n\n<p>We&#8217;re going to create a bfm class that contains the BFMs and the associated queues and access functions.  We import resources from <strong>cocotb<\/strong> and then start with a class declaration:<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>from cocotb.triggers import FallingEdge\nfrom cocotb.queue import QueueEmpty, Queue\nimport cocotb\nimport enum\nimport random\n\nclass TinyAluBfm:\n    def __init__(self, dut):\n        self.dut = dut\n        self.driver_queue = Queue(maxsize=1)\n        self.cmd_mon_queue = Queue(maxsize=0)\n        self.result_mon_queue = Queue(maxsize=0)<\/code><\/pre>\n\n\n\n<p><\/p>\n\n\n\n<p>The <code>TinyAluBfm<\/code> above has three queues that will store data.  Now we create the <code>get_result()<\/code> coroutine:<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>    async def get_result(self):\n        result = await self.result_mon_queue.get()\n        return result<\/code><\/pre>\n\n\n\n<p>That&#8217;s all there is to that. This coroutine returns the results in the order the TinyALU generated them, and blocks if the queue is empty.<\/p>\n\n\n\n<p>Now we need to fill the queue using a BFM written with a coroutine.  Notice that we were passed a <code>dut<\/code> object in the <code>__init__()<\/code> method. This object is analogous to a SystemVerilog interface. It gives us access to the DUT&#8217;s top -level signals.  Now we can recreate the SystemVerilog result monitor in Python:<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>    async def result_mon_bfm(self):\n        prev_done = 0\n        while True:\n            await FallingEdge(self.dut.clk)\n            try:\n                done = int(self.dut.done)\n            except ValueError:\n                done = 0\n\n            if done == 1 and prev_done == 0:\n                result = int(self.dut.result)\n                self.result_mon_queue.put_nowait(result)\n            prev_done = done<\/code><\/pre>\n\n\n\n<p>Here we see the same code as SystemVerilog.  We loop forever and <code>await FallingEdge(self.dut.clk)<\/code>. This is the same as <code>@(negedge dut.clk)<\/code>. The <code>FallingEdge<\/code> coroutine came from <strong>cocotb<\/strong> which provides a <a href=\"https:\/\/docs.cocotb.org\/en\/stable\/triggers.html\" target=\"_blank\" rel=\"noopener\">variety of triggers<\/a> such as <code>Edge<\/code>, <code>RisingEdge<\/code>, and <code>FallingEdge<\/code>.  You can also ask cocotb to count a number of clocks as we&#8217;ll see below.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">The TinyALU Driver BFM<\/h2>\n\n\n\n<p>We send commands to the TinyALU with the <code>send_op()<\/code> function and associated driving BFM.<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>    async def send_op(self, aa, bb, op):\n        await self.driver_queue.put((aa, bb, op))<\/code><\/pre>\n\n\n\n<p>In this example send_op() is a coroutine because we&#8217;ll be calling it from a coroutine.  If we were calling it from another Python thread then we&#8217;d make it a simple function.  We put two operands an an operation into the <code>driver_queue<\/code> where the driver BFM will retrieve it.<\/p>\n\n\n\n<p>Here is the driver BFM. As with the monitoring BFM we create a state machine and here we see a <strong>cocotb<\/strong> requirement. The coroutines cannot block, otherwise they hang the testbench and even the simulator. So, in this example we wait for the falling edge of the clock and try to get data from the queue with <code>get_nowait()<\/code>. If <code>driver_queue<\/code> is empty then <code>get_nowait() <\/code>raises a <code>queue.Empty<\/code> exception. We catch the exception with the <code>except<\/code> statement and execute a <code>pass<\/code> statement, which does nothing. Then we loop to the top and wait for the next clock edge.:<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>    async def driver_bfm(self):\n        self.dut.start &lt;= 0\n        self.dut.A &lt;= 0\n        self.dut.B &lt;= 0\n        self.dut.op &lt;= 0\n        while True:\n            await FallingEdge(self.dut.clk)\n            if self.dut.start.value == 0 and self.dut.done.value == 0:\n                try:\n                    (aa, bb, op) = self.driver_queue.get_nowait()\n                    self.dut.A = aa\n                    self.dut.B = bb\n                    self.dut.op = op\n                    self.dut.start = 1\n                except QueueEmpty:\n                    pass\n            elif self.dut.start == 1:\n                if self.dut.done.value == 1:\n                    self.dut.start = 0<\/code><\/pre>\n\n\n\n<p>If we get data to send to the TinyALU, we put it on the appropriate signals and raise the <code>start<\/code> signal. This state machine waits to see the <code>done<\/code> signal go high before lowering <code>start<\/code>.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">The cocotb Test<\/h2>\n\n\n\n<p>Tests in cocotb are coroutines decorated with the <code>@cocotb.test<\/code> decorator. When we run a simulation with <strong>cocotb<\/strong> it searches any number of Python files for decorated functions and runs them as tests.  Here is our TinyALU test. The test creates a <code>TinyAluBfm<\/code> object and uses it to start up the BFM coroutines and reset the DUT:<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>async def test_alu(dut):\n    clock = Clock(dut.clk, 2, units=\"us\")\n    cocotb.fork(clock.start())\n    bfm = TinyAluBfm(dut)\n    await bfm.startup_bfms()\n<\/code><\/pre>\n\n\n\n<p>Launching the BFMs<\/p>\n\n\n\n<p>The code above <code>await<\/code>ed teh <code>startup_bfms()<\/code>` coroutine. Here is how that coroutine reset the DUT and forked off the BFM coroutines.<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>    async def startup_bfms(self):\n        await self.reset()\n        cocotb.fork(self.driver_bfm())\n        cocotb.fork(self.cmd_mon_bfm())\n        cocotb.fork(self.result_mon_bfm())<\/code><\/pre>\n\n\n\n<p>Now the BFMs are running we can write a test.  We wait for the falling edge of the clock, then we send <code>`0xAA + 0x55<\/code> command to the TinyALU.  The result is <code>0xFF<\/code>. We check that our result was correct.<\/p>\n\n\n\n<pre class=\"wp-block-code\"><code>    await FallingEdge(dut.clk)\n    await bfm.send_op(0xAA, 0x55, 1)\n    await cocotb.triggers.ClockCycles(dut.clk, 5)\n    cmd = await bfm.get_cmd()\n    result = await bfm.get_result()\n    print(\"cmd:\", cmd)\n    print(\"result:\", result)\n    assert result == 0xFF<\/code><\/pre>\n\n\n\n<p>We see the following in the output:<\/p>\n\n\n<p># cmd: (170, 85, 1)<br \/>\n# result: 255<br \/>\n#  19000.00ns INFO     Test Passed: test_alu<\/p>\n\n\n\n<p>Our BFM works!<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">Next Step<\/h2>\n\n\n\n<p>In this blog post we learned how to create a simple BFM with <strong>cocotb<\/strong> and create functions that deliver the data to testbench software. One can write a testbench from this point that builds upon these ideas.<\/p>\n\n\n\n<p>However, this give us a reuse problem in that engineers will write widely different testbenches without a common methodology such as the UVM in the SystemVerilog world.<\/p>\n\n\n\n<p>If only we had a UVM for Python . . . and it turns out that we do. <strong><a href=\"https:\/\/github.com\/pyuvm\/pyuvm\" target=\"_blank\" rel=\"noopener\">pyuvm<\/a><\/strong> is a Python implementation of the UVM specification IEEE 1800.2 that can use <strong>cocotb<\/strong> to connect to a simulation. We&#8217;ll turn to <strong>pyuvm<\/strong> in the next blog post.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>In this series we&#8217;re talking about using Python as the testbench software in this testbench diagram: The testbench software uses&#8230;<\/p>\n","protected":false},"author":74314,"featured_media":15952,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[984,1,981,10],"tags":[],"industry":[],"product":[],"coauthors":[947],"class_list":["post-15951","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-cocotb","category-news","category-pyuvm","category-tips-tricks"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/54\/2021\/03\/Cocotb-Proxy.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/15951","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/users\/74314"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/comments?post=15951"}],"version-history":[{"count":4,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/15951\/revisions"}],"predecessor-version":[{"id":16577,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/posts\/15951\/revisions\/16577"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/media\/15952"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/media?parent=15951"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/categories?post=15951"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/tags?post=15951"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/industry?post=15951"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/product?post=15951"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/verificationhorizons\/wp-json\/wp\/v2\/coauthors?post=15951"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}