{"id":2855,"date":"2019-12-18T08:49:25","date_gmt":"2019-12-18T13:49:25","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/?p=2855"},"modified":"2026-03-26T12:02:12","modified_gmt":"2026-03-26T16:02:12","slug":"what-if-santa-built-an-electric-autonomous-sleigh","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/what-if-santa-built-an-electric-autonomous-sleigh\/","title":{"rendered":"What if Santa built an electric, autonomous sleigh?"},"content":{"rendered":"\n<p>Christmas Eve is always a special, if exhausting, day each\nyear for Santa Claus. Delivering gifts to children around the world in less\nthan 24 hours is a lot of work. So this year, Santa had an idea to make his\nholiday duties less stressful for him and his reindeer: using vehicle\nelectrification and autonomous driving technology.<\/p>\n\n\n\n<p>By partnering with Siemens, Santa developed an ambitious\nplan to exponentially boost the efficiency of his worldwide gift delivery\noperation.<\/p>\n\n\n\n<p>Here\u2019s how Santa Claus and his team did it:<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Electrification of\nthe sleigh<\/strong><\/h2>\n\n\n\n<p>Where could Santa maximize efficiency? While Santa\u2019s\nreindeer are amazing at their jobs, he doesn\u2019t want to overwork them. So, he considered\nways to minimize the burden of flying on his reindeer. His first thought was\nthrough electrification. But, how could he build an electric sleigh with optimal\nperformance and a large enough range?<\/p>\n\n\n\n<p>Santa gathered his best engineering elves and tasked them\nwith designing, developing and electrifying his cherry red sleigh. The elves knew\nthat every function and feature in an electric vehicle needed to be electrified\nand controlled by <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/webinar\/vehicle-electrification-perform-eng-simulation\/42101\" target=\"_blank\" rel=\"noopener\">software<\/a>.<\/p>\n\n\n\n<p>They chose to simulate, validate and verify the capabilities\nof the sleigh, make necessary changes and then ensure all the engineering teams\nhad the latest iterations at their fingertips. Getting to full electrification takes\na lot of virtual design and analysis, but the benefits were well worth the effort.\nThey were able to develop a re-envisioned sleigh more quickly with simulation\nthen show how a variety of conditions including headwinds, cold weather,\naltitude, acceleration, weight of presents, and a dash of reindeer magic, would\nimpact <a href=\"https:\/\/blogs.sw.siemens.com\/thought-leadership\/future-electric-cars-must-focus-on-battery-architecture-development\/\">battery\nperformance<\/a>.<\/p>\n\n\n\n<p>With the electrification of the sleigh complete, Santa\nturned his attention to other opportunities to make his deliveries more\nefficient.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>The autonomous sleigh<\/strong><\/h2>\n\n\n\n<p>Santa then considered the idea of making his sleigh fully autonomous.\nThe autonomy of the sleigh allowed him to focus less on steering and more on\nhigher value tasks, such as organizing the presents.<\/p>\n\n\n\n<p>The new design incorporated special light detection and ranging\n(LIDAR), radar and camera sensors. These sensors will capture sensor data as\nthe sleigh travels across the sky and landing on countless roofs around the\nworld.<\/p>\n\n\n\n<p>The data from each sensor feeds into an innovative\nautonomous driving platform based in the North Pole workshop. The result is a\nconsistent, high resolution, 360-degree view of the sleigh\u2019s surroundings. The\nsleigh\u2019s driving decision AI algorithms and steering actuators nimbly navigate\nthe vehicle as it travels autonomously across the globe.<\/p>\n\n\n\n<p>Once the self-driving sleigh prototype was perfected, Santa wanted\nto ensure safety and that the sleigh would operate as designed. So, Santa\u2019s\nengineers looked at super computer-class simulation of the sleigh and environment\nso to minimize the need for extensive physical prototyping. This dramatically\nreduced the need for hundreds of millions of logged test miles necessary to\ndemonstrate the safety of the sleigh. The right simulation platform produced\nhighly realistic, physics-based simulations of an unlimited number of potential\nflying situations and other parameters. Santa can now rely on an autonomous\nflying system that can travel safely to its destination and land on a variety\nof rooftops without worrying about a single glass of spilled milk.<\/p>\n\n\n\n<p>Santa could see it all coming together, but he was not quite\nsatisfied with its efficiency. It was time to design one more time-saving feature.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>The last mile of\ndelivery<\/strong><\/h2>\n\n\n\n<p>Santa has millions of chimneys to descend and presents to put\nin place. While all that work is rewarding, it is also time-consuming. So, having\nimplemented autonomous applications for the sleigh, Santa decided to automate\nthe <a href=\"https:\/\/blogs.sw.siemens.com\/thought-leadership\/last-mile-delivery-paves-for-way-electrified-autonomous-vehicles\/\">last\nmile of delivery<\/a>.<\/p>\n\n\n\n<p>Imagine Santa\u2019s sleigh landing on a single roof in your neighborhood,\nthen deploying tiny autonomous vehicles, or mini sleighs, to deliver presents\nto all the houses in the area at once.<\/p>\n\n\n\n<p>Santa can dramatically reduce average delivery time and the\nelves loved this idea.<\/p>\n\n\n\n<p>Testing of the new deployment process in the North Pole\ncommenced. During live experiments, the complex prototypes were tasked with identifying\nand encountering many hazardous situations \u2014 an active fireplace, children who\nare awake, dogs barking and more. This information was then used to create\nre-useable and configurable software simulation scenarios. Sleigh-to-sleigh and\nsleigh-to-city analytics were automatically determined for best routing\ndecisions, ensuring children are asleep before delivering presents and whether\nbattery power will be sufficient to cover the route to the destination and back\nto the sleigh where they could recharge. <\/p>\n\n\n\n<p>Analytics can now be used to improve fleet utilization and provide\ninsight so that the Christmas delivery program remains efficient and presents\nare delivered on-time.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>What\u2019s Santa doing?<\/strong><\/h2>\n\n\n\n<p>Even with all this automation and analytics, Santa remains the\nman in charge, and will be ready to take the reins, if needed. Meanwhile, he is\nfocusing on other aspects of the present-delivery system, such as ensuring\nample room on his sleigh for more presents, checking his digitalized lists thrice\nand having the freedom to watch his state-of-the-art system work autonomously with\nhis feet propped up smoking his pipe. <\/p>\n\n\n\n<p>With the help of comprehensive digital twin technology,\nautomation and analytics tools, Santa has accomplished his off-season goal of\nbuilding an autonomous, electric sleigh and creating a more efficient system\nwhen delivering presents around the world.<\/p>\n\n\n\n<p>Happy Holidays to all from Siemens!<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Christmas Eve is always a special, if exhausting, day each year for Santa Claus. Delivering gifts to children around the&#8230;<\/p>\n","protected":false},"author":69235,"featured_media":2856,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[],"industry":[],"product":[],"coauthors":[],"class_list":["post-2855","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/19\/2019\/12\/Santa-Autonomous-Electric-Sleigh.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/posts\/2855","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/users\/69235"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/comments?post=2855"}],"version-history":[{"count":1,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/posts\/2855\/revisions"}],"predecessor-version":[{"id":2857,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/posts\/2855\/revisions\/2857"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/media\/2856"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/media?parent=2855"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/categories?post=2855"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/tags?post=2855"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/industry?post=2855"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/product?post=2855"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/thought-leadership\/wp-json\/wp\/v2\/coauthors?post=2855"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}