{"id":840,"date":"2020-03-30T09:36:05","date_gmt":"2020-03-30T16:36:05","guid":{"rendered":"http:\/\/blogs.mentor.com\/tessent\/?p=840"},"modified":"2026-03-26T16:05:44","modified_gmt":"2026-03-26T20:05:44","slug":"a-leap-forward-for-in-system-test-for-automotive-ics","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/tessent\/2020\/03\/30\/a-leap-forward-for-in-system-test-for-automotive-ics\/","title":{"rendered":"A leap forward for in-system test for automotive ICs"},"content":{"rendered":"<p><em>An improvement to BIST improves test coverage and time to improve functional safety of automotive ICs<\/em><\/p>\n<p><!--more-->The growth of electronics in automobiles has spurred significant innovation in the development of advanced safety mechanisms for all the electrical and electronic systems in a vehicle. In addition to very high-quality manufacturing test, ICs for safety-critical applications need in-system test to detect faults and monitor circuit aging. Scan-based logic built-in-self-test (LBIST) is the technique used for in-system test, but traditional LBIST often can\u2019t meet the coverage goals within the required diagnostic test time interval (DTTI).<\/p>\n<p><a href=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/48\/2020\/03\/LBIST-OST-dtti.jpg\"><img loading=\"lazy\" decoding=\"async\" class=\"alignnone size-medium wp-image-841\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/48\/2020\/03\/LBIST-OST-dtti-520x263.jpg\" alt=\"\" width=\"520\" height=\"263\" \/><\/a><\/p>\n<p>Designers need an LBIST solution that allows them to meet 90% fault coverage within the DTTI required, without adding to the area overhead. A new LBIST technology that dramatically improves the efficiency of in-system test has been proven out by major automotive IC design houses. The new LBIST technology is called LBIST-OST (Logic BIST with Observation Scan Technology).<\/p>\n<p>In a recent Tech Talk with Semiconductor Engineering, Mentor automotive product manager Mohammed Abdelwahid talks about how to maximize coverage in the different ASIL standards for logic BIST,\u00a0 how to make testing more efficient, and what impact that has on area and test time. You can watch that video <a href=\"https:\/\/www.youtube.com\/watch?v=O3I_9umvDf8\/?cmpid=10595\" target=\"_blank\" rel=\"noopener noreferrer\">here<\/a><\/p>\n<h4>LBIST for in-system test<\/h4>\n<p>LBIST is widely used for in-system test to detect faults that could violate safety goals. However, the pseudo-random nature of LBIST poses a challenge to automotive IC designers it simply cannot meet the coverage goal within the assigned DTTI. Reaching the coverage goal of 90% for Automotive Safety Integrity Level (ASIL) D certification might involve increasing the LBIST to a point where the area overhead makes the chip unviable from a cost perspective.<\/p>\n<p>The pseudo-random nature of LBIST is not the only challenge to DTTI; another impediment is that fault detection happens only during the capture phase of the LBIST cycle. Each LBIST cycle has two phases\u2014shift and capture. There are as many shift cycles as the length of the longest scan chain. The capture phase uses the values written into the scan chain to drive the combinational logic and capture potential faults. That means all the time spent on the shift phase is time faults are not being detected. What if you could observe circuit responses during those shift cycles? It greatly improves the overall observability of the design.<\/p>\n<h4>Better LBIST with Observation Scan Technology (OST)<\/h4>\n<p>Control and observe test points improve LBIST random-pattern test coverage. In the LBIST-OST architecture, an LFSR on the input side operates as a decompressor in ATPG, and as a pseudo-random pattern generator in LBIST mode. On the output side, a spatial compactor drives channel pins during ATPG, and drives the MISR in LBIST mode.<\/p>\n<p>Unlike traditional test points, the LBIST-OST observe points use a new scan cell functionality that essentially connects the observe points in separate chains. This allows them to capture circuit responses not just during a capture cycle, but also during the shift cycles.<\/p>\n<p><a href=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/48\/2020\/03\/LBIST-OST-architecture.jpg\"><img loading=\"lazy\" decoding=\"async\" class=\"alignnone size-medium wp-image-842\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/48\/2020\/03\/LBIST-OST-architecture-520x238.jpg\" alt=\"\" width=\"520\" height=\"238\" \/><\/a><\/p>\n<p>LBIST-OST technology leverages test points to reduce the DTTI by increasing the fault detection period, delivering up to 10x faster in-system test than traditional LBIST and reduces the number of test patterns needed.<\/p>\n<p>For ICs that need to meet ISO 26262 and achieve ASIL D certification, in-system test is a requirement. Designers can reduce in-system test time (DTTI) and area overhead using LBIST-OST. Observation scan completes tests faster, thereby simplifying key-on, key-off, and periodic checkups during functional operation.<\/p>\n<p><a href=\"http:\/\/bit.ly\/1hf2bMq\" target=\"_blank\" rel=\"noopener noreferrer\"><img loading=\"lazy\" decoding=\"async\" class=\"alignnone wp-image-61 size-full\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/48\/2015\/09\/LinkedIn-Button.jpg\" alt=\"\" width=\"300\" height=\"70\" \/><\/a><\/p>\n","protected":false},"excerpt":{"rendered":"<p>An improvement to BIST improves test coverage and time to improve functional safety of automotive ICs<\/p>\n","protected":false},"author":71644,"featured_media":0,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[],"industry":[],"product":[],"coauthors":[],"class_list":["post-840","post","type-post","status-publish","format-standard","hentry","category-news"],"_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/posts\/840","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/users\/71644"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/comments?post=840"}],"version-history":[{"count":1,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/posts\/840\/revisions"}],"predecessor-version":[{"id":2392,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/posts\/840\/revisions\/2392"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/media?parent=840"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/categories?post=840"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/tags?post=840"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/industry?post=840"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/product?post=840"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/tessent\/wp-json\/wp\/v2\/coauthors?post=840"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}