Solid Edge is a portfolio of affordable, easy-to-use software tools that address all aspects of the product development process.
Solid Edge is part of Siemens Xcelerator, the comprehensive and integrated portfolio of software, hardware, and services that provides an innovative approach to product development.Choose an option from the list to learn what Solid Edge can do for you!
Drawings are the final deliverable for many engineering processes—they represent a contract between design and manufacturing, which means that accuracy is critical. But as product designs and assemblies become more complex, and with a host of global drawing standards to consider, creating, annotating, and updating drawings can be a challenge. With Solid Edge, drawing layout, detailing, annotation, and dimensioning controls automatically comply with the mechanical drafting standard you select.
|
With Solid Edge, we have significantly reduced the time required to complete product designs, with automatic drawing creation and BOM generation playing a key role here. |
|
|
Bala Kannan Manager of Design & Engineering at Summits Hygronics |
3D design enables faster time to market while reducing engineering costs. Solid Edge 3D design is distinguished by its ability to provide superior part and assembly modeling, flexible drafting, best-in-class sheet metal capabilities, and industry-leading visualization. These attributes enable Solid Edge to deliver a fast and flexible design experience while easing the challenges inherent in product development. With synchronous technology to help you accelerate product design, make revisions faster, and improve design data re-use, Solid Edge lets you design at the speed of creative thought.
|
Solid Edge with synchronous technology accelerates the entire design process. The software can be used to read and edit the data produced by all 3D software, which enables exceptionally fast and accurate modeling and change management. |
|
|
Zhang Mingtian Assistant Manager of Engineering and Technical Department at Precision Timer |
Solid Edge streamlines the entire sheet metal product development process, from CAD design through flat pattern and drawing development, to meet unique sheet metal design challenges like manufacturability.
|
Solid Edge meets our expectations both in terms of sheet metal results and processing speed. Models can now be unfolded anywhere, and streamlined sequences lead to more flexible and faster sheet metal processing. |
|
|
Liu Huakung Chairman at Taiwan Fylin |
Industrial design is used to create product value. Designs that are visually appealing, while also being functional and manufacturable, give companies a competitive advantage. Solid Edge includes advanced shape creation and manipulation capabilities that aid in the conceptualization of unique products, letting your products stand out in a crowded market.
|
Innovation is the core of what we do. Our ideas are realized using Solid Edge, which helps our designers to work quickly and efficiently. We are particularly satisfied with the functions of synchronous modeling for easy editing without the need to edit sketches every time. |
|
|
Gustav Kågesson Design Manager at NP Innovation |
As designs become more complex, the number of parts in an assembly often grows. Solid Edge helps you quickly and easily create and manage even the largest assemblies, without lags or crashes. Create exact representations of all components—including tubes, pipes, wires, weldments, and sheet metal—in a complete digital mockup that allows for more accurate design and analysis. Solid Edge helps you quickly detect and fix clash and interference issues, generate assembly instructions, and conduct customer reviews—reducing the need for costly prototypes.
|
Solid Edge has assisted us greatly in ensuring that we go from design to production without time-consuming and costly prototyping stages. While every product is different, I can safely say that by using Solid Edge we now deliver a working solution more than twice as fast as we did before. |
|
|
James Reid Owner of Red Ant Agri Engineering |
Solid Edge Model Based Definition enables the production of a complete digital definition of parts and/or assemblies using a 3D model, moving users to a fully digitalized manufacturing and design environment. Annotated 3D models are far easier to understand than complex drawings, which reduces time spent on engineering documentation and drives downstream validation and manufacturing efforts. This can result in a paperless design office that provides less amendment work, faster time to manufacturing, quicker documentation, and clearer manufacturing communication.
|
Using Solid Edge, I can handle the many changes and variants that occur in the design process much faster than in the past. The possibility to model parts within an assembly, as well as the integrated data management functions, offer a big advantage. |
|
|
Jens Schneider Chief Designer at Grossmann Uhren |
From rudimentary 2D pipe planning to full-scale 3D piping systems, Solid Edge modular plant design solutions streamline workflow processes. Linked 3D piping, support for piping and instrumentation diagrams (P&ID), and Isogen® output ensure that your products are designed right—the first time, and every time. These software modules allow users to easily capture design intent/logic in a 2D schematic, then develop 2D P&IDs into a comprehensive 3D model of a process plant.
|
Because the company’s products are modular systems, the assembly-oriented design capabilities of Solid Edge enabled ProMinent engineers to easily design layouts of system modules, and the drafting tools simplified their conversion to 2D drawings that document the designs for production, assembly and installation. |
|
|
ProMinent |
Solid Edge helps you overcome electromechanical design challenges with a dedicated solution for electrical design—enabling true co-design collaboration across electrical and mechanical domains. Based on industry-leading technology, our electrical design products are trusted and proven around the world.
|
[Our machines] were designed using Solid Edge, which helped the integration of the electronic design, reduction of the physical prototyping and enabled simulated testing scenarios. |
|
|
Brian Howes Lead Mechanical Design Engineer at Mecmesin |
The industry’s most powerful PCB layout technology combines ease of use with highly automated functionality to give engineers exceptional control over designs. Groundbreaking sketch router technology combines routing power with user control during interactive editing operations, producing high-quality results with exceptional performance.
|
With the help of Solid Edge, WashTech has accelerated and improved its overall product development process. The company designs wiring circuits 60% faster, their assembly process is 20% faster, and product testing costs are down 57%. |
|
|
WashTech |
Using the industry standard Simcenter Nastran solver, Solid Edge Simulation delivers structural simulation results, such as identifying deformation, stress and strain, etc. caused by a static loading, finding the natural frequencies of vibration, or determining buckling loads of a design. Steady and transient heat transfer analysis validates cooling performance by evaluating the temperature distribution of the model. In addition, the coupled thermal and structural analysis can be applied to determine thermal effects to the structural stress/strain.
|
Solid Edge has enabled product development breakthroughs in our company. With 3D animation and simulation, I can be fairly certain whether a new idea is practicable without even leaving my chair. |
|
|
Chen Yongming VP of Toong-woei |
Fully embedded in Solid Edge, Simcenter FLOEFD for Solid Edge extends the power of CAD environments to computational fluid dynamics (CFD) analysis, optimizing product performance and reliability for fluid flow, heat transfer and electromagnetic effects. A fast, flexible, and accurate solution for modeling thermo-fluid systems, Simcenter Flomaster for Solid Edge automatically creates a model based on CAD data, aiding in the computation and visualization of flow velocity, temperature, and pressure drop in pipe works in a 1D environment.
|
With Solid Edge and Simcenter FLOEFD, we have increased the fuel cell’s efficiency by more than 10 percent and reduced platinum content by a factor of 10, decreasing the weight and volume of the entire system to 30 percent of the original design. |
|
|
Juan Alvarez Founder and CEO of JALVASUB Engineering |
Solid Edge allows you to take full advantage of additive manufacturing, whether you are creating individual prototypes or manufacturing larger volumes of components. Our tools support your end-to-end workflow, from design-for-manufacture using additive techniques, to preparing and outputting your designs to 3D printing hardware and services.
|
The use of Solid Edge to manage the entire product lifecycle delivered the expected good results. We are excited about the new product development with a drastic reduction of errors, costly rework, and timelines. |
|
|
Sushilkumar General Manager of Operation and Engineering at NGCT Cleansys |
Avoid the need for, and the cost of, multiple CAM systems in the machine shop with Solid Edge CAM Pro. This scalable solution offers a wide range of in-depth NC programming capabilities, providing flexibility and maximizing the value of your investment. In addition to the 2.5-axis milling capabilities included with Solid Edge Classic, Foundation, and Premium active maintenance contracts, CAM Pro is available in 2.5-axis, 3-axis, and 5-axis bundles. These configurations, along with numerous add-on functionalities, allow you to customize a right-sized solution to meet your individual manufacturing needs.
|
One of the most obvious consequences since we began programming with Solid Edge CAM Pro is the speed. For example, programming one part that requires 20 drills at the foot of the machine could have taken me an hour. Now it takes me 10 minutes. |
|
|
Borja Fernández Technician in Charge of Machine Programming at LCN Mecánica |
The ability to clearly communicate the correct manufacturing, installation, and maintenance procedures for your designs is essential to the performance of your products and the success of your business. Using Solid Edge technical publications solutions, designers can quickly create many types of technical documents—from simple illustrations for end-user manuals to interactive 3D technical documents for manufacturing and service. You can reduce the need for specialist technical authors or external services and produce top-quality documents in-house.
Scalable CAD data management solutions meet the needs of all manufacturers, from startups and very small firms to larger manufacturers with distributed operations. Data management in Solid Edge shares product information and collaborates with downstream functions such as manufacturing to improve quality and reduce costly errors.
|
In the past, much of the knowledge we relied on was solely in the heads of individuals. Using Teamcenter Data Management as a single source of product data optimizes processes, reduces errors, and eliminates rework. |
|
|
Thomas Friederich IT Manager at Lista Office LO |
Instantly, securely, and easily collaborate with colleagues, partners, and customers with Siemens’ next-generation, cloud-based collaboration solution, Xcelerator Share. Xcelerator Share and Solid Edge offer a wide range of collaboration features. Xcelerator Share’s rich set of capabilities addresses your cloud collaboration needs, from providing your team with secure, central storage with optional data management tools, to enabling ad hoc collaboration with external stakeholders thanks to easy email address-based sharing.
|
From day one of using Xcelerator Share, I could easily log in and access the progress of our hoist design no matter where I was working – whether from home on my phone, on the road with my laptop, or in the office on my desktop computer. On many occasions throughout the design process, I was also able to address issues and make suggestions. It didn’t matter if I was 20 feet or 500 miles away. |
|
|
Bob Brown President Harsh International |
© 2023 Siemens Industry Software Inc. Siemens and the Siemens logo are registered trademarks of Siemens AG.
All other trademarks, registered trademarks or service marks belong to their respective holders.